File List
Here is a list of all files with brief descriptions:
 ADC.hAnalog to Digital Conversion (ADC) Input Driver
 ADCBuf.hAnalog to Digital Conversion Buffer (ADCBuf) Input Driver
 ADCBufLPF3.hADCBuf driver implementation for an LPF3 analog-to-digital converter
 ADCLPF3.hADC driver implementation for the ADC peripheral on Low Power F3 devices
 AnsiColor.h
 APULPF3.hPRELIMINARY APU driver interface
 APULPF3_FW.h
 BatMonSupportLPF3.hBatMon Support layer
 BatteryMonitor.hBattery Monitor driver
 BatteryMonitorLPF3.hBattery Monitor driver implementation for the LPF3 family
 Board.hPortable board-specific symbols
 Button.hButton driver
 CAN.hController Area Network (CAN) Driver Interface
 CANCC27XX.hCAN driver implementation for the CC27XX family
 CANMCAN.hCommon CAN functions for MCAN configuration
 ClockP.hClock interface for the RTOS Porting Interface
 ClockPLPF3.h
 CommonResourceXXF3.hShared resources to arbitrate access to the HSM, CAN, and APU
 Comparator.hComparator Driver
 ComparatorLPF3LP.h
 DebugP.hDebug support
 Display.hGeneric interface for text output
 DisplayHost.hDisplay driver for printf-like output
 DisplayUart2.hDisplay.h implementation for UART output
 Driver_Init.h
 EventP.hEvent Group support
 GPIO.hGeneral Purpose I/O driver interface
 GPIOLPF3.hGPIO driver implementation for Low Power F3 devices
 HSMResourceXXF3.hShared resources to arbitrate access to the HSM
 hw_cpu_dwt.h
 hw_cpu_itm.h
 hw_cpu_scs.h
 hw_cpu_tpiu.h
 HwiP.hHardware Interrupt module for the RTOS Porting Interface
 I2C.hInter-Integrated Circuit (I2C) Controller Driver
 I2CLPF3.hI2C driver implementation for a Low Power F3 device I2C controller
 I2CSupport.hHolder of common helper functions for the I2C driver
 I2CTarget.hI2CTarget driver interface
 I2CTargetLPF3.hI2CTarget driver implementation for a Low Power F3 device I2C target
 I2S.hInter-Integrated Circuit Sound (I2S) Bus Driver
 I2SLPF3.hI2S driver implementation for LPF3 devices
 ITM.hITM driver header
 ITMLPF3.hCC27XX specific ITM implementation
 LED.hLED driver
 LGPTimerLPF3.hLGPTimer driver implementation for Low Power F3 devices
 List.hLinked List interface for use in drivers
 LogSinkBuf.h
 LogSinkITM.hPRELIMINARY LogSinkITM interface
 LogSinkTraceLPF3.hPRELIMINARY LogSinkTraceLPF3 interface
 LogSinkUART.hPRELIMINARY LogSinkUART interface
 Math.hMath utility functions
 MCAN.hHardware abstraction layer for M_CAN Controller v3.2.1
 MCAN_reg.hM_CAN controller v3.2.1 register definitions
 MessageQueueP.hMessageQueue module for the RTOS Porting Interface
 MutexP.hMutex module for the RTOS Porting Interface
 NoRTOS.hNoRTOS framework module
 NVS.hNon-Volatile Storage driver interface
 NVSLPF3.hNon-Volatile Storage driver for Low Power F3 devices
 NVSRAM.hRAM implementation of the NVS driver
 NVSSPI25X.hNon-Volatile Storage driver implementation for SPI flash peripherals
 Power.hPower Manager
 PowerCC23X0.hPower manager interface for CC23X0 devices
 PowerCC27XX.hPower manager interface for CC27XX
 PowerCC27XX_s.hInterface for Secure Power driver for CC27XX. Not to be used by non-secure application
 PowerCC27XX_veneers.hSecure Power API functions available from non-secure context through veneers
 PWM.hPulse Width Modulation (PWM) driver
 PWMTimerLPF3.hPWM driver implementation for Low Power F3 devices
 QueueP.h
 RingBuf.h
 SD.hSecure Digital (SD) Driver
 SDFatFS.hFile Allocation Table File System (FATFS) Driver
 SDSPI.hSD driver implementation built on the TI SPI driver
 SecureCallback.h
 SecureCallback_s.h
 SemaphoreP.hSemaphore module for the RTOS Porting Interface
 SPI.hSerial Peripheral Interface (SPI) Driver Interface
 spiffs.h
 SPIFFSNVS.hModule to enable the SPI Flash File System (SPIFFS) on the TI NVS driver
 SPILPF3DMA.hSPI driver implementation for a Low Power F3 device SPI controller using the UDMA controller
 StructRingBuf.h
 SwiP.hSoftware Interrupt module for the RTOS Porting Interface
 SystemP.hSystem module for the RTOS Porting Interface
 TaskP.hTask module for the RTOS Porting Interface
 TCAN455X.hTCAN455X Driver Interface
 TCAN455X_reg.hTCAN455X device-specific register definitions
 Temperature.hTemperature driver
 TemperatureLPF3.hTemperature driver implementation for the Low Power F3 family
 TimestampP.hTimestamp module for the RTOS Porting Interface
 types.h
 UART2.hPRELIMINARY UART driver interface
 UART2LPF3.hUART driver implementation for a Low Power F3 device UART controller
 UART2Support.hHolder of common helper functions for the UART driver
 UDMALPF3.hUDMALPF3 driver implementation
 unistd.h
 Watchdog.hWatchdog driver interface
 WatchdogLPF3.hWatchdog driver implementation for Low Power F3 devices
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale