Data Structures | Macros | Typedefs | Enumerations | Functions
MutexP.h File Reference

Detailed Description

Mutex module for the RTOS Porting Interface.

============================================================================

The MutexP module allows tasks to maintain critical region segments. The MutexP module has two main functions: MutexP_lock and MutexP_unlock.

The MutexP module supports recursive calls to the MutexP_lock API by a single task. The same number of MutexP_unlock calls must be done for the mutex to be release. Note: the returned key must be provided in the LIFO order. For example:

uintptr_t key1, key2;
key1 = MutexP_lock();
key2 = MutexP_lock();

#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
Include dependency graph for MutexP.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

union  MutexP_Struct
 MutexP structure. More...
 
struct  MutexP_Params
 Basic MutexP Parameters. More...
 

Macros

#define MutexP_STRUCT_SIZE   (80)
 Number of bytes greater than or equal to the size of any RTOS MutexP object. More...
 

Typedefs

typedef union MutexP_Struct MutexP_Struct
 MutexP structure. More...
 
typedef void * MutexP_Handle
 Opaque client reference to an instance of a MutexP. More...
 

Enumerations

enum  MutexP_Status { MutexP_OK = 0, MutexP_FAILURE = -1 }
 Status codes for MutexP APIs. More...
 

Functions

MutexP_Handle MutexP_construct (MutexP_Struct *handle, MutexP_Params *params)
 Function to construct a mutex. More...
 
void MutexP_destruct (MutexP_Struct *mutexP)
 Function to destruct a mutex object. More...
 
MutexP_Handle MutexP_create (MutexP_Params *params)
 Function to create a mutex. More...
 
void MutexP_delete (MutexP_Handle handle)
 Function to delete a mutex. More...
 
void MutexP_Params_init (MutexP_Params *params)
 Initialize params structure to default values. More...
 
uintptr_t MutexP_lock (MutexP_Handle handle)
 Function to lock a mutex. More...
 
void MutexP_unlock (MutexP_Handle handle, uintptr_t key)
 Function to unlock a mutex. More...
 

Macro Definition Documentation

§ MutexP_STRUCT_SIZE

#define MutexP_STRUCT_SIZE   (80)

Number of bytes greater than or equal to the size of any RTOS MutexP object.

NoRTOS: 12 BIOS 6.x: 40 BIOS 7.x: 40 FreeRTOS: 80

Typedef Documentation

§ MutexP_Struct

MutexP structure.

Opaque structure that should be large enough to hold any of the RTOS specific MutexP objects.

§ MutexP_Handle

typedef void* MutexP_Handle

Opaque client reference to an instance of a MutexP.

A MutexP_Handle returned from the MutexP_create represents that instance. and then is used in the other instance based functions (e.g. MutexP_lock, MutexP_unlock, etc.).

Enumeration Type Documentation

§ MutexP_Status

Status codes for MutexP APIs.

Enumerator
MutexP_OK 

API completed successfully

MutexP_FAILURE 

API failed

Function Documentation

§ MutexP_construct()

MutexP_Handle MutexP_construct ( MutexP_Struct handle,
MutexP_Params params 
)

Function to construct a mutex.

Parameters
handlePointer to a MutexP_Struct object
paramsPointer to the instance configuration parameters. NULL denotes to use the default parameters (MutexP default parameters as noted in MutexP_Params_init.
Returns
A MutexP_Handle on success or a NULL on an error

§ MutexP_destruct()

void MutexP_destruct ( MutexP_Struct mutexP)

Function to destruct a mutex object.

Parameters
mutexPPointer to a MutexP_Struct object that was passed to MutexP_construct().
Returns

§ MutexP_create()

MutexP_Handle MutexP_create ( MutexP_Params params)

Function to create a mutex.

Parameters
paramsPointer to the instance configuration parameters. NULL denotes to use the default parameters. The MutexP default parameters are noted in MutexP_Params_init.
Returns
A MutexP_Handle on success or a NULL on an error

§ MutexP_delete()

void MutexP_delete ( MutexP_Handle  handle)

Function to delete a mutex.

Parameters
handleA MutexP_Handle returned from MutexP_create

§ MutexP_Params_init()

void MutexP_Params_init ( MutexP_Params params)

Initialize params structure to default values.

The default parameters are: callback - NULL.

Parameters
paramsPointer to the instance configuration parameters.

§ MutexP_lock()

uintptr_t MutexP_lock ( MutexP_Handle  handle)

Function to lock a mutex.

This function can only be called from a Task. It cannot be called from an interrupt. The lock will block until the mutex is available.

Users of a mutex should make every attempt to minimize the duration that that they have it locked. This is to minimize latency. It is recommended that the users of the mutex do not block while they have the mutex locked.

This function locks the mutex. If the mutex is locked multiple times by the caller, the same number of unlocks must be called.

Parameters
handleA MutexP_Handle returned from MutexP_create
Returns
A key is returned. This key must be passed into MutexP_unlock.

§ MutexP_unlock()

void MutexP_unlock ( MutexP_Handle  handle,
uintptr_t  key 
)

Function to unlock a mutex.

This function unlocks the mutex. If the mutex is locked multiple times by the caller, the same number of unlocks must be called. The order of the keys must be reversed. For example

uintptr_t key1, key2;
key1 = MutexP_lock();
key2 = MutexP_lock();
Parameters
handleA MutexP_Handle returned from MutexP_create
keyReturn from MutexP_lock.
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale