Data Structures | Enumerations
I2SLPF3.h File Reference

Detailed Description

I2S driver implementation for LPF3 devices.

============================================================================

Limitations

Supported I2S_MemoryLength values

Only the following memory lengths are supported:

I2S_Params Attributes Limitations

Some attributes in the I2S_Params structure have a limited set of supported values. These limitations are described below:


Sample Buffers

This section describes the structure and requirements for the sample buffers used in the I2S_Transaction objects.

Sample words are read from or written to the sample buffers in little-endian byte order, meaning that the least significant byte (LSByte) is stored at the lower byte address, and the most significant byte (MSByte) is stored at the higher byte address.

The sample buffers are divided into frames which are further subdivided into channels, and if a channel is used by both SD0 and SD1 (where the direction of the two pins are the same), then that channel is further subdivided into a sample word for first SD0 and then SD1.

Buffer Size Requirements

The size of the buffers used in I2S_Transaction objects must be an even multiple of the number of bytes per frame. I.e. the number of bytes in the buffers must be of the form: 2*n*k, where k is the size of a frame in bytes and n is an integer satisfying n>=2. 2*n is the number of frames in the buffer.

General Sample Buffer Structure

Below code describes the general structure of a sample buffer if SD0 and SD1 are configured to the same direction.

struct
{
#if SD0_USE_CHANNEL_0 || SD1_USE_CHANNEL_0
struct
{
#if SD0_USE_CHANNEL_0
uint8_t sd0SampleWord[BYTES_PER_WORD];
#endif
#if SD1_USE_CHANNEL_0
uint8_t sd1SampleWord[BYTES_PER_WORD];
#endif
} channel0;
#endif
#if SD0_USE_CHANNEL_1 || SD1_USE_CHANNEL_1
struct
{
#if SD0_USE_CHANNEL_1
uint8_t sd0SampleWord[BYTES_PER_WORD];
#endif
#if SD1_USE_CHANNEL_1
uint8_t sd1SampleWord[BYTES_PER_WORD];
#endif
} channel1;
#endif
// ...
#if SD0_USE_CHANNEL_8 || SD1_USE_CHANNEL_8
struct
{
#if SD0_USE_CHANNEL_8
uint8_t sd0SampleWord[BYTES_PER_WORD];
#endif
#if SD1_USE_CHANNEL_8
uint8_t sd1SampleWord[BYTES_PER_WORD];
#endif
} channel8;
#endif
} sampleBufferFrames[FRAMES_PER_BUFFER];

Notes:

If SD0 and SD1 are not configured to the same direction (or only one is used) then the structure can be simplified as below:

struct
{
#if USE_CHANNEL_0
uint8_t channel0SampleWord[BYTES_PER_WORD];
#endif
#if USE_CHANNEL_1
uint8_t channel1SampleWord[BYTES_PER_WORD];
#endif
// ...
#if USE_CHANNEL_8
uint8_t channel8SampleWord[BYTES_PER_WORD];
#endif
} sampleBufferFrames[FRAMES_PER_BUFFER];

Notes:

Sample Buffer Structure Example

If for example SD0 and SD1 are configured to the same direction and if channel 0 and 1 are used for SD0 and channel 0 is used for SD1, then the sample buffer would be structured as in the code below.

struct
{
struct
{
uint8_t sd0SampleWord[BYTES_PER_WORD];
uint8_t sd1SampleWord[BYTES_PER_WORD];
} channel0;
struct
{
uint8_t sd0SampleWord[BYTES_PER_WORD];
} channel1;
} sampleBufferFrames[FRAMES_PER_BUFFER];
// Access LSB of sample 10 of channel 0 on SD1
uint8_t tmp = sampleBufferFrames[10].channel0.sd1SampleWord[0];

Selecting the Audio Frequency Clock

Using I2SLPF3_HWAttrs.afclkSrc it is possible to select the audio frequency clock (AFCLK) source. AFCLK is used by the I2S hardware module when the I2S driver is opened in Controller mode (I2S_Params.moduleRole == I2S_CONTROLLER) The I2S hardware module will divide the AFCLK to generate the I2S clocks (BCLK (SCK), WCLK (Ws) and CCLK). The AFCLK therefore directly determines the possible sample rates, i.e. the frequency of WCLK.

To achieve a desired sample frequency (f_s), the following requirements must be met, where f_afclk is the frequency of the AFCLK:

For example, if f_s = 44.1 kHz, then the first requirement is met if for example f_afclk = 90.3168 MHz = 2048 * 44.1 kHz. The second requirement is met if for example the number of bits per frame is 32, because it evenly divides into 2048.

If the requirements are not met, the closest possible sampling frequency to the desired sampling frequency will be used.

To achieve the most common sample frequencies, it is suggested to select AFOSC as the AFCLK source, since its frequency can be configured to be a multiple of the most common sample rates.

Using AFOSC

See PowerLPF3_AfoscFreq for the list of possible frequencies that the AFOSC can be configured to. The frequencies most suited to be used with I2S are listed below:


#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/I2S.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/Power.h>
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(driverlib/ckmd.h)>
Include dependency graph for I2SLPF3.h:

Go to the source code of this file.

Data Structures

struct  I2SLPF3_HWAttrs
 I2S Hardware attributes. More...
 

Enumerations

enum  I2SLPF3_AfclkSrc { I2SLPF3_AFCLK_SRC_CLKREF = CKMD_AFCLK_SOURCE_CLKREF, I2SLPF3_AFCLK_SRC_CLKHF = CKMD_AFCLK_SOURCE_CLKHF, I2SLPF3_AFCLK_SRC_CLKAF = CKMD_AFCLK_SOURCE_CLKAF }
 Audio Frequency Clock Source. More...
 

Enumeration Type Documentation

§ I2SLPF3_AfclkSrc

Audio Frequency Clock Source.

Option to select the clock source used by the I2S hardware module when the I2S driver is opened in Controller mode.

See also
Selecting the Audio Frequency Clock
Enumerator
I2SLPF3_AFCLK_SRC_CLKREF 

48MHz reference clock (HFXT)

I2SLPF3_AFCLK_SRC_CLKHF 

96MHz CLKHF

I2SLPF3_AFCLK_SRC_CLKAF 

AFOSC clock

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale