![]() |
![]() |
Shared resources to arbitrate access to the HSM.
============================================================================

Go to the source code of this file.
Functions | |
| void | HSMResourceXXF3_constructRTOSObject (void) |
| bool | HSMResourceXXF3_acquireLock (uint32_t timeout) |
| void | HSMResourceXXF3_releaseLock (void) |
| void HSMResourceXXF3_constructRTOSObject | ( | void | ) |
| bool HSMResourceXXF3_acquireLock | ( | uint32_t | timeout | ) |
| void HSMResourceXXF3_releaseLock | ( | void | ) |