![]() |
![]() |
Shared resources to arbitrate access to the HSM, CAN, and APU.
============================================================================

Go to the source code of this file.
Functions | |
| void | CommonResourceXXF3_constructRTOSObjects (void) |
| bool | CommonResourceXXF3_acquireLock (uint32_t timeout) |
| void | CommonResourceXXF3_releaseLock (void) |
| bool | CommonResourceXXF3_acquireLockWithDelay (void) |
| void CommonResourceXXF3_constructRTOSObjects | ( | void | ) |
| bool CommonResourceXXF3_acquireLock | ( | uint32_t | timeout | ) |
| void CommonResourceXXF3_releaseLock | ( | void | ) |
| bool CommonResourceXXF3_acquireLockWithDelay | ( | void | ) |