RTC

Instance: RTC
Component: RTC
Base address: 0x40002000


ULL Real Time Clock module
RTC includes 2 channels.
- Channel 0 is a compare channel
- Channel 1 is a capture channel

TOP:RTC Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

DESC

RO

32

0x6442 1010

0x0000 0000

0x4000 2000

CTL

RW

32

0x0000 0000

0x0000 0004

0x4000 2004

ARMSET

RW

32

0x0000 0000

0x0000 0008

0x4000 2008

ARMCLR

RW

32

0x0000 0000

0x0000 000C

0x4000 200C

TIME250N

RO

32

0x0000 0000

0x0000 0010

0x4000 2010

TIME1U

RO

32

0x0000 0000

0x0000 0014

0x4000 2014

TIME8U

RO

32

0x0000 0000

0x0000 0018

0x4000 2018

TIME524M

RO

32

0x0000 0000

0x0000 001C

0x4000 201C

CH0CC250N

RW

32

0x0000 0000

0x0000 0020

0x4000 2020

CH0CC1U

RW

32

0x0000 0000

0x0000 0024

0x4000 2024

CH0CC8U

RW

32

0x0000 0000

0x0000 0028

0x4000 2028

CH1CC8U

RO

32

0x0000 0000

0x0000 0038

0x4000 2038

CH1CFG

RW

32

0x0000 0000

0x0000 003C

0x4000 203C

IMASK

RW

32

0x0000 0000

0x0000 0044

0x4000 2044

RIS

RO

32

0x0000 0000

0x0000 0048

0x4000 2048

MIS

RO

32

0x0000 0000

0x0000 004C

0x4000 204C

ISET

WO

32

0x0000 0000

0x0000 0050

0x4000 2050

ICLR

WO

32

0x0000 0000

0x0000 0054

0x4000 2054

IMSET

WO

32

0x0000 0000

0x0000 0058

0x4000 2058

IMCLR

WO

32

0x0000 0000

0x0000 005C

0x4000 205C

EMU

RW

32

0x0000 0000

0x0000 0060

0x4000 2060

DTIME

WO

32

0x0000 0000

0x0000 0068

0x4000 2068

TOP:RTC Register Descriptions

TOP:RTC:DESC

Address Offset 0x0000 0000
Physical Address 0x4000 2000 Instance 0x4000 2000
Description Description Register. This register provides IP module ID, revision information, instance index and standard MMR registers offset.
Type RO
Bits Field Name Description Type Reset
31:16 MODID Module identifier used to uniquely identify this IP. RO 0x6442
15:12 STDIPOFF Standard IP MMR block offset. Standard IP MMRs are the set of from aggregated IRQ registers till DTB.

0: Standard IP MMRs do not exist

0x1-0xF: Standard IP MMRs begin at offset of (64*STDIPOFF from the base IP address)
RO 0x1
11:8 INSTIDX IP Instance ID number. If multiple instances of IP exist in the device, this field can identify the instance number (0-15). RO 0x0
7:4 MAJREV Major revision of IP (0-15). RO 0x1
3:0 MINREV Minor revision of IP (0-15). RO 0x0

TOP:RTC:CTL

Address Offset 0x0000 0004
Physical Address 0x4000 2004 Instance 0x4000 2004
Description RTC Control register. This register controls resetting the of RTC counter
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 RST RTC counter reset. Writing 1 to this bit will reset the RTC counter, and cause it to resume counting from 0x0
Value ENUM Name Description
0x0 NOEFF No effect
0x1 CLR Reset the timer.
WO 0

TOP:RTC:ARMSET

Address Offset 0x0000 0008
Physical Address 0x4000 2008 Instance 0x4000 2008
Description RTC channel mode set register. Read to each bit field of this register provides the current channel mode.
- Read of 1'b0 indicates the channel is unarmed.
- Read of 1'b1 indicates the channel is either in capture or compare mode.

A write to each bitfield of this register the following effect:
- Write of 1'b0 has no effect on channel mode.
- Write of 1'b1 has no effect on the compare channel. While write of 1'b1 for capture channel will arm it in capture mode if it is disabled.
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 CH1 Arming Channel 1 for capture operation.
Value ENUM Name Description
0x0 NOEFF No effect on the channel
0x1 SET Enable the Channel 1 for capture operation
RW 0
0 CH0 No effect on arming the channel. Read will give the status of the Channel 0.
Value ENUM Name Description
0x0 NOEFF No effect on the channel
0x1 SET No effect on the compare channel
RW 0

TOP:RTC:ARMCLR

Address Offset 0x0000 000C
Physical Address 0x4000 200C Instance 0x4000 200C
Description RTC channel mode clear register. Read to each bit field of this register provides the current channel mode.
- Read of 1'b0 indicates the channel is unarmed.
- Read of 1'b1 indicates the channel is either in capture or compare mode.

A write to each bitfield of this register the following effect:
- Write of 1'b0 has no effect on channel mode.
- Write of 1'b1 for capture/compare channel will disarm it without triggering event unless a compare/capture event happens in the same cycle.
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 CH1 Disarming Channel 1
Value ENUM Name Description
0x0 NOEFF No effect on the channel
0x1 CLR Set channel in UNARMED state without triggering event unless a capture event happens in the same cycle
RW 0
0 CH0 Disarming Channel 0
Value ENUM Name Description
0x0 NOEFF No effect on the channel
0x1 CLR Set channel in UNARMED state without triggering event unless a compare event happens in the same cycle
RW 0

TOP:RTC:TIME250N

Address Offset 0x0000 0010
Physical Address 0x4000 2010 Instance 0x4000 2010
Description RTC Time value register. 32-bit unsigned integer representing [29:-2] time slice of the real time clock counter. The counter runs on LFCLK. This field has a resolution of 250ns, and range of about 17.8 minutes.
Type RO
Bits Field Name Description Type Reset
31:0 VAL [29:-2] slice of RTC TIME[50:-2]. Slice has an LSB weight of 250 ns and modular range 17m 53.74182002 s. RTC.TIME is updated every LF clock modulo by a fixed or measured LFINC value and will thus on average update only every ~30.5 us.

SYSTIM.TIME is synchronized to RTC TIME[31:-2] and is updated every 250 ns if better resolution is needed (in addition to having a much shorter access time of 1-2 cycles instead of 22-26 cycles for RTC.TIMEx).
RO 0x0000 0000

TOP:RTC:TIME1U

Address Offset 0x0000 0014
Physical Address 0x4000 2014 Instance 0x4000 2014
Description RTC Time value register. 32-bit unsigned integer representing [31:0] time slice of the real time clock counter. The counter runs on LFCLK. This field has a resolution of 1us, and range of about 1.19 hours.
Type RO
Bits Field Name Description Type Reset
31:0 VAL [31:0] slice of RTC TIME[50:-2]. Slice has an LSB weight of 1 us and modular range 1h 11m 34.967296s. RTC.TIME is updated every LF clock modulo by a fixed or measured LFINC value and will thus on average update only every ~30.5 us.

SYSTIM.TIME is synchronized to RTC TIME[31:-2] and is updated every 250 ns if better resolution is needed (in addition to having a much shorter access time of 1-2 cycles instead of 22-26 cycles for RTC.TIMEx).
RO 0x0000 0000

TOP:RTC:TIME8U

Address Offset 0x0000 0018
Physical Address 0x4000 2018 Instance 0x4000 2018
Description RTC Time value register. 32-bit unsigned integer representing [34:3] time slice of the real time clock counter. The counter runs on LFCLK. This field has a resolution of 8us, and range of about 9.5 hours.
Type RO
Bits Field Name Description Type Reset
31:0 VAL [34:3] slice of RTC TIME[50:-2]. Slice has an LSB weight of 8 us and modular range 9h 32m 39.73836s. RTC.TIME is updated every LF clock modulo by a fixed or measured LFINC value and will thus on average update only every ~30.5 us.

SYSTIM.TIME is synchronized to RTC TIME[31:-2] and is updated every 250 ns if better resolution is needed (in addition to having a much shorter access time of 1-2 cycles instead of 22-26 cycles for RTC.TIMEx).
RO 0x0000 0000

TOP:RTC:TIME524M

Address Offset 0x0000 001C
Physical Address 0x4000 201C Instance 0x4000 201C
Description RTC time value register. 32-bit unsigned integer representing [50:19] time slice of the real time clock counter. This field has a resolution of about 0.5s and a range of about 71.4 years.
Type RO
Bits Field Name Description Type Reset
31:0 VAL [50:19] slice of RTC TIME[50:-2]. Slice has an LSB weight of 0.524288s and modular range of approximately 71 years 147 days 11h 56m 53s. RTC.TIME is updated every LF clock modulo by a fixed or measured LFINC value and will thus on average update only every ~30.5 us.

SYSTIM.TIME is synchronized to RTC TIME[31:-2] and is updated every 250 ns if better resolution is needed (in addition to having a much shorter access time of 1-2 cycles instead of 22-26 cycles for RTC.TIMEx).
RO 0x0000 0000

TOP:RTC:CH0CC250N

Address Offset 0x0000 0020
Physical Address 0x4000 2020 Instance 0x4000 2020
Description Channel 0 compare value with 250ns resolution. A read to this register returns the value {CH0CC8U[29:3], 5b’0}
A write to this register arms the channel in compare mode. Event would occur at the same time +/ Tlfclk/2 on the RTC as if it was written to SYSTIM.
Type RW
Bits Field Name Description Type Reset
31:0 VAL RTC Channel 0 compare value. This value is compared against TIME8U.VAL. A Channel 0 event is generated when TIME8U.VAL value reaches or exceeds this compare value. RW 0x0000 0000

TOP:RTC:CH0CC1U

Address Offset 0x0000 0024
Physical Address 0x4000 2024 Instance 0x4000 2024
Description Channel 0 compare value with 1us resolution. A read to this register returns the value {CH0CC8U[31:3], 3b’0}
A write to this register arms the channel in compare mode. Event would occur at the same time +/ Tlfclk/2 on the RTC as if it was written to SYSTIM.
Type RW
Bits Field Name Description Type Reset
31:0 VAL RTC Channel 0 compare value. This value is compared against TIME8U.VAL. A Channel 0 event is generated when TIME8U.VAL value reaches or exceeds this compare value. RW 0x0000 0000

TOP:RTC:CH0CC8U

Address Offset 0x0000 0028
Physical Address 0x4000 2028 Instance 0x4000 2028
Description Channel 0 compare value. A write to this register automatically enables the channel to trigger an event when RTC timer reaches the programmed value or if the programmed value is 1 sec in the past.
Type RW
Bits Field Name Description Type Reset
31:0 VAL RTC Channel 0 compare value. This value is compared against TIME8U.VAL. A Channel 0 event is generated when TIME8U.VAL value reaches or exceeds this compare value. RW 0x0000 0000

TOP:RTC:CH1CC8U

Address Offset 0x0000 0038
Physical Address 0x4000 2038 Instance 0x4000 2038
Description Channel 1 capture value. This register captures the RTC time slice [34:3] on each selected edge of the capture event when the ARMSET.CH1 = 1.
Type RO
Bits Field Name Description Type Reset
31:21 RESERVED21 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000
20:0 VAL TIME8U.VAL captured value at the last selected edge of capture event. RO 0b0 0000 0000 0000 0000 0000

TOP:RTC:CH1CFG

Address Offset 0x0000 003C
Physical Address 0x4000 203C Instance 0x4000 203C
Description Channel 1 configuration register. This register can be used to select the capture edge for generating the capture event.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 EDGE Edge detect configuration for capture source
Value ENUM Name Description
0x0 RISE Rising Edge.
0x1 FALL Falling Edge.
RW 0

TOP:RTC:IMASK

Address Offset 0x0000 0044
Physical Address 0x4000 2044 Instance 0x4000 2044
Description Interrupt Mask. If a bit is set, then corresponding interrupt is un-masked. Un-masking the interrupt causes the raw interrupt to be visible in IIDX, as well as MIS.
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 EV1 Channel 1 Event Interrupt Mask.
Value ENUM Name Description
0x0 DIS Clear Interrupt Mask
0x1 EN Enable Interrrupt Mask
RW 0
0 EV0 Channel 0 Event Interrupt Mask.
Value ENUM Name Description
0x0 DIS Disable Interrupt Mask
0x1 EN Enable Interrrupt Mask
RW 0

TOP:RTC:RIS

Address Offset 0x0000 0048
Physical Address 0x4000 2048 Instance 0x4000 2048
Description Interrupt mask. This register selects interrupt sources which are allowed to pass from RIS to MIS when the corresponding bit-fields are set to 1.
Type RO
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 EV1 Raw interrupt status for Channel 1 event.
This bit is set to 1 when a capture event is received on Channel 1.
This bit will be cleared when the bit in ICLR.EV1 is set to 1 or when the captured time value is read from the CH1CC8U register.
Value ENUM Name Description
0x0 CLR Interrupt did not occur
0x1 SET Interrupt occured
RO 0
0 EV0 Raw interrupt status for Channel 0 event.
This bit is set to 1 when a compare event occurs on Channel 0.
This bit will be cleared. When the corresponding bit in ICLR.EV0 is set to 1. Or when a new compare value is written in CH0CC8U register
Value ENUM Name Description
0x0 CLR Interrupt did not occur
0x1 SET Interrupt occured
RO 0

TOP:RTC:MIS

Address Offset 0x0000 004C
Physical Address 0x4000 204C Instance 0x4000 204C
Description Masked interrupt status. This register is simply a bitwise AND of the contents of IMASK and RIS.*] registers. A flag set in this register can be cleared by writing 1 to the corresponding ICLR register bit.
Type RO
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 EV1 Masked interrupt status for channel 1 event.
Value ENUM Name Description
0x0 CLR Interrupt did not occur
0x1 SET Interrupt occured
RO 0
0 EV0 Masked interrupt status for channel 0 event.
Value ENUM Name Description
0x0 CLR Interrupt did not occur
0x1 SET Interrupt occured
RO 0

TOP:RTC:ISET

Address Offset 0x0000 0050
Physical Address 0x4000 2050 Instance 0x4000 2050
Description Interrupt set register. This register can used by software for diagnostics and safety checking purposes. Writing a 1 to a bit in this register will set the event and the corresponding RIS bit also gets set. If the corresponding IMASK bit is set, then the corresponding MIS register bit also gets set.
Type WO
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 EV1 Set Channel 1 event Interrupt.
Value ENUM Name Description
0x0 NO_EFFECT Writing 0 has no effect
0x1 SET Set interrupt
WO 0
0 EV0 Set Channel 0 event Interrupt.
Value ENUM Name Description
0x0 NO_EFFECT Writing 0 has no effect
0x1 SET Set interrupt
WO 0

TOP:RTC:ICLR

Address Offset 0x0000 0054
Physical Address 0x4000 2054 Instance 0x4000 2054
Description Interrupt clear register. This register allows software to clear interrupts. Writing a 1 to a bit in this register will clear the event and the corresponding RIS bit also gets cleared. If the corresponding IMASK bit is set, then the corresponding MIS register bit also gets cleared.
Type WO
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 EV1 Clears channel 1 event interrupt.
Value ENUM Name Description
0x0 NO_EFF Writing 0 has no effect
0x1 CLR Clear Interrupt
WO 0
0 EV0 Clears channel 0 event interrupt.
Value ENUM Name Description
0x0 NO_EFF Writing 0 has no effect
0x1 CLR Clear Interrupt.
WO 0

TOP:RTC:IMSET

Address Offset 0x0000 0058
Physical Address 0x4000 2058 Instance 0x4000 2058
Description Interrupt mask set register. Writing a 1 to a bit in this register will set the corresponding IMASK bit.
Type WO
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 EV1 Set channel 1 event interrupt mask.
Value ENUM Name Description
0x0 NO_EFF Writing 0 has no effect
0x1 SET Set interrupt mask
WO 0
0 EV0 Set channel 0 event interrupt mask.
Value ENUM Name Description
0x0 NO_EFF Writing 0 has no effect
0x1 SET Set interrupt mask
WO 0

TOP:RTC:IMCLR

Address Offset 0x0000 005C
Physical Address 0x4000 205C Instance 0x4000 205C
Description Interrupt mask clear register. Writing a 1 to a bit in this register will clear the corresponding IMASK bit.
Type WO
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 EV1 Clears Channel 1 event interrupt mask.
Value ENUM Name Description
0x0 NO_EFF Writing 0 has no effect
0x1 CLR Clear Interrupt Mask
WO 0
0 EV0 Clears Channel 0 event interrupt mask.
Value ENUM Name Description
0x0 NO_EFF Writing 0 has no effect
0x1 CLR Clear Interrupt Mask
WO 0

TOP:RTC:EMU

Address Offset 0x0000 0060
Physical Address 0x4000 2060 Instance 0x4000 2060
Description Emulation control register. This register controls the behavior of the IP related to core halted input.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 HALT Halt control.
Value ENUM Name Description
0x0 RUN Free run option. The IP ignores the state of the core halted input.
0x1 STOP Freeze option. The IP freezes functionality when the core halted input is asserted, and resumes when it is deasserted. The freeze can either be immediate or after the IP has reached a boundary from where it can resume without corruption.
RW 0

TOP:RTC:DTIME

Address Offset 0x0000 0068
Physical Address 0x4000 2068 Instance 0x4000 2068
Description A delta time mechanism is implemented for RTC that allows the TIME value to be adjusted under software control. This is used by boot code to perform the compensation for reset duration (accomplished by adding MMR write to FCFG.generalTrims copylist to avoid ROM changes)
TIME[50:-2] is adjusted by TIME += sxt(MANT[30:0], 53) * 2^(22*EXP).
In other words:
(EXP==0): TIME is adjusted by MANT * 250 ns (range +/-134 s)
(EXP==1): TIME is adjusted by MANT * 1.049 s (range +/- 35.7 yr)
If used by an application to adjust RTC TIME value, the write to DTIME must occur as quickly as possible after an lftick event. It should also be followed by a write of 1 to SYSTIM.STATUS.SYNCUP to ensure that SYSTIM resynchronizes to the new RTC TIME value at the next lftick event.
Type WO
Bits Field Name Description Type Reset
31 EXP Exponent WO 0
30:0 MANT Mantissa WO 0b000 0000 0000 0000 0000 0000 0000 0000