Instance: AES
Component: AES
Base address: 0x400C0000
The AES-128 crypto peripheral accellerates AES-128 block cipher encryption and decryption. The peripheral does also offer hardware features to accellerate cipher modes implemented in software:
* CBC-MAC
* CBC
* CTR
* CFB
* OFB
* PCBC
The module provides two data registers that can be input to AES operation. These are termed TXT and BUF. TXT is the AES-128 work buffer, and content changes during an AES operation. Software cannot update TXT during an ongoing AES operation. BUF is an auxiliary 128-bit buffer with multiple purposes:
* initialization vector(IV) storage
* counter in CTR cipher mode
* hold next value of TXT
Software can update BUF during an AES operation. This allows software to write next TXT during an ongoing AES operation and hence save AES idle times.
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
|
RO |
32 |
0x6B42 4010 |
0x0000 0000 |
0x400C 0000 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0010 |
0x400C 0010 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0014 |
0x400C 0014 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0018 |
0x400C 0018 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 001C |
0x400C 001C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0x400C 0020 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x400C 0024 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0x400C 0028 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x400C 002C |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0050 |
0x400C 0050 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0054 |
0x400C 0054 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0058 |
0x400C 0058 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 005C |
0x400C 005C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0070 |
0x400C 0070 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0074 |
0x400C 0074 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0078 |
0x400C 0078 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 007C |
0x400C 007C |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0080 |
0x400C 0080 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0084 |
0x400C 0084 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0088 |
0x400C 0088 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 008C |
0x400C 008C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0090 |
0x400C 0090 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0094 |
0x400C 0094 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0098 |
0x400C 0098 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 009C |
0x400C 009C |
|
|
RO |
32 |
0x0000 0000 |
0x0000 00A0 |
0x400C 00A0 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 00A4 |
0x400C 00A4 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 00A8 |
0x400C 00A8 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 00AC |
0x400C 00AC |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0104 |
0x400C 0104 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0108 |
0x400C 0108 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 010C |
0x400C 010C |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0110 |
0x400C 0110 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0114 |
0x400C 0114 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0118 |
0x400C 0118 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 011C |
0x400C 011C |
| Address Offset | 0x0000 0000 | ||
| Physical Address | 0x400C 0000 | Instance | 0x400C 0000 |
| Description | Description Register. This register provides IP module ID, revision information, instance index and standard MMR registers offset. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | MODID | Module Identifier This register is used to uniquely identify this IP. |
RO | 0x6B42 | ||
| 15:12 | STDIPOFF | Standard IP MMR block offset Standard IP MMRs are the set from aggregated IRQ registers till DTB. 0: Standard IP MMRs do not exist. 0x1-0xF: Standard IP MMRs begin at offset of 64*STDIPOFF from the base IP address. |
RO | 0x4 | ||
| 11:8 | INSTIDX | IP Instance ID number If multiple instances of IP exist in the device, this field can identify the instance number (0-15). |
RO | 0x0 | ||
| 7:4 | MAJREV | Major revision of IP (0-15) | RO | 0x1 | ||
| 3:0 | MINREV | Minor Revision of IP(0-15) | RO | 0x0 | ||
| Address Offset | 0x0000 0010 | ||
| Physical Address | 0x400C 0010 | Instance | 0x400C 0010 |
| Description | Trigger This register is used to manually trigger operations. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||||||||||||||
| 3 | DMACHA | Manually trigger channel A request
|
WO | 0 | ||||||||||||||
| 2 | DMACHB | Manually trigger channel B request
|
WO | 0 | ||||||||||||||
| 1:0 | AESOP | AES Operation Write an enumerated value to this field when STA.STATE = IDLE to manually trigger an AES operation. If condition is not met, the trigger is ignored. Non-enumerated values are ignored. Enumerated value indicates source of AES operation
|
WO | 0b00 | ||||||||||||||
| Address Offset | 0x0000 0014 | ||
| Physical Address | 0x400C 0014 | Instance | 0x400C 0014 |
| Description | Abort This register is used to abort current AES operation. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 0 | ABORTAES | Abort AES operation Abort an ongoing AES operation. An abort will clear TXT, BUF, DMA, AUTOCFG registers
|
WO | 0 | |||||||||||
| Address Offset | 0x0000 0018 | ||
| Physical Address | 0x400C 0018 | Instance | 0x400C 0018 |
| Description | Clear This register is used to clear contents of TXT and BUF when STA.STATE = IDLE. If condition is not met, the contents remain unchanged. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 1 | TXT | Clear TXT
|
WO | 0 | |||||||||||
| 0 | BUF | Clear BUF
|
WO | 0 | |||||||||||
| Address Offset | 0x0000 001C | ||
| Physical Address | 0x400C 001C | Instance | 0x400C 001C |
| Description | Status This register provides information on AES accellerator state and BUF status. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:5 | RESERVED5 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 4:3 | KEYINTID | KEY Initiator ID ID of the most recent AHB Initiator which has written into one of the KEY0 to KEY3 registers
|
RO | 0b00 | |||||||||||
| 2 | KEYSTATE | KEY State Indicates whether data in KEY0 to KEY3 is valid or not. AES operations are not allowed until KEY is valid
|
RO | 0 | |||||||||||
| 1 | BUFSTA | BUF Status Field gives the status of BUF, indicating EMPTY or FULL, when AUTOCFG.TRGAES = WRBUF3. If AUTOCFG.TRGAES != WRBUF3, then STA.BUFSTA will hold the value 0. Note : Useful for CBC-MAC
|
RO | 0 | |||||||||||
| 0 | STATE | State Field gives the state of the AES engine.
|
RO | 0 | |||||||||||
| Address Offset | 0x0000 0020 | ||
| Physical Address | 0x400C 0020 | Instance | 0x400C 0020 |
| Description | Direct Memory Access This register controls the conditions that will generate burst requests on each DMA channel. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||
| 31:20 | RESERVED20 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 | ||||||||||||||||||||
| 19:16 | DONEACT | Done Action This field determines the side effects of DMA done. It is allowed to configure this field with an OR-combination of supported enums, with the exception that GATE_TRGAES_ON_CHA and GATE_TRGAES_ON_CHA_DEL must be mutually exclusive
|
RW | 0x0 | ||||||||||||||||||||
| 15:14 | RESERVED14 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||||||||||||||||||||
| 13:12 | ADRCHB | Channel B Read Write Address The DMA accesses DMACHB to read or write contents of TXT and BUF as a response to a burst request. This field specifes the start address of the first DMA transfer that follows the burst request. The internal address gets incremented automatically for subsequent accesses. The DMA can transfer 8-bit, 16-bit, or 32-bit words, and must always complete a 16-byte transfer before re-arbitration.
|
RW | 0b00 | ||||||||||||||||||||
| 11 | RESERVED11 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||||||||||||||||||||
| 10:8 | TRGCHB | Channel B Trigger Select the condition that triggers DMA channel B request. Non-enumerated values are not supported and ignored.
|
RW | 0b000 | ||||||||||||||||||||
| 7:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||||||||||||||||||||
| 5:4 | ADRCHA | Channel A Read Write Address The DMA accesses DMACHA to read or write contents of TXT and BUF as a response to a burst request. This field specifes the start address of the first DMA transfer that follows the burst request. The internal address gets incremented automatically for subsequent accesses. The DMA can transfer 8-bit, 16-bit, or 32-bit words, and must always complete a 16-byte transfer before re-arbitration.
|
RW | 0b00 | ||||||||||||||||||||
| 3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||||||||||||||||||||
| 2:0 | TRGCHA | Channel A Trigger Select the condition that triggers DMA channel A request. Non-enumerated values are not supported and ignored.
|
RW | 0b000 | ||||||||||||||||||||
| Address Offset | 0x0000 0024 | ||
| Physical Address | 0x400C 0024 | Instance | 0x400C 0024 |
| Description | DMA Channel A data transfer DMA accesses this register to read or write contents from sequential addresses specifed by DMA.ADRCHA. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value transferred through DMA Channel A | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0028 | ||
| Physical Address | 0x400C 0028 | Instance | 0x400C 0028 |
| Description | DMA Channel B data transfer DMA accesses this register to read or write contents from sequential addresses specifed by DMA.ADRCHB. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value transferred through DMA Channel B | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 002C | ||
| Physical Address | 0x400C 002C | Instance | 0x400C 002C |
| Description | Automatic Configuration This register configures automatic hardware updates to TXT and BUF. Configure this register to reduce software overhead during cipher modes. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||
| 31:29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 | |||||||||||||||||||||||
| 28 | CHBDNCLR | This field enable auto-clear of RIS.CHBDONE interrupt on read/write of TXT3/BUF3/TXTX3/TXTXBUF3 .
|
RW | 0 | |||||||||||||||||||||||
| 27 | CHADNCLR | This field enables auto-clear of RIS.CHADONE interrupt on read/write of TXT3/BUF3/TXTX3/TXTXBUF3 .
|
RW | 0 | |||||||||||||||||||||||
| 26 | CLRAESST | Clear AES Start This field enables auto-clear of RIS.AESSTART interrupt on read/write of TXT3/BUF3/TXTX3/TXTXBUF3 .
|
RW | 0 | |||||||||||||||||||||||
| 25 | CLRAESDN | Clear AES Done This field enables auto-clear of RIS.AESDONE interrupt on read/write of TXT3/BUF3/TXTX3/TXTXBUF3 .
|
RW | 0 | |||||||||||||||||||||||
| 24 | BUSHALT | Bus Halt This field decides if bus halts on access to KEY, TXT, BUF, TXTX and TXTXBUF when STA.STATE = BUSY.
|
RW | 0 | |||||||||||||||||||||||
| 23:22 | RESERVED22 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | |||||||||||||||||||||||
| 21:19 | CTRSIZE | Counter Size Configures size of counter as either 8,16,32,64 or 128 Non-enumerated values are not supported and ignored
|
RW | 0b000 | |||||||||||||||||||||||
| 18 | CTRALIGN | Counter Alignment Specifies alignment of counter
|
RW | 0 | |||||||||||||||||||||||
| 17 | CTRENDN | Counter Endianness Specifies Endianness of counter
|
RW | 0 | |||||||||||||||||||||||
| 16:10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | |||||||||||||||||||||||
| 9:8 | TRGTXT | Trigger for TXT This field determines if and when hardware automatically XORs BUF into TXT. Non-enumerated values are not supported and ignored. It is allowed to configure this field with an OR-combination of supported enums.
|
RW | 0b00 | |||||||||||||||||||||||
| 7:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | |||||||||||||||||||||||
| 5:4 | AESSRC | AES Source This field specifies the data source to hardware-triggered AES operations. Non-enumerated values are not supported and ignored.
|
RW | 0b00 | |||||||||||||||||||||||
| 3:0 | TRGAES | Trigger Electronic Codebook This field specifies one or more actions that indirectly trigger AES operation. It is allowed to configure this field with an OR-combination of supported enums.
|
RW | 0x0 | |||||||||||||||||||||||
| Address Offset | 0x0000 0050 | ||
| Physical Address | 0x400C 0050 | Instance | 0x400C 0050 |
| Description | Key Word 0 Write KEY0 through KEY3 to populate the 128-bit key. The key is not consumed by the hardware. It is hence not required to reload the key for subsequent block encryptions/decryptions unless required by the application. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of KEY[31:0] | WO | 0x0000 0000 | ||
| Address Offset | 0x0000 0054 | ||
| Physical Address | 0x400C 0054 | Instance | 0x400C 0054 |
| Description | Key Word 1 Write KEY0 through KEY3 to populate the 128-bit key. The key is not consumed by the hardware. It is hence not required to reload the key for subsequent block encryptions/decryptions unless required by the application. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of KEY[63:32] | WO | 0x0000 0000 | ||
| Address Offset | 0x0000 0058 | ||
| Physical Address | 0x400C 0058 | Instance | 0x400C 0058 |
| Description | Key Word 2 Write KEY0 through KEY3 to populate the 128-bit key. The key is not consumed by the hardware. It is hence not required to reload the key for subsequent block encryptions/decryptions unless required by the application. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of KEY[95:64] | WO | 0x0000 0000 | ||
| Address Offset | 0x0000 005C | ||
| Physical Address | 0x400C 005C | Instance | 0x400C 005C |
| Description | Key Word 3 Write KEY0 through KEY3 to populate the 128-bit key. The key is not consumed by the hardware. It is hence not required to reload the key for subsequent block encryptions/decryptions unless required by the application. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of KEY[127:96] | WO | 0x0000 0000 | ||
| Address Offset | 0x0000 0070 | ||
| Physical Address | 0x400C 0070 | Instance | 0x400C 0070 |
| Description | Text Word 0 TXT is the 128-bit buffer, the AES-128 algorithm performs its operations on. AES input can be written to TXT, and ciphertext can be read from TXT. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of TXT[31:0] | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0074 | ||
| Physical Address | 0x400C 0074 | Instance | 0x400C 0074 |
| Description | Text Word 1 TXT is the 128-bit buffer, the AES-128 algorithm performs its operations on. AES input can be written to TXT, and ciphertext can be read from TXT. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of TXT[63:32] | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0078 | ||
| Physical Address | 0x400C 0078 | Instance | 0x400C 0078 |
| Description | Text Word 2 TXT is the 128-bit buffer, the AES-128 algorithm performs its operations on. AES input can be written to TXT, and ciphertext can be read from TXT. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of TXT[95:64] | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 007C | ||
| Physical Address | 0x400C 007C | Instance | 0x400C 007C |
| Description | Text Word 3 TXT is the 128-bit buffer, the AES-128 algorithm performs its operations on. AES input can be written to TXT, and ciphertext can be read from TXT. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of TXT[127:96] AUTOCFG.TRGAES decides if a write to or a read of this field triggers an AES operation. |
RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0080 | ||
| Physical Address | 0x400C 0080 | Instance | 0x400C 0080 |
| Description | Text Word 0 XOR Write data to this register to XOR data with contents in TXT0.VAL. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value in TXT0 will be TXT0.VAL = VAL XOR TXT0.VAL | WO | 0x0000 0000 | ||
| Address Offset | 0x0000 0084 | ||
| Physical Address | 0x400C 0084 | Instance | 0x400C 0084 |
| Description | Text Word 1 XOR Write data to this register to XOR data with contents in TXT1.VAL. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value in TXT1 will be TXT1.VAL = VAL XOR TXT1.VAL | WO | 0x0000 0000 | ||
| Address Offset | 0x0000 0088 | ||
| Physical Address | 0x400C 0088 | Instance | 0x400C 0088 |
| Description | Text Word 2 XOR Write data to this register to XOR data with contents in TXT2.VAL. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value in TXT2 will be TXT2.VAL = VAL XOR TXT2.VAL | WO | 0x0000 0000 | ||
| Address Offset | 0x0000 008C | ||
| Physical Address | 0x400C 008C | Instance | 0x400C 008C |
| Description | Text Word 3 XOR Write data to this register to XOR data with contents in TXT3.VAL. AUTOCFG.TRGAES decides if a write to or a read of this field triggers an AES operation. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value in TXT3 will be TXT3.VAL = VAL XOR TXT3.VAL | WO | 0x0000 0000 | ||
| Address Offset | 0x0000 0090 | ||
| Physical Address | 0x400C 0090 | Instance | 0x400C 0090 |
| Description | Buffer Word 0 BUF is a 128-bit auxiliary register that functions as a buffer, counter, or storage of operations in cipher modes. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of BUF[31:0] | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0094 | ||
| Physical Address | 0x400C 0094 | Instance | 0x400C 0094 |
| Description | Buffer Word 1 BUF is a 128-bit auxiliary register that functions as a buffer, counter, or storage of operations in cipher modes. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of BUF[63:32] | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0098 | ||
| Physical Address | 0x400C 0098 | Instance | 0x400C 0098 |
| Description | Buffer Word 2 BUF is a 128-bit auxiliary register that functions as a buffer, counter, or storage of operations in cipher modes. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of BUF[95:64] | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 009C | ||
| Physical Address | 0x400C 009C | Instance | 0x400C 009C |
| Description | Buffer Word 3 BUF is a 128-bit auxiliary register that functions as a buffer, counter, or storage of operations in cipher modes. AUTOCFG.TRGAES decides if a write to this field triggers an AES operation. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value of BUF[127:96] | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 00A0 | ||
| Physical Address | 0x400C 00A0 | Instance | 0x400C 00A0 |
| Description | Text Word 0 XOR Buffer Word 0 Read this register to obtain plaintext during CFB decryption. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value read will be TXT0.VAL XOR BUF0.VAL | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 00A4 | ||
| Physical Address | 0x400C 00A4 | Instance | 0x400C 00A4 |
| Description | Text Word 1 XOR Buffer Word 1 Read this register to obtain plaintext during CFB decryption. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value read will be TXT1.VAL XOR BUF1.VAL | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 00A8 | ||
| Physical Address | 0x400C 00A8 | Instance | 0x400C 00A8 |
| Description | Text Word 2 XOR Buffer Word 2 Read this register to obtain plaintext during CFB decryption. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value read will be TXT2.VAL XOR BUF2.VAL | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 00AC | ||
| Physical Address | 0x400C 00AC | Instance | 0x400C 00AC |
| Description | Text Word 3 XOR Buffer Word3 Read this register to obtain plaintext during CFB decryption. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | VAL | Value read will be TXT3.VAL XOR BUF3.VAL | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 0104 | ||
| Physical Address | 0x400C 0104 | Instance | 0x400C 0104 |
| Description | Interrupt Mask register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||
| 3 | CHBDONE | DMA Channel B Done interrupt mask
|
RW | 0 | |||||||||||
| 2 | CHADONE | DMA Channel A Done interrupt mask
|
RW | 0 | |||||||||||
| 1 | AESSTART | AES Start interrupt mask
|
RW | 0 | |||||||||||
| 0 | AESDONE | AES Done interrupt mask
|
RW | 0 | |||||||||||
| Address Offset | 0x0000 0108 | ||
| Physical Address | 0x400C 0108 | Instance | 0x400C 0108 |
| Description | Raw Interrupt Status register | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||
| 3 | CHBDONE | Raw Interrupt Status for DMA Channel B Done
|
RO | 0 | |||||||||||
| 2 | CHADONE | Raw Interrupt Status for DMA Channel A Done
|
RO | 0 | |||||||||||
| 1 | AESSTART | Raw Interrupt Status for AES Start
|
RO | 0 | |||||||||||
| 0 | AESDONE | Raw Interrupt Status for AES Done
|
RO | 0 | |||||||||||
| Address Offset | 0x0000 010C | ||
| Physical Address | 0x400C 010C | Instance | 0x400C 010C |
| Description | Masked Interrupt Status register | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||
| 3 | CHBDONE | Masked Interrupt Status for DMA Channel B Done
|
RO | 0 | |||||||||||
| 2 | CHADONE | Masked Interrupt Status for DMA Channel A Done
|
RO | 0 | |||||||||||
| 1 | AESSTART | Masked Interrupt Status for AES Start
|
RO | 0 | |||||||||||
| 0 | AESDONE | Masked Interrupt Status for AES Done
|
RO | 0 | |||||||||||
| Address Offset | 0x0000 0110 | ||
| Physical Address | 0x400C 0110 | Instance | 0x400C 0110 |
| Description | Interrupt Set register | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||
| 3 | CHBDONE | Set DMA Channel B Done interrupt
|
WO | 0 | |||||||||||
| 2 | CHADONE | Set DMA Channel A Done interrupt
|
WO | 0 | |||||||||||
| 1 | AESSTART | Set AES Start interrupt
|
WO | 0 | |||||||||||
| 0 | AESDONE | Set AES Done interrupt
|
WO | 0 | |||||||||||
| Address Offset | 0x0000 0114 | ||
| Physical Address | 0x400C 0114 | Instance | 0x400C 0114 |
| Description | Interrupt Clear register | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||
| 3 | CHBDONE | Clear DMA Channel B Done interrupt
|
WO | 0 | |||||||||||
| 2 | CHADONE | Clear DMA Channel A Done interrupt
|
WO | 0 | |||||||||||
| 1 | AESSTART | Clear AES Start interrupt
|
WO | 0 | |||||||||||
| 0 | AESDONE | Clear AES Done interrupt
|
WO | 0 | |||||||||||
| Address Offset | 0x0000 0118 | ||
| Physical Address | 0x400C 0118 | Instance | 0x400C 0118 |
| Description | Interrupt Mask Set register | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||
| 3 | CHBDONE | Set DMA Channel B Done interrupt mask
|
WO | 0 | |||||||||||
| 2 | CHADONE | Set DMA Channel A Done interrupt mask
|
WO | 0 | |||||||||||
| 1 | AESSTART | Set AES Start interrupt mask
|
WO | 0 | |||||||||||
| 0 | AESDONE | Set AES Done interrupt mask
|
WO | 0 | |||||||||||
| Address Offset | 0x0000 011C | ||
| Physical Address | 0x400C 011C | Instance | 0x400C 011C |
| Description | Interrupt Mask Clear register | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||
| 3 | CHBDONE | Clear DMA Channel B Done interrupt mask
|
WO | 0 | |||||||||||
| 2 | CHADONE | Clear DMA Channel A Done interrupt mask
|
WO | 0 | |||||||||||
| 1 | AESSTART | Clear AES Start interrupt mask
|
WO | 0 | |||||||||||
| 0 | AESDONE | Clear AES Done interrupt mask
|
WO | 0 | |||||||||||
| © 2015 - 2016. Texas Instruments | All Rights Reserved |