![]() |
![]() |
|
CC27xxDriverLibrary
|
#include "uart.h"
Functions | |
| void | UARTConfigSetExpClk (uint32_t base, uint32_t UARTClkFreq, uint32_t baudFreq, uint32_t config) |
| Sets the configuration of a UART. More... | |
| void | UARTDisable (uint32_t base) |
| Disables transmitting and receiving. More... | |
| uint8_t | UARTGetChar (uint32_t base) |
| Waits for a character from the specified port. More... | |
| void | UARTPutChar (uint32_t base, uint8_t data) |
| Waits to send a character to the specified port. More... | |