CC27xxDriverLibrary
tz_context.h
Go to the documentation of this file.
1 /******************************************************************************
2  * @file tz_context.h
3  * @brief Context Management for Armv8-M TrustZone
4  * @version V1.0.1
5  * @date 10. January 2018
6  ******************************************************************************/
7 /*
8  * Copyright (c) 2017-2018 Arm Limited. All rights reserved.
9  *
10  * SPDX-License-Identifier: Apache-2.0
11  *
12  * Licensed under the Apache License, Version 2.0 (the License); you may
13  * not use this file except in compliance with the License.
14  * You may obtain a copy of the License at
15  *
16  * www.apache.org/licenses/LICENSE-2.0
17  *
18  * Unless required by applicable law or agreed to in writing, software
19  * distributed under the License is distributed on an AS IS BASIS, WITHOUT
20  * WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
21  * See the License for the specific language governing permissions and
22  * limitations under the License.
23  */
24 
25 #if defined ( __ICCARM__ )
26  #pragma system_include /* treat file as system include file for MISRA check */
27 #elif defined (__clang__)
28  #pragma clang system_header /* treat file as system include file */
29 #endif
30 
31 #ifndef TZ_CONTEXT_H
32 #define TZ_CONTEXT_H
33 
34 #include <stdint.h>
35 
36 #ifndef TZ_MODULEID_T
37 #define TZ_MODULEID_T
38 typedef uint32_t TZ_ModuleId_t;
40 #endif
41 
43 typedef uint32_t TZ_MemoryId_t;
44 
47 uint32_t TZ_InitContextSystem_S (void);
48 
54 
59 
63 uint32_t TZ_LoadContext_S (TZ_MemoryId_t id);
64 
68 uint32_t TZ_StoreContext_S (TZ_MemoryId_t id);
69 
70 #endif // TZ_CONTEXT_H
uint32_t TZ_LoadContext_S(TZ_MemoryId_t id)
uint32_t TZ_MemoryId_t
Definition: tz_context.h:43
uint32_t TZ_InitContextSystem_S(void)
uint32_t TZ_FreeModuleContext_S(TZ_MemoryId_t id)
TZ_MemoryId_t TZ_AllocModuleContext_S(TZ_ModuleId_t module)
uint32_t TZ_StoreContext_S(TZ_MemoryId_t id)
uint32_t TZ_ModuleId_t
Definition: tz_context.h:39