CC27xxDriverLibrary
sw_ecrypt-sync.h
Go to the documentation of this file.
1 /******************************************************************************
2  * Filename: sw_ecrypt-sync.h
3  ******************************************************************************/
4 /* ecrypt-sync.h */
5 
6 /*
7  * Header file for synchronous stream ciphers without authentication
8  * mechanism.
9  *
10  * *** Please only edit parts marked with "[edit]". ***
11  */
12 
13 #ifndef ECRYPT_SYNC
14 #define ECRYPT_SYNC
15 
16 #include "sw_ecrypt-portable.h"
17 
18 /* ------------------------------------------------------------------------- */
19 
20 /* Cipher parameters */
21 
22 /*
23  * The name of your cipher.
24  */
25 #define ECRYPT_NAME "ChaCha8"
26 #define ECRYPT_PROFILE "_____"
27 
28 /*
29  * Specify which key and IV sizes are supported by your cipher. A user
30  * should be able to enumerate the supported sizes by running the
31  * following code:
32  *
33  * for (i = 0; ECRYPT_KEYSIZE(i) <= ECRYPT_MAXKEYSIZE; ++i)
34  * {
35  * keysize = ECRYPT_KEYSIZE(i);
36  *
37  * ...
38  * }
39  *
40  * All sizes are in bits.
41  */
42 
43 #define ECRYPT_MAXKEYSIZE 256 /* [edit] */
44 #define ECRYPT_KEYSIZE(i) (128 + (i)*128) /* [edit] */
45 
46 #define ECRYPT_MAXIVSIZE 64 /* [edit] */
47 #define ECRYPT_IVSIZE(i) (64 + (i)*64) /* [edit] */
48 
49 /* ------------------------------------------------------------------------- */
50 
51 /* Data structures */
52 
53 /*
54  * ECRYPT_ctx is the structure containing the representation of the
55  * internal state of your cipher.
56  */
57 
58 typedef struct
59 {
60  u32 input[16]; /* could be compressed */
61  /*
62  * [edit]
63  *
64  * Put here all state variable needed during the encryption process.
65  */
66 } ECRYPT_ctx;
67 
68 /* ------------------------------------------------------------------------- */
69 
70 /* Mandatory functions */
71 
72 /*
73  * Key and message independent initialization. This function will be
74  * called once when the program starts (e.g., to build expanded S-box
75  * tables).
76  */
77 void ECRYPT_init(void);
78 
79 /*
80  * Key setup. It is the user's responsibility to select the values of
81  * keysize and ivsize from the set of supported values specified
82  * above.
83  */
84 void ECRYPT_keysetup(ECRYPT_ctx *ctx,
85  const u8 *key,
86  u32 keysize, /* Key size in bits. */
87  u32 ivsize); /* IV size in bits. */
88 
89 /*
90  * IV setup. After having called ECRYPT_keysetup(), the user is
91  * allowed to call ECRYPT_ivsetup() different times in order to
92  * encrypt/decrypt different messages with the same key but different
93  * IV's.
94  */
95 void ECRYPT_ivsetup(ECRYPT_ctx *ctx, const u8 *iv);
96 
97 /*
98  * Encryption/decryption of arbitrary length messages.
99  *
100  * For efficiency reasons, the API provides two types of
101  * encrypt/decrypt functions. The ECRYPT_encrypt_bytes() function
102  * (declared here) encrypts byte strings of arbitrary length, while
103  * the ECRYPT_encrypt_blocks() function (defined later) only accepts
104  * lengths which are multiples of ECRYPT_BLOCKLENGTH.
105  *
106  * The user is allowed to make multiple calls to
107  * ECRYPT_encrypt_blocks() to incrementally encrypt a long message,
108  * but he is NOT allowed to make additional encryption calls once he
109  * has called ECRYPT_encrypt_bytes() (unless he starts a new message
110  * of course). For example, this sequence of calls is acceptable:
111  *
112  * ECRYPT_keysetup();
113  *
114  * ECRYPT_ivsetup();
115  * ECRYPT_encrypt_blocks();
116  * ECRYPT_encrypt_blocks();
117  * ECRYPT_encrypt_bytes();
118  *
119  * ECRYPT_ivsetup();
120  * ECRYPT_encrypt_blocks();
121  * ECRYPT_encrypt_blocks();
122  *
123  * ECRYPT_ivsetup();
124  * ECRYPT_encrypt_bytes();
125  *
126  * The following sequence is not:
127  *
128  * ECRYPT_keysetup();
129  * ECRYPT_ivsetup();
130  * ECRYPT_encrypt_blocks();
131  * ECRYPT_encrypt_bytes();
132  * ECRYPT_encrypt_blocks();
133  */
134 
135 void ECRYPT_encrypt_bytes(ECRYPT_ctx *ctx, const u8 *plaintext, u8 *ciphertext, u32 msglen); /* Message length in bytes.
136  */
137 
138 void ECRYPT_decrypt_bytes(ECRYPT_ctx *ctx, const u8 *ciphertext, u8 *plaintext, u32 msglen); /* Message length in bytes.
139  */
140 
141 /* ------------------------------------------------------------------------- */
142 
143 /* Optional features */
144 
145 /*
146  * For testing purposes it can sometimes be useful to have a function
147  * which immediately generates keystream without having to provide it
148  * with a zero plaintext. If your cipher cannot provide this function
149  * (e.g., because it is not strictly a synchronous cipher), please
150  * reset the ECRYPT_GENERATES_KEYSTREAM flag.
151  */
152 
153 #define ECRYPT_GENERATES_KEYSTREAM
154 #ifdef ECRYPT_GENERATES_KEYSTREAM
155 
156 void ECRYPT_keystream_bytes(ECRYPT_ctx *ctx, u8 *keystream, u32 length); /* Length of keystream in bytes. */
157 
158 #endif
159 
160 /* ------------------------------------------------------------------------- */
161 
162 /* Optional optimizations */
163 
164 /*
165  * By default, the functions in this section are implemented using
166  * calls to functions declared above. However, you might want to
167  * implement them differently for performance reasons.
168  */
169 
170 /*
171  * All-in-one encryption/decryption of (short) packets.
172  *
173  * The default definitions of these functions can be found in
174  * "ecrypt-sync.c". If you want to implement them differently, please
175  * undef the ECRYPT_USES_DEFAULT_ALL_IN_ONE flag.
176  */
177 #define ECRYPT_USES_DEFAULT_ALL_IN_ONE /* [edit] */
178 
179 void ECRYPT_encrypt_packet(ECRYPT_ctx *ctx, const u8 *iv, const u8 *plaintext, u8 *ciphertext, u32 msglen);
180 
181 void ECRYPT_decrypt_packet(ECRYPT_ctx *ctx, const u8 *iv, const u8 *ciphertext, u8 *plaintext, u32 msglen);
182 
183 /*
184  * Encryption/decryption of blocks.
185  *
186  * By default, these functions are defined as macros. If you want to
187  * provide a different implementation, please undef the
188  * ECRYPT_USES_DEFAULT_BLOCK_MACROS flag and implement the functions
189  * declared below.
190  */
191 
192 #define ECRYPT_BLOCKLENGTH 64 /* [edit] */
193 
194 #define ECRYPT_USES_DEFAULT_BLOCK_MACROS /* [edit] */
195 #ifdef ECRYPT_USES_DEFAULT_BLOCK_MACROS
196 
197  #define ECRYPT_encrypt_blocks(ctx, plaintext, ciphertext, blocks) \
198  ECRYPT_encrypt_bytes(ctx, plaintext, ciphertext, (blocks)*ECRYPT_BLOCKLENGTH)
199 
200  #define ECRYPT_decrypt_blocks(ctx, ciphertext, plaintext, blocks) \
201  ECRYPT_decrypt_bytes(ctx, ciphertext, plaintext, (blocks)*ECRYPT_BLOCKLENGTH)
202 
203  #ifdef ECRYPT_GENERATES_KEYSTREAM
204 
205  #define ECRYPT_keystream_blocks(ctx, keystream, blocks) \
206  ECRYPT_keystream_bytes(ctx, keystream, (blocks)*ECRYPT_BLOCKLENGTH)
207 
208  #endif
209 
210 #else
211 
212 void ECRYPT_encrypt_blocks(ECRYPT_ctx *ctx, const u8 *plaintext, u8 *ciphertext, u32 blocks); /* Message length in
213  blocks. */
214 
215 void ECRYPT_decrypt_blocks(ECRYPT_ctx *ctx, const u8 *ciphertext, u8 *plaintext, u32 blocks); /* Message length in
216  blocks. */
217 
218  #ifdef ECRYPT_GENERATES_KEYSTREAM
219 
220 void ECRYPT_keystream_blocks(ECRYPT_ctx *ctx, const u8 *keystream, u32 blocks); /* Keystream length in blocks. */
221 
222  #endif
223 
224 #endif
225 
226 /*
227  * If your cipher can be implemented in different ways, you can use
228  * the ECRYPT_VARIANT parameter to allow the user to choose between
229  * them at compile time (e.g., gcc -DECRYPT_VARIANT=3 ...). Please
230  * only use this possibility if you really think it could make a
231  * significant difference and keep the number of variants
232  * (ECRYPT_MAXVARIANT) as small as possible (definitely not more than
233  * 10). Note also that all variants should have exactly the same
234  * external interface (i.e., the same ECRYPT_BLOCKLENGTH, etc.).
235  */
236 #define ECRYPT_MAXVARIANT 1 /* [edit] */
237 
238 #ifndef ECRYPT_VARIANT
239  #define ECRYPT_VARIANT 1
240 #endif
241 
242 #if (ECRYPT_VARIANT > ECRYPT_MAXVARIANT)
243  #error this variant does not exist
244 #endif
245 
246 /* ------------------------------------------------------------------------- */
247 
248 #endif
void ECRYPT_keystream_bytes(ECRYPT_ctx *ctx, u8 *keystream, u32 length)
Definition: sw_chacha.c:143
void ECRYPT_decrypt_packet(ECRYPT_ctx *ctx, const u8 *iv, const u8 *ciphertext, u8 *plaintext, u32 msglen)
void ECRYPT_init(void)
Definition: sw_chacha.c:59
void ECRYPT_encrypt_bytes(ECRYPT_ctx *ctx, const u8 *plaintext, u8 *ciphertext, u32 msglen)
Definition: sw_chacha.c:102
void ECRYPT_ivsetup(ECRYPT_ctx *ctx, const u8 *iv)
Definition: sw_chacha.c:94
void ECRYPT_encrypt_packet(ECRYPT_ctx *ctx, const u8 *iv, const u8 *plaintext, u8 *ciphertext, u32 msglen)
void ECRYPT_keysetup(ECRYPT_ctx *ctx, const u8 *key, u32 keysize, u32 ivsize)
Definition: sw_chacha.c:67
#define ECRYPT_keystream_blocks(ctx, keystream, blocks)
Definition: sw_ecrypt-sync.h:205
#define ECRYPT_decrypt_blocks(ctx, ciphertext, plaintext, blocks)
Definition: sw_ecrypt-sync.h:200
Definition: sw_ecrypt-sync.h:58
void ECRYPT_decrypt_bytes(ECRYPT_ctx *ctx, const u8 *ciphertext, u8 *plaintext, u32 msglen)
Definition: sw_chacha.c:138
#define ECRYPT_encrypt_blocks(ctx, plaintext, ciphertext, blocks)
Definition: sw_ecrypt-sync.h:197