|
| static void | SPIConfig (uint32_t baseAddr, uint32_t freq, uint32_t format, uint32_t mode, uint32_t bitRate, uint32_t dataSize, uint32_t dsample) |
| |
| void | SPIConfigSetExpClk (uint32_t base, uint32_t spiClk, uint32_t protocol, uint32_t mode, uint32_t bitRate, uint32_t dataWidth) |
| | Configures the serial peripheral port. More...
|
| |
| int32_t | SPIPutDataNonBlocking (uint32_t base, uint32_t data) |
| | Puts a data element into the SPI transmit FIFO. More...
|
| |
| void | SPIPutData (uint32_t base, uint32_t data) |
| | Puts a data element into the SPI transmit FIFO. More...
|
| |
| void | SPIGetData (uint32_t base, uint32_t *data) |
| | Gets a data element from the SPI receive FIFO. More...
|
| |
| int32_t | SPIGetDataNonBlocking (uint32_t base, uint32_t *data) |
| | Gets a data element from the SPI receive FIFO. More...
|
| |
| void | SPIRegisterInt (uint32_t base, void(*pfnHandler)(void)) |
| | Registers an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
|
| |
| void | SPIUnregisterInt (uint32_t base) |
| | Unregisters an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
|
| |