CC27xxDriverLibrary
pmu_armv8.h
Go to the documentation of this file.
1 /******************************************************************************
2  * @file pmu_armv8.h
3  * @brief CMSIS PMU API for Armv8.1-M PMU
4  * @version V1.0.1
5  * @date 15. April 2020
6  ******************************************************************************/
7 /*
8  * Copyright (c) 2020 Arm Limited. All rights reserved.
9  *
10  * SPDX-License-Identifier: Apache-2.0
11  *
12  * Licensed under the Apache License, Version 2.0 (the License); you may
13  * not use this file except in compliance with the License.
14  * You may obtain a copy of the License at
15  *
16  * www.apache.org/licenses/LICENSE-2.0
17  *
18  * Unless required by applicable law or agreed to in writing, software
19  * distributed under the License is distributed on an AS IS BASIS, WITHOUT
20  * WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
21  * See the License for the specific language governing permissions and
22  * limitations under the License.
23  */
24 
25 #if defined ( __ICCARM__ )
26  #pragma system_include /* treat file as system include file for MISRA check */
27 #elif defined (__clang__)
28  #pragma clang system_header /* treat file as system include file */
29 #endif
30 
31 #ifndef ARM_PMU_ARMV8_H
32 #define ARM_PMU_ARMV8_H
33 
39 #define ARM_PMU_SW_INCR 0x0000
40 #define ARM_PMU_L1I_CACHE_REFILL 0x0001
41 #define ARM_PMU_L1D_CACHE_REFILL 0x0003
42 #define ARM_PMU_L1D_CACHE 0x0004
43 #define ARM_PMU_LD_RETIRED 0x0006
44 #define ARM_PMU_ST_RETIRED 0x0007
45 #define ARM_PMU_INST_RETIRED 0x0008
46 #define ARM_PMU_EXC_TAKEN 0x0009
47 #define ARM_PMU_EXC_RETURN 0x000A
48 #define ARM_PMU_PC_WRITE_RETIRED 0x000C
49 #define ARM_PMU_BR_IMMED_RETIRED 0x000D
50 #define ARM_PMU_BR_RETURN_RETIRED 0x000E
51 #define ARM_PMU_UNALIGNED_LDST_RETIRED 0x000F
52 #define ARM_PMU_BR_MIS_PRED 0x0010
53 #define ARM_PMU_CPU_CYCLES 0x0011
54 #define ARM_PMU_BR_PRED 0x0012
55 #define ARM_PMU_MEM_ACCESS 0x0013
56 #define ARM_PMU_L1I_CACHE 0x0014
57 #define ARM_PMU_L1D_CACHE_WB 0x0015
58 #define ARM_PMU_L2D_CACHE 0x0016
59 #define ARM_PMU_L2D_CACHE_REFILL 0x0017
60 #define ARM_PMU_L2D_CACHE_WB 0x0018
61 #define ARM_PMU_BUS_ACCESS 0x0019
62 #define ARM_PMU_MEMORY_ERROR 0x001A
63 #define ARM_PMU_INST_SPEC 0x001B
64 #define ARM_PMU_BUS_CYCLES 0x001D
65 #define ARM_PMU_CHAIN 0x001E
66 #define ARM_PMU_L1D_CACHE_ALLOCATE 0x001F
67 #define ARM_PMU_L2D_CACHE_ALLOCATE 0x0020
68 #define ARM_PMU_BR_RETIRED 0x0021
69 #define ARM_PMU_BR_MIS_PRED_RETIRED 0x0022
70 #define ARM_PMU_STALL_FRONTEND 0x0023
71 #define ARM_PMU_STALL_BACKEND 0x0024
72 #define ARM_PMU_L2I_CACHE 0x0027
73 #define ARM_PMU_L2I_CACHE_REFILL 0x0028
74 #define ARM_PMU_L3D_CACHE_ALLOCATE 0x0029
75 #define ARM_PMU_L3D_CACHE_REFILL 0x002A
76 #define ARM_PMU_L3D_CACHE 0x002B
77 #define ARM_PMU_L3D_CACHE_WB 0x002C
78 #define ARM_PMU_LL_CACHE_RD 0x0036
79 #define ARM_PMU_LL_CACHE_MISS_RD 0x0037
80 #define ARM_PMU_L1D_CACHE_MISS_RD 0x0039
81 #define ARM_PMU_OP_COMPLETE 0x003A
82 #define ARM_PMU_OP_SPEC 0x003B
83 #define ARM_PMU_STALL 0x003C
84 #define ARM_PMU_STALL_OP_BACKEND 0x003D
85 #define ARM_PMU_STALL_OP_FRONTEND 0x003E
86 #define ARM_PMU_STALL_OP 0x003F
87 #define ARM_PMU_L1D_CACHE_RD 0x0040
88 #define ARM_PMU_LE_RETIRED 0x0100
89 #define ARM_PMU_LE_SPEC 0x0101
90 #define ARM_PMU_BF_RETIRED 0x0104
91 #define ARM_PMU_BF_SPEC 0x0105
92 #define ARM_PMU_LE_CANCEL 0x0108
93 #define ARM_PMU_BF_CANCEL 0x0109
94 #define ARM_PMU_SE_CALL_S 0x0114
95 #define ARM_PMU_SE_CALL_NS 0x0115
96 #define ARM_PMU_DWT_CMPMATCH0 0x0118
97 #define ARM_PMU_DWT_CMPMATCH1 0x0119
98 #define ARM_PMU_DWT_CMPMATCH2 0x011A
99 #define ARM_PMU_DWT_CMPMATCH3 0x011B
100 #define ARM_PMU_MVE_INST_RETIRED 0x0200
101 #define ARM_PMU_MVE_INST_SPEC 0x0201
102 #define ARM_PMU_MVE_FP_RETIRED 0x0204
103 #define ARM_PMU_MVE_FP_SPEC 0x0205
104 #define ARM_PMU_MVE_FP_HP_RETIRED 0x0208
105 #define ARM_PMU_MVE_FP_HP_SPEC 0x0209
106 #define ARM_PMU_MVE_FP_SP_RETIRED 0x020C
107 #define ARM_PMU_MVE_FP_SP_SPEC 0x020D
108 #define ARM_PMU_MVE_FP_MAC_RETIRED 0x0214
109 #define ARM_PMU_MVE_FP_MAC_SPEC 0x0215
110 #define ARM_PMU_MVE_INT_RETIRED 0x0224
111 #define ARM_PMU_MVE_INT_SPEC 0x0225
112 #define ARM_PMU_MVE_INT_MAC_RETIRED 0x0228
113 #define ARM_PMU_MVE_INT_MAC_SPEC 0x0229
114 #define ARM_PMU_MVE_LDST_RETIRED 0x0238
115 #define ARM_PMU_MVE_LDST_SPEC 0x0239
116 #define ARM_PMU_MVE_LD_RETIRED 0x023C
117 #define ARM_PMU_MVE_LD_SPEC 0x023D
118 #define ARM_PMU_MVE_ST_RETIRED 0x0240
119 #define ARM_PMU_MVE_ST_SPEC 0x0241
120 #define ARM_PMU_MVE_LDST_CONTIG_RETIRED 0x0244
121 #define ARM_PMU_MVE_LDST_CONTIG_SPEC 0x0245
122 #define ARM_PMU_MVE_LD_CONTIG_RETIRED 0x0248
123 #define ARM_PMU_MVE_LD_CONTIG_SPEC 0x0249
124 #define ARM_PMU_MVE_ST_CONTIG_RETIRED 0x024C
125 #define ARM_PMU_MVE_ST_CONTIG_SPEC 0x024D
126 #define ARM_PMU_MVE_LDST_NONCONTIG_RETIRED 0x0250
127 #define ARM_PMU_MVE_LDST_NONCONTIG_SPEC 0x0251
128 #define ARM_PMU_MVE_LD_NONCONTIG_RETIRED 0x0254
129 #define ARM_PMU_MVE_LD_NONCONTIG_SPEC 0x0255
130 #define ARM_PMU_MVE_ST_NONCONTIG_RETIRED 0x0258
131 #define ARM_PMU_MVE_ST_NONCONTIG_SPEC 0x0259
132 #define ARM_PMU_MVE_LDST_MULTI_RETIRED 0x025C
133 #define ARM_PMU_MVE_LDST_MULTI_SPEC 0x025D
134 #define ARM_PMU_MVE_LD_MULTI_RETIRED 0x0260
135 #define ARM_PMU_MVE_LD_MULTI_SPEC 0x0261
136 #define ARM_PMU_MVE_ST_MULTI_RETIRED 0x0261
137 #define ARM_PMU_MVE_ST_MULTI_SPEC 0x0265
138 #define ARM_PMU_MVE_LDST_UNALIGNED_RETIRED 0x028C
139 #define ARM_PMU_MVE_LDST_UNALIGNED_SPEC 0x028D
140 #define ARM_PMU_MVE_LD_UNALIGNED_RETIRED 0x0290
141 #define ARM_PMU_MVE_LD_UNALIGNED_SPEC 0x0291
142 #define ARM_PMU_MVE_ST_UNALIGNED_RETIRED 0x0294
143 #define ARM_PMU_MVE_ST_UNALIGNED_SPEC 0x0295
144 #define ARM_PMU_MVE_LDST_UNALIGNED_NONCONTIG_RETIRED 0x0298
145 #define ARM_PMU_MVE_LDST_UNALIGNED_NONCONTIG_SPEC 0x0299
146 #define ARM_PMU_MVE_VREDUCE_RETIRED 0x02A0
147 #define ARM_PMU_MVE_VREDUCE_SPEC 0x02A1
148 #define ARM_PMU_MVE_VREDUCE_FP_RETIRED 0x02A4
149 #define ARM_PMU_MVE_VREDUCE_FP_SPEC 0x02A5
150 #define ARM_PMU_MVE_VREDUCE_INT_RETIRED 0x02A8
151 #define ARM_PMU_MVE_VREDUCE_INT_SPEC 0x02A9
152 #define ARM_PMU_MVE_PRED 0x02B8
153 #define ARM_PMU_MVE_STALL 0x02CC
154 #define ARM_PMU_MVE_STALL_RESOURCE 0x02CD
155 #define ARM_PMU_MVE_STALL_RESOURCE_MEM 0x02CE
156 #define ARM_PMU_MVE_STALL_RESOURCE_FP 0x02CF
157 #define ARM_PMU_MVE_STALL_RESOURCE_INT 0x02D0
158 #define ARM_PMU_MVE_STALL_BREAK 0x02D3
159 #define ARM_PMU_MVE_STALL_DEPENDENCY 0x02D4
160 #define ARM_PMU_ITCM_ACCESS 0x4007
161 #define ARM_PMU_DTCM_ACCESS 0x4008
162 #define ARM_PMU_TRCEXTOUT0 0x4010
163 #define ARM_PMU_TRCEXTOUT1 0x4011
164 #define ARM_PMU_TRCEXTOUT2 0x4012
165 #define ARM_PMU_TRCEXTOUT3 0x4013
166 #define ARM_PMU_CTI_TRIGOUT4 0x4018
167 #define ARM_PMU_CTI_TRIGOUT5 0x4019
168 #define ARM_PMU_CTI_TRIGOUT6 0x401A
169 #define ARM_PMU_CTI_TRIGOUT7 0x401B
173 __STATIC_INLINE void ARM_PMU_Enable(void);
175 
176 __STATIC_INLINE void ARM_PMU_Set_EVTYPER(uint32_t num, uint32_t type);
177 
180 
181 __STATIC_INLINE void ARM_PMU_CNTR_Enable(uint32_t mask);
182 __STATIC_INLINE void ARM_PMU_CNTR_Disable(uint32_t mask);
183 
184 __STATIC_INLINE uint32_t ARM_PMU_Get_CCNTR(void);
185 __STATIC_INLINE uint32_t ARM_PMU_Get_EVCNTR(uint32_t num);
186 
188 __STATIC_INLINE void ARM_PMU_Set_CNTR_OVS(uint32_t mask);
189 
190 __STATIC_INLINE void ARM_PMU_Set_CNTR_IRQ_Enable(uint32_t mask);
192 
193 __STATIC_INLINE void ARM_PMU_CNTR_Increment(uint32_t mask);
194 
199 {
200  PMU->CTRL |= PMU_CTRL_ENABLE_Msk;
201 }
202 
207 {
208  PMU->CTRL &= ~PMU_CTRL_ENABLE_Msk;
209 }
210 
216 __STATIC_INLINE void ARM_PMU_Set_EVTYPER(uint32_t num, uint32_t type)
217 {
218  PMU->EVTYPER[num] = type;
219 }
220 
225 {
226  PMU->CTRL |= PMU_CTRL_CYCCNT_RESET_Msk;
227 }
228 
233 {
234  PMU->CTRL |= PMU_CTRL_EVENTCNT_RESET_Msk;
235 }
236 
245 {
246  PMU->CNTENSET = mask;
247 }
248 
257 {
258  PMU->CNTENCLR = mask;
259 }
260 
266 {
267  return PMU->CCNTR;
268 }
269 
275 __STATIC_INLINE uint32_t ARM_PMU_Get_EVCNTR(uint32_t num)
276 {
277  return PMU_EVCNTR_CNT_Msk & PMU->EVCNTR[num];
278 }
279 
287 {
288  return PMU->OVSSET;
289 }
290 
299 {
300  PMU->OVSCLR = mask;
301 }
302 
311 {
312  PMU->INTENSET = mask;
313 }
314 
323 {
324  PMU->INTENCLR = mask;
325 }
326 
333 {
334  PMU->SWINC = mask;
335 }
336 
337 #endif
__STATIC_INLINE void ARM_PMU_Enable(void)
PMU Functions.
Definition: pmu_armv8.h:198
__STATIC_INLINE void ARM_PMU_CNTR_Increment(uint32_t mask)
Software increment event counter.
Definition: pmu_armv8.h:332
__STATIC_INLINE uint32_t ARM_PMU_Get_CNTR_OVS(void)
Read counter overflow status.
Definition: pmu_armv8.h:286
__STATIC_INLINE void ARM_PMU_CYCCNT_Reset(void)
Reset cycle counter.
Definition: pmu_armv8.h:224
__STATIC_INLINE void ARM_PMU_EVCNTR_ALL_Reset(void)
Reset all event counters.
Definition: pmu_armv8.h:232
__STATIC_INLINE void ARM_PMU_Set_CNTR_IRQ_Enable(uint32_t mask)
Enable counter overflow interrupt request.
Definition: pmu_armv8.h:310
__STATIC_INLINE void ARM_PMU_CNTR_Enable(uint32_t mask)
Enable counters.
Definition: pmu_armv8.h:244
__STATIC_INLINE uint32_t ARM_PMU_Get_EVCNTR(uint32_t num)
Read event counter.
Definition: pmu_armv8.h:275
__STATIC_INLINE void ARM_PMU_Set_EVTYPER(uint32_t num, uint32_t type)
Set event to count for PMU eventer counter.
Definition: pmu_armv8.h:216
__STATIC_INLINE void ARM_PMU_Set_CNTR_IRQ_Disable(uint32_t mask)
Disable counter overflow interrupt request.
Definition: pmu_armv8.h:322
__STATIC_INLINE void ARM_PMU_CNTR_Disable(uint32_t mask)
Disable counters.
Definition: pmu_armv8.h:256
__STATIC_INLINE void ARM_PMU_Set_CNTR_OVS(uint32_t mask)
Clear counter overflow status.
Definition: pmu_armv8.h:298
__STATIC_INLINE uint32_t ARM_PMU_Get_CCNTR(void)
Read cycle counter.
Definition: pmu_armv8.h:265
__STATIC_INLINE void ARM_PMU_Disable(void)
Disable the PMU.
Definition: pmu_armv8.h:206
#define __STATIC_INLINE
Definition: cmsis_gcc.h:47