CC27xxDriverLibrary
lrfd.c File Reference
#include "lrfd.h"
#include <stdbool.h>
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_clkctl.h"
#include "../inc/hw_lrfddbell.h"
#include "../driverlib/interrupt.h"
#include "../driverlib/clkctl.h"
Include dependency graph for lrfd.c:

Enumerations

enum  { LRFD_NOT_CLOCKED = 0, LRFD_CLOCKED = 1, LRFD_UNKNOWN_CLOCK_STATUS = 2 }
 

Functions

void LRFDSetDependencySetsPtr (uint16_t(*dependencySetsPtr)[LRFD_NUM_CLK_DEP])
 
void LRFDSetClockDependency (uint16_t mask, uint8_t dependencySetId)
 Set clock dependency on a set of modules in LRFD. More...
 
void LRFDReleaseClockDependency (uint16_t mask, uint8_t dependencySetId)
 Release clock dependency on a set of modules in LRFD. More...
 
void LRFDApplyClockDependencies (void)
 Apply the currently set clock dependencies. More...
 

Variables

static enum { ... }  lrfdClockStatus = LRFD_UNKNOWN_CLOCK_STATUS
 
static uint16_t lrfdClockDependencySets [LRFD_NUM_CLK_DEP]
 
static uint16_t(* lrfdClockDependencySetsPtr )[LRFD_NUM_CLK_DEP] = &lrfdClockDependencySets
 

Enumeration Type Documentation

§ anonymous enum

anonymous enum
Enumerator
LRFD_NOT_CLOCKED 
LRFD_CLOCKED 
LRFD_UNKNOWN_CLOCK_STATUS 

Function Documentation

§ LRFDSetDependencySetsPtr()

void LRFDSetDependencySetsPtr ( uint16_t(*)  dependencySetsPtr[LRFD_NUM_CLK_DEP])

Variable Documentation

§ lrfdClockStatus

enum { ... } lrfdClockStatus

§ lrfdClockDependencySets

uint16_t lrfdClockDependencySets[LRFD_NUM_CLK_DEP]
static

§ lrfdClockDependencySetsPtr

uint16_t(* lrfdClockDependencySetsPtr)[LRFD_NUM_CLK_DEP] = &lrfdClockDependencySets
static