CC27xxDriverLibrary
[sha256sw.h] SHA2 256/224 SW APIs

SHA2 256/224 SW APIs. More...

Collaboration diagram for [sha256sw.h] SHA2 256/224 SW APIs:

Data Structures

struct  SHA256SW_Object
 SHA256SW Object. More...
 

Macros

#define SHA256SWHashData   HAPI_TABLE_POINTER->sha256SwHashData
 
#define SHA256SWStart   HAPI_TABLE_POINTER->sha256SwStart
 
#define SHA256SWAddData   HAPI_TABLE_POINTER->sha256SwAddData
 
#define SHA256SWFinalize   HAPI_TABLE_POINTER->sha256SwFinalize
 

Typedefs

typedef SHA256SW_ObjectSHA256SW_Handle
 A handle to a SHA256SW_Object. More...
 

Functions

int_fast16_t SHA256SWHashData (SHA256SW_Handle handle, SHA2SW_HashType hashType, const void *data, size_t length, uint32_t digest[8])
 Performs a complete hash operation, producing a final digest for the data. More...
 
int_fast16_t SHA256SWStart (SHA256SW_Handle handle, SHA2SW_HashType hashType)
 Initialize a SHA256SW_Handle, preparing for hashing data. More...
 
int_fast16_t SHA256SWAddData (SHA256SW_Handle handle, const void *data, size_t length)
 Add data to a SHA256/224 operation. More...
 
int_fast16_t SHA256SWFinalize (SHA256SW_Handle handle, uint32_t digest[8])
 Finalize a SHA256/224 operation, creating the final digest. More...
 

Detailed Description

SHA2 256/224 SW APIs.

Overview

Provides top-level general purpose SHA2 256/224 APIs. SHA2 algorithm is implemented in SW with no HW acceleration. The implementation is highly optimized for speed and code size. These functions reside in ROM, and are exposed through HAPI, and also through the function prototypes and macros below.

Availability of SHA2 224 depends on build configuration. See file sha2sw_config.h.

Limitations


Usage

There are two general ways to execute a SHA2 operation:

The multi-step approach allows the hash to be extended by adding more data.

All input data is to be in little-endian (LE) format and the resulting hash values produced by these APIs are in LE format.

Synopsis

The following is a quick overview of one-step hashing.

// Import SHA2 SW Driver definitions
#include <sha256sw.h>
// Create an object and handle
SHA256SW_Object sha256SWObject;
SHA256SW_Handle sha256SWHandle = &sha256SWObject;
// Allocate space for digest output
uint32_t actualDigest[8];
result = SHA256SWHashData(sha256SWHandle, SHA2SW_HASH_TYPE_256,
message, strlen(message), actualDigest);

Examples

Hashing data in one call

SHA256SW_Object sha256SWObject;
SHA256SW_Handle sha256SWHandle = &sha256SWObject;
int_fast16_t sha2SWresult;
uint32_t finalDigest[8];
int notsame;
char message[] =
"abcdefghijklmnabcdefghijklmnabcdefghijklmnabcdefghijklmn1234";
uint8_t expectedDigest[] =
{ 0x60, 0x06, 0x00, 0x24, 0x13, 0xe4, 0x27, 0x0d,
0x4d, 0xdb, 0x66, 0x93, 0x42, 0xa9, 0xe2, 0xdb,
0x66, 0x5e, 0xc8, 0x70, 0x73, 0xc4, 0x2e, 0xb5,
0x44, 0x99, 0x62, 0xf1, 0x2a, 0xb2, 0xe8, 0x60 };
sha2SWresult = SHA256SWHashData(sha256SWHandle, SHA2SW_HASH_TYPE_256,
message, strlen(message), finalDigest);
if (sha2SWresult != SHA2SW_STATUS_SUCCESS)
{
while(1);
}
// NOTE: If expectedDigest is a secret value, a timing constant comparison
// routine shall be used instead of memcmp.
notsame = memcmp(finalDigest, expectedDigest, sizeof(finalDigest));
if (notsame)
{
while(1);
}

Hashing data in multiple calls

SHA256SW_Object sha256SWObject;
SHA256SW_Handle sha256SWHandle = &sha256SWObject;
int_fast16_t sha2SWresult;
uint32_t finalDigest[8];
int notsame;
char message[] =
"abcdefghijklmnabcdefghijklmnabcdefghijklmnabcdefghijklmn1234";
uint8_t expectedDigest[] =
{ 0x60, 0x06, 0x00, 0x24, 0x13, 0xe4, 0x27, 0x0d,
0x4d, 0xdb, 0x66, 0x93, 0x42, 0xa9, 0xe2, 0xdb,
0x66, 0x5e, 0xc8, 0x70, 0x73, 0xc4, 0x2e, 0xb5,
0x44, 0x99, 0x62, 0xf1, 0x2a, 0xb2, 0xe8, 0x60, };
sha2SWresult = SHA256SWStart(sha256SWHandle, SHA2SW_HASH_TYPE_256);
if (sha2SWresult == SHA2SW_STATUS_SUCCESS) {
sha2SWresult = SHA256SWAddData(sha256SWHandle, message, 20);
}
if (sha2SWresult == SHA2SW_STATUS_SUCCESS) {
sha2SWresult = SHA256SWAddData(sha256SWHandle, &message[20], strlen(message) - 20);
}
if (sha2SWresult == SHA2SW_STATUS_SUCCESS) {
sha2SWresult = SHA256SWFinalize(sha256SWHandle, finalDigest);
}
if (sha2SWresult != SHA2SW_STATUS_SUCCESS)
{
while(1);
}
// NOTE: If expectedDigest is a secret value, a timing constant comparison
// routine shall be used instead of memcmp.
notsame = memcmp(finalDigest, expectedDigest, sizeof(finalDigest));
if (notsame)
{
while(1);
}

Configuration

See file sha2sw_config.h for full configuration information.

If SHA2SW_VALIDATE_INPUTS is not defined then:

Macro Definition Documentation

§ SHA256SWHashData

#define SHA256SWHashData   HAPI_TABLE_POINTER->sha256SwHashData

§ SHA256SWStart

#define SHA256SWStart   HAPI_TABLE_POINTER->sha256SwStart

§ SHA256SWAddData

#define SHA256SWAddData   HAPI_TABLE_POINTER->sha256SwAddData

§ SHA256SWFinalize

#define SHA256SWFinalize   HAPI_TABLE_POINTER->sha256SwFinalize

Typedef Documentation

§ SHA256SW_Handle

Function Documentation

§ SHA256SWHashData()

int_fast16_t SHA256SWHashData ( SHA256SW_Handle  handle,
SHA2SW_HashType  hashType,
const void *  data,
size_t  length,
uint32_t  digest[8] 
)

Performs a complete hash operation, producing a final digest for the data.

This function wraps SHA256SWStart(), SHA256SWAddData(), and SHA256SWFinalize().

There is no need to call SHA256SWStart() prior to calling this function.

The total length of data that can be hashed by this implementation is 512MiB (0x20000000 bytes.)

Parameters
[in]handleA SHA256SW_Handle.
[in]hashTypeThe type of hash (256 or 224) to perform.
[in]datadata (message) to hash. May point to zero.
[in]lengththe number of bytes (pointed to by data parameter) to add to the hash.
[out]digestOutput location for the final digest. Must be able to hold 32 bytes of output and be 32-bit aligned.
Return values
SHA2SW_STATUS_SUCCESSThe hash operation succeeded.
SHA2SW_STATUS_ERRORThe hash operation failed.
SHA2SW_STATUS_UNSUPPORTEDRequested Hash Type is unsupported.
SHA2SW_STATUS_LENGTH_TOO_LARGEThe requested length of data to hash is more than the implementation supports.
SHA2SW_STATUS_NULL_INPUTOne or more of the pointer inputs is NULL.

§ SHA256SWStart()

int_fast16_t SHA256SWStart ( SHA256SW_Handle  handle,
SHA2SW_HashType  hashType 
)

Initialize a SHA256SW_Handle, preparing for hashing data.

Parameters
[in]handleA SHA256SW_Handle.
[in]hashTypeThe type of hash (256 or 224) to perform.
Return values
SHA2SW_STATUS_SUCCESSThe hash operation succeeded.
SHA2SW_STATUS_UNSUPPORTEDRequested Hash Type is unsupported.
SHA2SW_STATUS_NULL_INPUTOne or more of the pointer inputs is NULL.
See also
SHA256SWAddData()
SHA256SWFinalize()

§ SHA256SWAddData()

int_fast16_t SHA256SWAddData ( SHA256SW_Handle  handle,
const void *  data,
size_t  length 
)

Add data to a SHA256/224 operation.

Adds data to a hash operation. The handle must have been initialized by a call to SHA256SWStart first.

The total length of data that can be hashed by this implementation is 512MiB (0x20000000 bytes.)

After passing in all data to be hashed, call SHA256SWFinalize() to obtain the final digest.

Precondition
handle was previously passed to SHA256SWStart().
Parameters
[in]handleA SHA256SW_Handle.
[in]datadata (message) to add to the hash. May point to zero.
[in]lengththe number of bytes (pointed to by data parameter) to add to the hash.
Return values
SHA2SW_STATUS_SUCCESSThe hash operation succeeded.
SHA2SW_STATUS_LENGTH_TOO_LARGEThe requested length of data to hash is more than the implementation supports.
SHA2SW_STATUS_NULL_INPUTOne or more of the pointer inputs is NULL.
See also
SHA256SWStart()
SHA256SWFinalize()

§ SHA256SWFinalize()

int_fast16_t SHA256SWFinalize ( SHA256SW_Handle  handle,
uint32_t  digest[8] 
)

Finalize a SHA256/224 operation, creating the final digest.

After calling this function, handle should not be used again until it has been reinitialized via a call to SHA256SWStart().

Precondition
handle was previously passed to SHA256SWStart() and data to be hashed was passed to SHA256SWAddData()
Parameters
[in]handleA SHA256SW_Handle.
[out]digestOutput location for the final digest. Must be able to hold 32 bytes of output and be 32-bit aligned.
Return values
SHA2SW_STATUS_SUCCESSThe hash operation succeeded.
SHA2SW_STATUS_NULL_INPUTOne or more of the pointer inputs is NULL.
See also
SHA256SWStart()
SHA256SWAddData()