Introduction
The GPIO module allows software to control the pins of the device directly.
The System CPU can access the GPIO module to read the value of any DIO of the device and if the IOC module has been configured such that one or more DIOs are GPIO controlled (software controlled) the System CPU can write these DIOs through the GPIO module.
The IOC module can also be configured to generate events on edge detection and these events can be read and cleared in the GPIO module by the System CPU.
API
The API functions can be grouped like this:
Set and get direction of DIO (output enable):
Write DIO (requires IOC to be configured for GPIO usage):
Set, clear, or toggle DIO (requires IOC to be configured for GPIO usage):
Read DIO (even if IOC is NOT configured for GPIO usage; however, the DIO must be configured for input enable in IOC):
Read or clear events (even if IOC is NOT configured for GPIO usage; however, the DIO must be configured for input enable in IOC):
§ GPIO_DIO_0_MASK
| #define GPIO_DIO_0_MASK 0x00000001 |
§ GPIO_DIO_1_MASK
| #define GPIO_DIO_1_MASK 0x00000002 |
§ GPIO_DIO_2_MASK
| #define GPIO_DIO_2_MASK 0x00000004 |
§ GPIO_DIO_3_MASK
| #define GPIO_DIO_3_MASK 0x00000008 |
§ GPIO_DIO_4_MASK
| #define GPIO_DIO_4_MASK 0x00000010 |
§ GPIO_DIO_5_MASK
| #define GPIO_DIO_5_MASK 0x00000020 |
§ GPIO_DIO_6_MASK
| #define GPIO_DIO_6_MASK 0x00000040 |
§ GPIO_DIO_7_MASK
| #define GPIO_DIO_7_MASK 0x00000080 |
§ GPIO_DIO_8_MASK
| #define GPIO_DIO_8_MASK 0x00000100 |
§ GPIO_DIO_9_MASK
| #define GPIO_DIO_9_MASK 0x00000200 |
§ GPIO_DIO_10_MASK
| #define GPIO_DIO_10_MASK 0x00000400 |
§ GPIO_DIO_11_MASK
| #define GPIO_DIO_11_MASK 0x00000800 |
§ GPIO_DIO_12_MASK
| #define GPIO_DIO_12_MASK 0x00001000 |
§ GPIO_DIO_13_MASK
| #define GPIO_DIO_13_MASK 0x00002000 |
§ GPIO_DIO_14_MASK
| #define GPIO_DIO_14_MASK 0x00004000 |
§ GPIO_DIO_15_MASK
| #define GPIO_DIO_15_MASK 0x00008000 |
§ GPIO_DIO_16_MASK
| #define GPIO_DIO_16_MASK 0x00010000 |
§ GPIO_DIO_17_MASK
| #define GPIO_DIO_17_MASK 0x00020000 |
§ GPIO_DIO_18_MASK
| #define GPIO_DIO_18_MASK 0x00040000 |
§ GPIO_DIO_19_MASK
| #define GPIO_DIO_19_MASK 0x00080000 |
§ GPIO_DIO_20_MASK
| #define GPIO_DIO_20_MASK 0x00100000 |
§ GPIO_DIO_21_MASK
| #define GPIO_DIO_21_MASK 0x00200000 |
§ GPIO_DIO_22_MASK
| #define GPIO_DIO_22_MASK 0x00400000 |
§ GPIO_DIO_23_MASK
| #define GPIO_DIO_23_MASK 0x00800000 |
§ GPIO_DIO_24_MASK
| #define GPIO_DIO_24_MASK 0x01000000 |
§ GPIO_DIO_25_MASK
| #define GPIO_DIO_25_MASK 0x02000000 |
§ GPIO_DIO_26_MASK
| #define GPIO_DIO_26_MASK 0x04000000 |
§ GPIO_DIO_27_MASK
| #define GPIO_DIO_27_MASK 0x08000000 |
§ GPIO_DIO_28_MASK
| #define GPIO_DIO_28_MASK 0x10000000 |
§ GPIO_DIO_29_MASK
| #define GPIO_DIO_29_MASK 0x20000000 |
§ GPIO_DIO_30_MASK
| #define GPIO_DIO_30_MASK 0x40000000 |
§ GPIO_DIO_ALL_MASK
| #define GPIO_DIO_ALL_MASK 0xFFFFFFFF |
§ GPIO_OUTPUT_DISABLE
| #define GPIO_OUTPUT_DISABLE 0x00000000 |
§ GPIO_OUTPUT_ENABLE
| #define GPIO_OUTPUT_ENABLE 0x00000001 |
§ GPIOReadDio()
§ GPIOReadMultiDio()
Reads the input value for the specified DIOs.
This function returns the input value for multiple DIOs. The value returned is not shifted and hence matches the corresponding dioMask bits.
- Parameters
-
| dioMask | is the bit-mask representation of the DIOs to read. The parameter must be a bitwise OR'ed combination of the following:
|
- Returns
- Returns a bit vector reflecting the input value of the corresponding DIOs.
- 0 : Corresponding DIO is low.
- 1 : Corresponding DIO is high.
- See also
- GPIOReadDio(), GPIOWriteDio(), GPIOWriteMultiDio()
References ASSERT, and GPIO_DIO_ALL_MASK.
§ GPIOWriteDio()
§ GPIOWriteMultiDio()
| __STATIC_INLINE void GPIOWriteMultiDio |
( |
uint32_t |
dioMask, |
|
|
uint32_t |
bitVectoredValue |
|
) |
| |
Writes masked data to the specified DIOs.
Enables for writing multiple bits simultaneously. The value to write must be shifted so it matches the corresponding dioMask bits.
- Note
- Note that this is a read-modify-write operation and hence not atomic.
- Parameters
-
| dioMask | is the bit-mask representation of the DIOs to write. The parameter must be a bitwise OR'ed combination of the following:
|
| bitVectoredValue | holds the value to be written to the corresponding DIO-bits. |
- Returns
- None
- See also
- GPIOWriteDio(), GPIOReadDio(), GPIOReadMultiDio()
References ASSERT, and GPIO_DIO_ALL_MASK.
§ GPIOSetDio()
§ GPIOSetMultiDio()
§ GPIOClearDio()
§ GPIOClearMultiDio()
§ GPIOToggleDio()
Toggles a specific DIO.
- Parameters
-
| dioNumber | specifies the DIO to toggle (0-31). |
- Returns
- None
- See also
- GPIOToggleMultiDio()
References ASSERT.
§ GPIOToggleMultiDio()
Toggles the specified DIOs.
- Parameters
-
| dioMask | is the bit-mask representation of the DIOs to toggle. The parameter must be a bitwise OR'ed combination of the following:
|
- Returns
- None
- See also
- GPIOToggleDio()
References ASSERT, and GPIO_DIO_ALL_MASK.
§ GPIOGetOutputEnableDio()
Gets the output enable status of a specific DIO.
This function returns the output enable status for the specified DIO. The DIO can be configured as either input or output under software control.
- Parameters
-
| dioNumber | specifies the DIO to get the output enable setting from (0-31). |
- Returns
- Returns one of the enumerated data types (0 or 1):
- See also
- GPIOGetOutputEnableMultiDio(), GPIOSetOutputEnableDio(), GPIOSetOutputEnableMultiDio()
References ASSERT.
§ GPIOGetOutputEnableMultiDio()
Gets the output enable setting of the specified DIOs.
This function returns the output enable setting for multiple DIOs. The value returned is not shifted and hence matches the corresponding dioMask bits.
- Parameters
-
| dioMask | is the bit-mask representation of the DIOs to return the output enable settings from. The parameter must be a bitwise OR'ed combination of the following:
|
- Returns
- Returns the output enable setting for multiple DIOs as a bit vector corresponding to the dioMask bits.
- 0 : Corresponding DIO is configured with output disabled.
- 1 : Corresponding DIO is configured with output enabled.
- See also
- GPIOGetOutputEnableDio(), GPIOSetOutputEnableDio(), GPIOSetOutputEnableMultiDio()
References ASSERT, and GPIO_DIO_ALL_MASK.
§ GPIOSetOutputEnableDio()
| __STATIC_INLINE void GPIOSetOutputEnableDio |
( |
uint32_t |
dioNumber, |
|
|
uint32_t |
outputEnableValue |
|
) |
| |
§ GPIOSetOutputEnableMultiDio()
| __STATIC_INLINE void GPIOSetOutputEnableMultiDio |
( |
uint32_t |
dioMask, |
|
|
uint32_t |
bitVectoredOutputEnable |
|
) |
| |
Configures the output enable setting for all specified DIOs.
This function configures the output enable setting for the specified DIOs. The output enable setting must be shifted so it matches the corresponding dioMask bits. The DIOs can be configured as either an input or output under software control.
- Note
- Note that this is a read-modify-write operation and hence not atomic.
- Parameters
-
| dioMask | is the bit-mask representation of the DIOs on which to configure the output enable setting. The parameter must be a bitwise OR'ed combination of the following:
|
| bitVectoredOutputEnable | holds the output enable setting the corresponding DIO-bits:
- 0 : Corresponding DIO is configured with output disabled.
- 1 : Corresponding DIO is configured with output enabled.
|
- Returns
- None
- See also
- GPIOSetOutputEnableDio(), GPIOGetOutputEnableDio(), GPIOGetOutputEnableMultiDio()
References ASSERT, and GPIO_DIO_ALL_MASK.
§ GPIOGetEventDio()
§ GPIOGetEventMultiDio()
Gets the event status of the specified DIOs.
This function returns the event status for multiple DIOs. The value returned is not shifted and hence matches the corresponding dioMask bits.
- Parameters
-
| dioMask | is the bit-mask representation of the DIOs to get the event status from (0-31). The parameter must be a bitwise OR'ed combination of the following:
|
- Returns
- Returns a bit vector with the current event status corresponding to the specified DIOs.
- 0 : Corresponding DIO has no triggered event.
- 1 : Corresponding DIO has a triggered event.
- See also
- GPIOGetEventDio(), GPIOClearEventDio(), GPIOClearEventMultiDio()
References ASSERT, and GPIO_DIO_ALL_MASK.
§ GPIOClearEventDio()
§ GPIOClearEventMultiDio()