Go to the documentation of this file. 25 #if defined ( __ICCARM__ ) 26 #pragma system_include 27 #elif defined (__clang__) 28 #pragma clang system_header 31 #ifndef __CMSIS_VERSION_H 32 #define __CMSIS_VERSION_H 35 #define __CM_CMSIS_VERSION_MAIN ( 5U) 36 #define __CM_CMSIS_VERSION_SUB ( 6U) 37 #define __CM_CMSIS_VERSION ((__CM_CMSIS_VERSION_MAIN << 16U) | \ 38 __CM_CMSIS_VERSION_SUB )