29 #ifndef __CMSIS_ICCARM_H__ 30 #define __CMSIS_ICCARM_H__ 33 #error This file should only be compiled by ICCARM 36 #pragma system_include 38 #define __IAR_FT _Pragma("inline=forced") __intrinsic 40 #if (__VER__ >= 8000000) 48 #define __ALIGNED(x) __attribute__((aligned(x))) 49 #elif (__VER__ >= 7080000) 51 #define __ALIGNED(x) __attribute__((aligned(x))) 53 #warning No compiler specific solution for __ALIGNED.__ALIGNED is ignored. 61 #if __ARM_ARCH_6M__ || __ARM_ARCH_7M__ || __ARM_ARCH_7EM__ || __ARM_ARCH_8M_BASE__ || __ARM_ARCH_8M_MAIN__ 64 #if defined(__ARM8M_MAINLINE__) || defined(__ARM8EM_MAINLINE__) 65 #define __ARM_ARCH_8M_MAIN__ 1 66 #elif defined(__ARM8M_BASELINE__) 67 #define __ARM_ARCH_8M_BASE__ 1 68 #elif defined(__ARM_ARCH_PROFILE) && __ARM_ARCH_PROFILE == 'M' 70 #define __ARM_ARCH_6M__ 1 73 #define __ARM_ARCH_7EM__ 1 75 #define __ARM_ARCH_7M__ 1 82 #if !defined(__ARM_ARCH_6M__) && !defined(__ARM_ARCH_7M__) && !defined(__ARM_ARCH_7EM__) && \ 83 !defined(__ARM_ARCH_8M_BASE__) && !defined(__ARM_ARCH_8M_MAIN__) 84 #if defined(__ARM6M__) && (__CORE__ == __ARM6M__) 85 #define __ARM_ARCH_6M__ 1 86 #elif defined(__ARM7M__) && (__CORE__ == __ARM7M__) 87 #define __ARM_ARCH_7M__ 1 88 #elif defined(__ARM7EM__) && (__CORE__ == __ARM7EM__) 89 #define __ARM_ARCH_7EM__ 1 90 #elif defined(__ARM8M_BASELINE__) && (__CORE == __ARM8M_BASELINE__) 91 #define __ARM_ARCH_8M_BASE__ 1 92 #elif defined(__ARM8M_MAINLINE__) && (__CORE == __ARM8M_MAINLINE__) 93 #define __ARM_ARCH_8M_MAIN__ 1 94 #elif defined(__ARM8EM_MAINLINE__) && (__CORE == __ARM8EM_MAINLINE__) 95 #define __ARM_ARCH_8M_MAIN__ 1 97 #error "Unknown target." 103 #if defined(__ARM_ARCH_6M__) && __ARM_ARCH_6M__==1 104 #define __IAR_M0_FAMILY 1 105 #elif defined(__ARM_ARCH_8M_BASE__) && __ARM_ARCH_8M_BASE__==1 106 #define __IAR_M0_FAMILY 1 108 #define __IAR_M0_FAMILY 0 112 #define __NO_INIT __attribute__ ((section (".noinit"))) 115 #define __ALIAS(x) __attribute__ ((alias(x))) 122 #ifndef __COMPILER_BARRIER 123 #define __COMPILER_BARRIER() __ASM volatile("":::"memory") 127 #define __INLINE inline 132 #define __NO_RETURN __attribute__((__noreturn__)) 134 #define __NO_RETURN _Pragma("object_attribute=__noreturn") 140 #define __PACKED __attribute__((packed, aligned(1))) 143 #define __PACKED __packed 147 #ifndef __PACKED_STRUCT 149 #define __PACKED_STRUCT struct __attribute__((packed, aligned(1))) 152 #define __PACKED_STRUCT __packed struct 156 #ifndef __PACKED_UNION 158 #define __PACKED_UNION union __attribute__((packed, aligned(1))) 161 #define __PACKED_UNION __packed union 167 #define __RESTRICT __restrict 170 #define __RESTRICT restrict 174 #ifndef __STATIC_INLINE 175 #define __STATIC_INLINE static inline 178 #ifndef __FORCEINLINE 179 #define __FORCEINLINE _Pragma("inline=forced") 182 #ifndef __STATIC_FORCEINLINE 183 #define __STATIC_FORCEINLINE __FORCEINLINE __STATIC_INLINE 186 #ifndef __UNALIGNED_UINT16_READ 187 #pragma language=save 188 #pragma language=extended 191 return *(__packed uint16_t*)(ptr);
193 #pragma language=restore 194 #define __UNALIGNED_UINT16_READ(PTR) __iar_uint16_read(PTR) 198 #ifndef __UNALIGNED_UINT16_WRITE 199 #pragma language=save 200 #pragma language=extended 203 *(__packed uint16_t*)(ptr) = val;;
205 #pragma language=restore 206 #define __UNALIGNED_UINT16_WRITE(PTR,VAL) __iar_uint16_write(PTR,VAL) 209 #ifndef __UNALIGNED_UINT32_READ 210 #pragma language=save 211 #pragma language=extended 214 return *(__packed uint32_t*)(ptr);
216 #pragma language=restore 217 #define __UNALIGNED_UINT32_READ(PTR) __iar_uint32_read(PTR) 220 #ifndef __UNALIGNED_UINT32_WRITE 221 #pragma language=save 222 #pragma language=extended 225 *(__packed uint32_t*)(ptr) = val;;
227 #pragma language=restore 228 #define __UNALIGNED_UINT32_WRITE(PTR,VAL) __iar_uint32_write(PTR,VAL) 231 #ifndef __UNALIGNED_UINT32 232 #pragma language=save 233 #pragma language=extended 235 #pragma language=restore 236 #define __UNALIGNED_UINT32(PTR) (((struct __iar_u32 *)(PTR))->v) 241 #define __USED __attribute__((used)) 243 #define __USED _Pragma("__root") 250 #define __WEAK __attribute__((weak)) 252 #define __WEAK _Pragma("__weak") 256 #ifndef __PROGRAM_START 257 #define __PROGRAM_START __iar_program_start 261 #define __INITIAL_SP CSTACK$$Limit 264 #ifndef __STACK_LIMIT 265 #define __STACK_LIMIT CSTACK$$Base 268 #ifndef __VECTOR_TABLE 269 #define __VECTOR_TABLE __vector_table 272 #ifndef __VECTOR_TABLE_ATTRIBUTE 273 #define __VECTOR_TABLE_ATTRIBUTE @".intvec" 276 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 278 #define __STACK_SEAL STACKSEAL$$Base 281 #ifndef __TZ_STACK_SEAL_SIZE 282 #define __TZ_STACK_SEAL_SIZE 8U 285 #ifndef __TZ_STACK_SEAL_VALUE 286 #define __TZ_STACK_SEAL_VALUE 0xFEF5EDA5FEF5EDA5ULL 290 *((uint64_t *)stackTop) = __TZ_STACK_SEAL_VALUE;
294 #ifndef __ICCARM_INTRINSICS_VERSION__ 295 #define __ICCARM_INTRINSICS_VERSION__ 0 298 #if __ICCARM_INTRINSICS_VERSION__ == 2 316 #include "iccarm_builtin.h" 318 #define __disable_fault_irq __iar_builtin_disable_fiq 319 #define __disable_irq __iar_builtin_disable_interrupt 320 #define __enable_fault_irq __iar_builtin_enable_fiq 321 #define __enable_irq __iar_builtin_enable_interrupt 322 #define __arm_rsr __iar_builtin_rsr 323 #define __arm_wsr __iar_builtin_wsr 326 #define __get_APSR() (__arm_rsr("APSR")) 327 #define __get_BASEPRI() (__arm_rsr("BASEPRI")) 328 #define __get_CONTROL() (__arm_rsr("CONTROL")) 329 #define __get_FAULTMASK() (__arm_rsr("FAULTMASK")) 331 #if ((defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U)) && \ 332 (defined (__FPU_USED ) && (__FPU_USED == 1U)) ) 333 #define __get_FPSCR() (__arm_rsr("FPSCR")) 334 #define __set_FPSCR(VALUE) (__arm_wsr("FPSCR", (VALUE))) 336 #define __get_FPSCR() ( 0 ) 337 #define __set_FPSCR(VALUE) ((void)VALUE) 340 #define __get_IPSR() (__arm_rsr("IPSR")) 341 #define __get_MSP() (__arm_rsr("MSP")) 342 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 343 (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3))) 345 #define __get_MSPLIM() (0U) 347 #define __get_MSPLIM() (__arm_rsr("MSPLIM")) 349 #define __get_PRIMASK() (__arm_rsr("PRIMASK")) 350 #define __get_PSP() (__arm_rsr("PSP")) 352 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 353 (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3))) 355 #define __get_PSPLIM() (0U) 357 #define __get_PSPLIM() (__arm_rsr("PSPLIM")) 360 #define __get_xPSR() (__arm_rsr("xPSR")) 362 #define __set_BASEPRI(VALUE) (__arm_wsr("BASEPRI", (VALUE))) 363 #define __set_BASEPRI_MAX(VALUE) (__arm_wsr("BASEPRI_MAX", (VALUE))) 367 __arm_wsr(
"CONTROL", control);
371 #define __set_FAULTMASK(VALUE) (__arm_wsr("FAULTMASK", (VALUE))) 372 #define __set_MSP(VALUE) (__arm_wsr("MSP", (VALUE))) 374 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 375 (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3))) 377 #define __set_MSPLIM(VALUE) ((void)(VALUE)) 379 #define __set_MSPLIM(VALUE) (__arm_wsr("MSPLIM", (VALUE))) 381 #define __set_PRIMASK(VALUE) (__arm_wsr("PRIMASK", (VALUE))) 382 #define __set_PSP(VALUE) (__arm_wsr("PSP", (VALUE))) 383 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 384 (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3))) 386 #define __set_PSPLIM(VALUE) ((void)(VALUE)) 388 #define __set_PSPLIM(VALUE) (__arm_wsr("PSPLIM", (VALUE))) 391 #define __TZ_get_CONTROL_NS() (__arm_rsr("CONTROL_NS")) 395 __arm_wsr(
"CONTROL_NS", control);
399 #define __TZ_get_PSP_NS() (__arm_rsr("PSP_NS")) 400 #define __TZ_set_PSP_NS(VALUE) (__arm_wsr("PSP_NS", (VALUE))) 401 #define __TZ_get_MSP_NS() (__arm_rsr("MSP_NS")) 402 #define __TZ_set_MSP_NS(VALUE) (__arm_wsr("MSP_NS", (VALUE))) 403 #define __TZ_get_SP_NS() (__arm_rsr("SP_NS")) 404 #define __TZ_set_SP_NS(VALUE) (__arm_wsr("SP_NS", (VALUE))) 405 #define __TZ_get_PRIMASK_NS() (__arm_rsr("PRIMASK_NS")) 406 #define __TZ_set_PRIMASK_NS(VALUE) (__arm_wsr("PRIMASK_NS", (VALUE))) 407 #define __TZ_get_BASEPRI_NS() (__arm_rsr("BASEPRI_NS")) 408 #define __TZ_set_BASEPRI_NS(VALUE) (__arm_wsr("BASEPRI_NS", (VALUE))) 409 #define __TZ_get_FAULTMASK_NS() (__arm_rsr("FAULTMASK_NS")) 410 #define __TZ_set_FAULTMASK_NS(VALUE)(__arm_wsr("FAULTMASK_NS", (VALUE))) 412 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 413 (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3))) 415 #define __TZ_get_PSPLIM_NS() (0U) 416 #define __TZ_set_PSPLIM_NS(VALUE) ((void)(VALUE)) 418 #define __TZ_get_PSPLIM_NS() (__arm_rsr("PSPLIM_NS")) 419 #define __TZ_set_PSPLIM_NS(VALUE) (__arm_wsr("PSPLIM_NS", (VALUE))) 422 #define __TZ_get_MSPLIM_NS() (__arm_rsr("MSPLIM_NS")) 423 #define __TZ_set_MSPLIM_NS(VALUE) (__arm_wsr("MSPLIM_NS", (VALUE))) 425 #define __NOP __iar_builtin_no_operation 427 #define __CLZ __iar_builtin_CLZ 428 #define __CLREX __iar_builtin_CLREX 430 #define __DMB __iar_builtin_DMB 431 #define __DSB __iar_builtin_DSB 432 #define __ISB __iar_builtin_ISB 434 #define __LDREXB __iar_builtin_LDREXB 435 #define __LDREXH __iar_builtin_LDREXH 436 #define __LDREXW __iar_builtin_LDREX 438 #define __RBIT __iar_builtin_RBIT 439 #define __REV __iar_builtin_REV 440 #define __REV16 __iar_builtin_REV16 444 return (int16_t) __iar_builtin_REVSH(val);
447 #define __ROR __iar_builtin_ROR 448 #define __RRX __iar_builtin_RRX 450 #define __SEV __iar_builtin_SEV 453 #define __SSAT __iar_builtin_SSAT 456 #define __STREXB __iar_builtin_STREXB 457 #define __STREXH __iar_builtin_STREXH 458 #define __STREXW __iar_builtin_STREX 461 #define __USAT __iar_builtin_USAT 464 #define __WFE __iar_builtin_WFE 465 #define __WFI __iar_builtin_WFI 468 #define __SADD8 __iar_builtin_SADD8 469 #define __QADD8 __iar_builtin_QADD8 470 #define __SHADD8 __iar_builtin_SHADD8 471 #define __UADD8 __iar_builtin_UADD8 472 #define __UQADD8 __iar_builtin_UQADD8 473 #define __UHADD8 __iar_builtin_UHADD8 474 #define __SSUB8 __iar_builtin_SSUB8 475 #define __QSUB8 __iar_builtin_QSUB8 476 #define __SHSUB8 __iar_builtin_SHSUB8 477 #define __USUB8 __iar_builtin_USUB8 478 #define __UQSUB8 __iar_builtin_UQSUB8 479 #define __UHSUB8 __iar_builtin_UHSUB8 480 #define __SADD16 __iar_builtin_SADD16 481 #define __QADD16 __iar_builtin_QADD16 482 #define __SHADD16 __iar_builtin_SHADD16 483 #define __UADD16 __iar_builtin_UADD16 484 #define __UQADD16 __iar_builtin_UQADD16 485 #define __UHADD16 __iar_builtin_UHADD16 486 #define __SSUB16 __iar_builtin_SSUB16 487 #define __QSUB16 __iar_builtin_QSUB16 488 #define __SHSUB16 __iar_builtin_SHSUB16 489 #define __USUB16 __iar_builtin_USUB16 490 #define __UQSUB16 __iar_builtin_UQSUB16 491 #define __UHSUB16 __iar_builtin_UHSUB16 492 #define __SASX __iar_builtin_SASX 493 #define __QASX __iar_builtin_QASX 494 #define __SHASX __iar_builtin_SHASX 495 #define __UASX __iar_builtin_UASX 496 #define __UQASX __iar_builtin_UQASX 497 #define __UHASX __iar_builtin_UHASX 498 #define __SSAX __iar_builtin_SSAX 499 #define __QSAX __iar_builtin_QSAX 500 #define __SHSAX __iar_builtin_SHSAX 501 #define __USAX __iar_builtin_USAX 502 #define __UQSAX __iar_builtin_UQSAX 503 #define __UHSAX __iar_builtin_UHSAX 504 #define __USAD8 __iar_builtin_USAD8 505 #define __USADA8 __iar_builtin_USADA8 506 #define __SSAT16 __iar_builtin_SSAT16 507 #define __USAT16 __iar_builtin_USAT16 508 #define __UXTB16 __iar_builtin_UXTB16 509 #define __UXTAB16 __iar_builtin_UXTAB16 510 #define __SXTB16 __iar_builtin_SXTB16 511 #define __SXTAB16 __iar_builtin_SXTAB16 512 #define __SMUAD __iar_builtin_SMUAD 513 #define __SMUADX __iar_builtin_SMUADX 514 #define __SMMLA __iar_builtin_SMMLA 515 #define __SMLAD __iar_builtin_SMLAD 516 #define __SMLADX __iar_builtin_SMLADX 517 #define __SMLALD __iar_builtin_SMLALD 518 #define __SMLALDX __iar_builtin_SMLALDX 519 #define __SMUSD __iar_builtin_SMUSD 520 #define __SMUSDX __iar_builtin_SMUSDX 521 #define __SMLSD __iar_builtin_SMLSD 522 #define __SMLSDX __iar_builtin_SMLSDX 523 #define __SMLSLD __iar_builtin_SMLSLD 524 #define __SMLSLDX __iar_builtin_SMLSLDX 525 #define __SEL __iar_builtin_SEL 526 #define __QADD __iar_builtin_QADD 527 #define __QSUB __iar_builtin_QSUB 528 #define __PKHBT __iar_builtin_PKHBT 529 #define __PKHTB __iar_builtin_PKHTB 536 #define __CLZ __cmsis_iar_clz_not_active 537 #define __SSAT __cmsis_iar_ssat_not_active 538 #define __USAT __cmsis_iar_usat_not_active 539 #define __RBIT __cmsis_iar_rbit_not_active 540 #define __get_APSR __cmsis_iar_get_APSR_not_active 544 #if (!((defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U)) && \ 545 (defined (__FPU_USED ) && (__FPU_USED == 1U)) )) 546 #define __get_FPSCR __cmsis_iar_get_FPSR_not_active 547 #define __set_FPSCR __cmsis_iar_set_FPSR_not_active 550 #ifdef __INTRINSICS_INCLUDED 551 #error intrinsics.h is already included previously! 554 #include <intrinsics.h> 566 if (data == 0U) {
return 32U; }
569 uint32_t mask = 0x80000000U;
571 while ((data & mask) == 0U)
583 for (v >>= 1U;
v; v >>= 1U)
595 __asm(
"MRS %0,APSR" :
"=r" (res));
601 #if (!((defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U)) && \ 602 (defined (__FPU_USED ) && (__FPU_USED == 1U)) )) 605 #define __get_FPSCR() (0) 606 #define __set_FPSCR(VALUE) ((void)VALUE) 609 #pragma diag_suppress=Pe940 610 #pragma diag_suppress=Pe177 612 #define __enable_irq __enable_interrupt 613 #define __disable_irq __disable_interrupt 614 #define __NOP __no_operation 616 #define __get_xPSR __get_PSR 618 #if (!defined(__ARM_ARCH_6M__) || __ARM_ARCH_6M__==0) 622 return __LDREX((
unsigned long *)ptr);
627 return __STREX(value, (
unsigned long *)ptr);
633 #if (__CORTEX_M >= 0x03) 635 __IAR_FT uint32_t __RRX(uint32_t value)
638 __ASM volatile(
"RRX %0, %1" :
"=r"(result) :
"r" (value));
642 __IAR_FT void __set_BASEPRI_MAX(uint32_t value)
644 __asm
volatile(
"MSR BASEPRI_MAX,%0"::
"r" (value));
648 #define __enable_fault_irq __enable_fiq 649 #define __disable_fault_irq __disable_fiq 656 return (op1 >> op2) | (op1 << ((
sizeof(op1)*8)-op2));
659 #if ((defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) || \ 660 (defined (__ARM_ARCH_8M_BASE__ ) && (__ARM_ARCH_8M_BASE__ == 1)) ) 662 __IAR_FT uint32_t __get_MSPLIM(
void)
665 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 666 (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3))) 670 __asm
volatile(
"MRS %0,MSPLIM" :
"=r" (res));
675 __IAR_FT void __set_MSPLIM(uint32_t value)
677 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 678 (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3))) 682 __asm
volatile(
"MSR MSPLIM,%0" ::
"r" (value));
686 __IAR_FT uint32_t __get_PSPLIM(
void)
689 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 690 (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3))) 694 __asm
volatile(
"MRS %0,PSPLIM" :
"=r" (res));
699 __IAR_FT void __set_PSPLIM(uint32_t value)
701 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 702 (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3))) 706 __asm
volatile(
"MSR PSPLIM,%0" ::
"r" (value));
710 __IAR_FT uint32_t __TZ_get_CONTROL_NS(
void)
713 __asm
volatile(
"MRS %0,CONTROL_NS" :
"=r" (res));
717 __IAR_FT void __TZ_set_CONTROL_NS(uint32_t value)
719 __asm
volatile(
"MSR CONTROL_NS,%0" ::
"r" (value));
723 __IAR_FT uint32_t __TZ_get_PSP_NS(
void)
726 __asm
volatile(
"MRS %0,PSP_NS" :
"=r" (res));
730 __IAR_FT void __TZ_set_PSP_NS(uint32_t value)
732 __asm
volatile(
"MSR PSP_NS,%0" ::
"r" (value));
735 __IAR_FT uint32_t __TZ_get_MSP_NS(
void)
738 __asm
volatile(
"MRS %0,MSP_NS" :
"=r" (res));
742 __IAR_FT void __TZ_set_MSP_NS(uint32_t value)
744 __asm
volatile(
"MSR MSP_NS,%0" ::
"r" (value));
747 __IAR_FT uint32_t __TZ_get_SP_NS(
void)
750 __asm
volatile(
"MRS %0,SP_NS" :
"=r" (res));
753 __IAR_FT void __TZ_set_SP_NS(uint32_t value)
755 __asm
volatile(
"MSR SP_NS,%0" ::
"r" (value));
758 __IAR_FT uint32_t __TZ_get_PRIMASK_NS(
void)
761 __asm
volatile(
"MRS %0,PRIMASK_NS" :
"=r" (res));
765 __IAR_FT void __TZ_set_PRIMASK_NS(uint32_t value)
767 __asm
volatile(
"MSR PRIMASK_NS,%0" ::
"r" (value));
770 __IAR_FT uint32_t __TZ_get_BASEPRI_NS(
void)
773 __asm
volatile(
"MRS %0,BASEPRI_NS" :
"=r" (res));
777 __IAR_FT void __TZ_set_BASEPRI_NS(uint32_t value)
779 __asm
volatile(
"MSR BASEPRI_NS,%0" ::
"r" (value));
782 __IAR_FT uint32_t __TZ_get_FAULTMASK_NS(
void)
785 __asm
volatile(
"MRS %0,FAULTMASK_NS" :
"=r" (res));
789 __IAR_FT void __TZ_set_FAULTMASK_NS(uint32_t value)
791 __asm
volatile(
"MSR FAULTMASK_NS,%0" ::
"r" (value));
794 __IAR_FT uint32_t __TZ_get_PSPLIM_NS(
void)
797 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 798 (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3))) 802 __asm
volatile(
"MRS %0,PSPLIM_NS" :
"=r" (res));
807 __IAR_FT void __TZ_set_PSPLIM_NS(uint32_t value)
809 #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \ 810 (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3))) 814 __asm
volatile(
"MSR PSPLIM_NS,%0" ::
"r" (value));
818 __IAR_FT uint32_t __TZ_get_MSPLIM_NS(
void)
821 __asm
volatile(
"MRS %0,MSPLIM_NS" :
"=r" (res));
825 __IAR_FT void __TZ_set_MSPLIM_NS(uint32_t value)
827 __asm
volatile(
"MSR MSPLIM_NS,%0" ::
"r" (value));
834 #define __BKPT(value) __asm volatile ("BKPT %0" : : "i"(value)) 839 if ((sat >= 1U) && (sat <= 32U))
841 const int32_t max = (int32_t)((1U << (sat - 1U)) - 1U);
842 const int32_t min = -1 - max ;
859 const uint32_t max = ((1U << sat) - 1U);
860 if (val > (int32_t)max)
869 return (uint32_t)val;
873 #if (__CORTEX_M >= 0x03) 875 __IAR_FT uint8_t __LDRBT(
volatile uint8_t *addr)
878 __ASM volatile (
"LDRBT %0, [%1]" :
"=r" (res) :
"r" (addr) :
"memory");
879 return ((uint8_t)res);
882 __IAR_FT uint16_t __LDRHT(
volatile uint16_t *addr)
885 __ASM volatile (
"LDRHT %0, [%1]" :
"=r" (res) :
"r" (addr) :
"memory");
886 return ((uint16_t)res);
889 __IAR_FT uint32_t __LDRT(
volatile uint32_t *addr)
892 __ASM volatile (
"LDRT %0, [%1]" :
"=r" (res) :
"r" (addr) :
"memory");
896 __IAR_FT void __STRBT(uint8_t value,
volatile uint8_t *addr)
898 __ASM volatile (
"STRBT %1, [%0]" : :
"r" (addr),
"r" ((uint32_t)value) :
"memory");
901 __IAR_FT void __STRHT(uint16_t value,
volatile uint16_t *addr)
903 __ASM volatile (
"STRHT %1, [%0]" : :
"r" (addr),
"r" ((uint32_t)value) :
"memory");
906 __IAR_FT void __STRT(uint32_t value,
volatile uint32_t *addr)
908 __ASM volatile (
"STRT %1, [%0]" : :
"r" (addr),
"r" (value) :
"memory");
913 #if ((defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) || \ 914 (defined (__ARM_ARCH_8M_BASE__ ) && (__ARM_ARCH_8M_BASE__ == 1)) ) 917 __IAR_FT uint8_t __LDAB(
volatile uint8_t *ptr)
920 __ASM volatile (
"LDAB %0, [%1]" :
"=r" (res) :
"r" (ptr) :
"memory");
921 return ((uint8_t)res);
924 __IAR_FT uint16_t __LDAH(
volatile uint16_t *ptr)
927 __ASM volatile (
"LDAH %0, [%1]" :
"=r" (res) :
"r" (ptr) :
"memory");
928 return ((uint16_t)res);
931 __IAR_FT uint32_t __LDA(
volatile uint32_t *ptr)
934 __ASM volatile (
"LDA %0, [%1]" :
"=r" (res) :
"r" (ptr) :
"memory");
938 __IAR_FT void __STLB(uint8_t value,
volatile uint8_t *ptr)
940 __ASM volatile (
"STLB %1, [%0]" ::
"r" (ptr),
"r" (value) :
"memory");
943 __IAR_FT void __STLH(uint16_t value,
volatile uint16_t *ptr)
945 __ASM volatile (
"STLH %1, [%0]" ::
"r" (ptr),
"r" (value) :
"memory");
948 __IAR_FT void __STL(uint32_t value,
volatile uint32_t *ptr)
950 __ASM volatile (
"STL %1, [%0]" ::
"r" (ptr),
"r" (value) :
"memory");
953 __IAR_FT uint8_t __LDAEXB(
volatile uint8_t *ptr)
956 __ASM volatile (
"LDAEXB %0, [%1]" :
"=r" (res) :
"r" (ptr) :
"memory");
957 return ((uint8_t)res);
960 __IAR_FT uint16_t __LDAEXH(
volatile uint16_t *ptr)
963 __ASM volatile (
"LDAEXH %0, [%1]" :
"=r" (res) :
"r" (ptr) :
"memory");
964 return ((uint16_t)res);
967 __IAR_FT uint32_t __LDAEX(
volatile uint32_t *ptr)
970 __ASM volatile (
"LDAEX %0, [%1]" :
"=r" (res) :
"r" (ptr) :
"memory");
974 __IAR_FT uint32_t __STLEXB(uint8_t value,
volatile uint8_t *ptr)
977 __ASM volatile (
"STLEXB %0, %2, [%1]" :
"=r" (res) :
"r" (ptr),
"r" (value) :
"memory");
981 __IAR_FT uint32_t __STLEXH(uint16_t value,
volatile uint16_t *ptr)
984 __ASM volatile (
"STLEXH %0, %2, [%1]" :
"=r" (res) :
"r" (ptr),
"r" (value) :
"memory");
988 __IAR_FT uint32_t __STLEX(uint32_t value,
volatile uint32_t *ptr)
991 __ASM volatile (
"STLEX %0, %2, [%1]" :
"=r" (res) :
"r" (ptr),
"r" (value) :
"memory");
998 #undef __IAR_M0_FAMILY 1001 #pragma diag_default=Pe940 1002 #pragma diag_default=Pe177 1004 #define __SXTB16_RORn(ARG1, ARG2) __SXTB16(__ROR(ARG1, ARG2)) 1006 #define __SXTAB16_RORn(ARG1, ARG2, ARG3) __SXTAB16(ARG1, __ROR(ARG2, ARG3)) #define __STATIC_FORCEINLINE
Definition: cmsis_iccarm.h:183
__STATIC_FORCEINLINE uint32_t __USAT(int32_t val, uint32_t sat)
Unsigned Saturate.
Definition: cmsis_gcc.h:738
uint32_t v
Definition: cmsis_iccarm.h:234
#define __STATIC_INLINE
Definition: cmsis_iccarm.h:175
#define __IAR_FT
Definition: cmsis_iccarm.h:38
__STATIC_FORCEINLINE int16_t __REVSH(int16_t value)
Reverse byte order (16 bit)
Definition: cmsis_gcc.h:332
__IAR_FT uint32_t __ROR(uint32_t op1, uint32_t op2)
Definition: cmsis_iccarm.h:654
#define __ASM
Definition: cmsis_iccarm.h:119
__STATIC_FORCEINLINE uint32_t __RBIT(uint32_t value)
Reverse bit order of value.
Definition: cmsis_gcc.h:379
__STATIC_FORCEINLINE uint32_t __get_APSR(void)
Get APSR Register.
Definition: cmsis_gcc.h:1047
__IAR_FT void __iar_uint32_write(void const *ptr, uint32_t val)
Definition: cmsis_iccarm.h:223
__STATIC_FORCEINLINE uint8_t __CLZ(uint32_t value)
Count leading zeros.
Definition: cmsis_gcc.h:409
__STATIC_FORCEINLINE void __set_CONTROL(uint32_t control)
Set Control Register.
Definition: cmsis_gcc.h:1007
__IAR_FT uint32_t __LDREXW(uint32_t volatile *ptr)
Definition: cmsis_iccarm.h:620
__STATIC_FORCEINLINE int32_t __SSAT(int32_t val, uint32_t sat)
Signed Saturate.
Definition: cmsis_gcc.h:713
__IAR_FT uint32_t __iar_uint32_read(void const *ptr)
Definition: cmsis_iccarm.h:212
__IAR_FT uint16_t __iar_uint16_read(void const *ptr)
Definition: cmsis_iccarm.h:189
Definition: cmsis_iccarm.h:234
__IAR_FT void __iar_uint16_write(void const *ptr, uint16_t val)
Definition: cmsis_iccarm.h:201
__IAR_FT uint32_t __STREXW(uint32_t value, uint32_t volatile *ptr)
Definition: cmsis_iccarm.h:625