Instance: PMCTL
Component: PMCTL
Base address: 0x40000000
This component is the Power Management controller. Together with the System Controller, it controls system resets and the power states of the device.
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
|
RO |
32 |
0xD741 0010 |
0x0000 0000 |
0x4000 0000 |
|
|
RO |
32 |
0xFC00 0000 |
0x0000 0004 |
0x4000 0004 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0008 |
0x4000 0008 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0x4000 000C |
|
|
RO |
32 |
0x0000 0001 |
0x0000 0010 |
0x4000 0010 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0x4000 0014 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0020 |
0x4000 0020 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0024 |
0x4000 0024 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0028 |
0x4000 0028 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x4000 002C |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0030 |
0x4000 0030 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0034 |
0x4000 0034 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 003C |
0x4000 003C |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0040 |
0x4000 0040 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0044 |
0x4000 0044 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0064 |
0x4000 0064 |
|
|
RW |
32 |
0x0000 0001 |
0x0000 007C |
0x4000 007C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0080 |
0x4000 0080 |
|
|
RW |
32 |
0x0000 0002 |
0x0000 0084 |
0x4000 0084 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0088 |
0x4000 0088 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 008C |
0x4000 008C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0090 |
0x4000 0090 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0094 |
0x4000 0094 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0098 |
0x4000 0098 |
| Address Offset | 0x0000 0000 | ||
| Physical Address | 0x4000 0000 | Instance | 0x4000 0000 |
| Description | Description Register. This register provides IP module ID, revision information, instance index and standard MMR registers offset. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | MODID | Module identifier used to uniquely identify this IP. | RO | 0xD741 | ||
| 15:12 | STDIPOFF | Standard IP MMR block offset. Standard IP MMRs are the set of from aggregated IRQ registers till DTB. 0: Standard IP MMRs do not exist 0x1-0xF: Standard IP MMRs begin at offset of (64*STDIPOFF from the base IP address) |
RO | 0x0 | ||
| 11:8 | INSTIDX | IP Instance ID number. If multiple instances of IP exist in the device, this field can identify the instance number (0-15). | RO | 0x0 | ||
| 7:4 | MAJREV | Major revision of IP (0-15). | RO | 0x1 | ||
| 3:0 | MINREV | Minor revision of IP (0-15). | RO | 0x0 | ||
| Address Offset | 0x0000 0004 | ||
| Physical Address | 0x4000 0004 | Instance | 0x4000 0004 |
| Description | Extended Description Register. This register shows ULL IP availability and memory size configuration. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||||||||
| 31:30 | FLASHSZ | System flash availability
|
RO | 0b11 | |||||||||||||||||
| 29:28 | SRAMSZ | System SRAM availability
|
RO | 0b11 | |||||||||||||||||
| 27 | TSD | TSD (thermal shutdown) IP status on device
|
RO | 1 | |||||||||||||||||
| 26 | LPCMP | LPCMP (low power comparator) IP status on device
|
RO | 1 | |||||||||||||||||
| 25:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 | |||||||||||||||||
| Address Offset | 0x0000 0008 | ||
| Physical Address | 0x4000 0008 | Instance | 0x4000 0008 |
| Description | Shutdown Register. This register controls SHUTDOWN mode entry. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||||||||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||||||||
| 15:0 | KEY | Setting a valid key will trigger the device to enter SHUTDOWN mode.
|
WO | 0x0000 | ||||||||
| Address Offset | 0x0000 000C | ||
| Physical Address | 0x4000 000C | Instance | 0x4000 000C |
| Description | Sleep Control Register. This register controls I/O pad sleep mode. When I/O pad sleep mode is enabled all I/O pad outputs and I/O pad configurations are latched. Inputs are transparent if I/O pad is configured as input. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 0 | SLPN | The boot code will set this bit field and disable sleep mode, automatically unless waking up from a SHUTDOWN RSTSTA.SDDET is set. Application software must reconfigure the state for all IO's before setting this bit field upon waking up from a SHUTDOWN to avoid glitches on pins.
|
RW | 0 | |||||||||||
| Address Offset | 0x0000 0010 | ||
| Physical Address | 0x4000 0010 | Instance | 0x4000 0010 |
| Description | Wakeup Status Register This register shows the device wakeup source. Used to distinguish between wakeup from STANDBY, SHUTDOWN and reset. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 1:0 | SRC | This field shows the device wakeup source.
|
RO | 0b01 | |||||||||||
| Address Offset | 0x0000 0014 | ||
| Physical Address | 0x4000 0014 | Instance | 0x4000 0014 |
| Description | VDDR Control Register. This register contains VDDR regulator settings for the device. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 1 | STBY | Select between continuous or duty-cycled VDDR regulation in STANDBY mode.
|
RW | 0 | |||||||||||
| 0 | SELECT | Select between GLDO and DCDC as VDDR regulator (in ACTIVE, IDLE and STANDBY mode).
|
RW | 0 | |||||||||||
| Address Offset | 0x0000 0020 | ||
| Physical Address | 0x4000 0020 | Instance | 0x4000 0020 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:3 | RESERVED3 | Internal. Only to be used through TI provided API. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 2 | FLAG2 | Internal. Only to be used through TI provided API.
|
WO | 0 | |||||||||||
| 1 | FLAG1 | Internal. Only to be used through TI provided API.
|
WO | 0 | |||||||||||
| 0 | FLAG0 | Internal. Only to be used through TI provided API.
|
WO | 0 | |||||||||||
| Address Offset | 0x0000 0024 | ||
| Physical Address | 0x4000 0024 | Instance | 0x4000 0024 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:3 | RESERVED3 | Internal. Only to be used through TI provided API. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 2 | FLAG2 | Internal. Only to be used through TI provided API.
|
WO | 0 | |||||||||||
| 1 | FLAG1 | Internal. Only to be used through TI provided API.
|
WO | 0 | |||||||||||
| 0 | FLAG0 | Internal. Only to be used through TI provided API.
|
WO | 0 | |||||||||||
| Address Offset | 0x0000 0028 | ||
| Physical Address | 0x4000 0028 | Instance | 0x4000 0028 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:3 | RESERVED3 | Internal. Only to be used through TI provided API. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 2 | FLAG2 | Internal. Only to be used through TI provided API.
|
RO | 0 | |||||||||||
| 1 | FLAG1 | Internal. Only to be used through TI provided API.
|
RO | 0 | |||||||||||
| 0 | FLAG0 | Internal. Only to be used through TI provided API.
|
RO | 0 | |||||||||||
| Address Offset | 0x0000 002C | ||
| Physical Address | 0x4000 002C | Instance | 0x4000 002C |
| Description | Reset Control Register. This register configures and controls system reset. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 2 | LFLOSS | LF clock loss reset enable. Trigger system reset when LF clock loss is detected, which reset the entire device and causes a reboot of the system. The system reset event is captured as RSTSTA.RESETSRC set to SYSRESET and RSTSTA.SYSSRC set to LFLOSSEV.
|
RW | 0 | |||||||||||
| 1 | TSDEN | TSD (Thermal Shutdown) enable. TSD will trigger an immediate system reset, which reset the entire device and causes a reboot of the system. The device will be in reset until released by the TSD IP. The system reset event is captured as RSTSTA.TSDEV flag set.
|
RW | 0 | |||||||||||
| 0 | SYSRST | Trigger system reset, which will reset the entire device and causes a reboot of the system. The system reset event is captured as RSTSTA.RESETSRC set to SYSRESET and RSTSTA.SYSSRC set to SYSRSTEV.
|
RW | 0 | |||||||||||
| Address Offset | 0x0000 0030 | ||
| Physical Address | 0x4000 0030 | Instance | 0x4000 0030 |
| Description | Reset Status. This register contains the reset source and SHUTDOWN wakeup source for the system. Check WUSTA.SRC first to ensure that wakeup from STANDBY is not set. The capture feature is not rearmed until all of the possible reset sources have been released and the result has been copied to this register. During the copy and rearm process it is one 24MHz period in which an eventual new system reset will be reported as Power on reset regardless of the root cause. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||
| 31:18 | RESERVED18 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 | ||||||||||||||||||||||||||||||||
| 17 | SDDET | Wakeup from SHUTDOWN flag. Note: This flag will be cleared when SLPCTL.SLPN is asserted.
|
RO | 0 | ||||||||||||||||||||||||||||||||
| 16 | IOWUSD | Wakeup from SHUTDOWN on an I/O event flag. Note: This flag will be cleared when SLPCTL.SLPN is asserted.
|
RO | 0 | ||||||||||||||||||||||||||||||||
| 15:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 | ||||||||||||||||||||||||||||||||
| 7:4 | SYSSRC | Shows which reset event that triggered SYSRESET in RESETSRC
|
RO | 0x0 | ||||||||||||||||||||||||||||||||
| 3 | TSDEV | System reset triggered by TSD event
|
RO | 0 | ||||||||||||||||||||||||||||||||
| 2:0 | RESETSRC | Shows the root cause of the last system reset. More than one reported reset source can have been active during the last system reset, but only the root cause is reported. If reset cause is SYSRESET or PINRESET, the other reset flags must be read to determine actual root cause.
|
RO | 0b000 | ||||||||||||||||||||||||||||||||
| Address Offset | 0x0000 0034 | ||
| Physical Address | 0x4000 0034 | Instance | 0x4000 0034 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| 31:8 | RESERVED8 | Internal. Only to be used through TI provided API. | RO | 0x00 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| 7:0 | FLAG | Internal. Only to be used through TI provided API.
|
RW | 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Address Offset | 0x0000 003C | ||
| Physical Address | 0x4000 003C | Instance | 0x4000 003C |
| Description | AON Register Status 1. This register contains the general purpose AON flags for SW, and is updated through AONRSET1.FLAG and AONRCLR1.FLAG. The register is only reset on a POR event. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:18 | RESERVED18 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 | ||
| 17:0 | FLAG | State of the AON register flags | RO | 0b00 0000 0000 0000 0000 | ||
| Address Offset | 0x0000 0040 | ||
| Physical Address | 0x4000 0040 | Instance | 0x4000 0040 |
| Description | AON Register Set 1. This register sets the AON flags that can be read through AONRSTA1.FLAG. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:18 | RESERVED18 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 | |||||||||||
| 17:0 | FLAG | Write 1 to set AONRSTA1.FLAG
|
WO | 0b00 0000 0000 0000 0000 | |||||||||||
| Address Offset | 0x0000 0044 | ||
| Physical Address | 0x4000 0044 | Instance | 0x4000 0044 |
| Description | AON Register Clear 1. This register clears the AON flags that can be read through AONRSTA1.FLAG. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:18 | RESERVED18 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 | |||||||||||
| 17:0 | FLAG | Write 1 to clear AONRSTA1.FLAG
|
WO | 0b00 0000 0000 0000 0000 | |||||||||||
| Address Offset | 0x0000 0064 | ||
| Physical Address | 0x4000 0064 | Instance | 0x4000 0064 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | RESERVED0 | Internal. Only to be used through TI provided API. | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 007C | ||
| Physical Address | 0x4000 007C | Instance | 0x4000 007C |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:1 | RESERVED1 | Internal. Only to be used through TI provided API. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
| 0 | VAL | Internal. Only to be used through TI provided API. | RW | 1 | ||
| Address Offset | 0x0000 0080 | ||
| Physical Address | 0x4000 0080 | Instance | 0x4000 0080 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:1 | RESERVED1 | Internal. Only to be used through TI provided API. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
| 0 | VAL | Internal. Only to be used through TI provided API. | RW | 0 | ||
| Address Offset | 0x0000 0084 | ||
| Physical Address | 0x4000 0084 | Instance | 0x4000 0084 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:3 | RESERVED3 | Internal. Only to be used through TI provided API. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | ||
| 2:0 | VAL | Internal. Only to be used through TI provided API. | RW | 0b010 | ||
| Address Offset | 0x0000 0088 | ||
| Physical Address | 0x4000 0088 | Instance | 0x4000 0088 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | RESERVED0 | Internal. Only to be used through TI provided API. | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 008C | ||
| Physical Address | 0x4000 008C | Instance | 0x4000 008C |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | RESERVED0 | Internal. Only to be used through TI provided API. | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 0090 | ||
| Physical Address | 0x4000 0090 | Instance | 0x4000 0090 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | RESERVED0 | Internal. Only to be used through TI provided API. | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 0094 | ||
| Physical Address | 0x4000 0094 | Instance | 0x4000 0094 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | RESERVED0 | Internal. Only to be used through TI provided API. | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 0098 | ||
| Physical Address | 0x4000 0098 | Instance | 0x4000 0098 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | RESERVED0 | Internal. Only to be used through TI provided API. | RO | 0x0000 0000 | ||
| © 2015 - 2016. Texas Instruments | All Rights Reserved |