CC23x0R5DriverLibrary
sha2sw_common.h
Go to the documentation of this file.
1 /******************************************************************************
2  * Copyright (c) 2022-2023 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions are met:
6  *
7  * 1) Redistributions of source code must retain the above copyright notice,
8  * this list of conditions and the following disclaimer.
9  *
10  * 2) Redistributions in binary form must reproduce the above copyright notice,
11  * this list of conditions and the following disclaimer in the documentation
12  * and/or other materials provided with the distribution.
13  *
14  * 3) Neither the name of the copyright holder nor the names of its
15  * contributors may be used to endorse or promote products derived from this
16  * software without specific prior written permission.
17  *
18  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
19  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
20  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
21  * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
22  * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
23  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
24  * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
25  * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
26  * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
27  * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
28  * POSSIBILITY OF SUCH DAMAGE.
29  *
30  ******************************************************************************/
31 #ifndef SHA2SW_COMMON_H_
32 #define SHA2SW_COMMON_H_
33 
45 #include <stddef.h>
46 #include <stdint.h>
47 
48 #include "sha2sw_config.h"
49 
53 typedef enum
54 {
56 #if SHA2SW_SUPPORT_SHA2_224 == 1
57  SHA2SW_HASH_TYPE_224 = 1,
58 #endif
59 #if SHA2SW_SUPPORT_SHA2_384 == 1
60  SHA2SW_HASH_TYPE_384 = 2,
61 #endif
64 
68 #define SHA2SW_224_OR_256_ROUNDS ((uint8_t)64u)
69 
73 #define SHA2SW_384_OR_512_ROUNDS ((uint8_t)80u)
74 
78 #define SHA2SW_224_OR_256_BLOCK_SIZE ((uint8_t)64u)
79 
83 #define SHA2SW_384_OR_512_BLOCK_SIZE ((uint8_t)128u)
84 
89 #define SHA2SW_MAX_MESSAGE_BIT_LENGTH ((uint32_t)0x20000000u)
90 
105 #define SHA2SW_STATUS_SUCCESS ((int_fast16_t)0)
106 
113 #define SHA2SW_STATUS_ERROR ((int_fast16_t)-100)
114 
120 #define SHA2SW_STATUS_UNSUPPORTED ((int_fast16_t)-102)
121 
127 #define SHA2SW_STATUS_LENGTH_TOO_LARGE ((int_fast16_t)-103)
128 
134 #define SHA2SW_STATUS_NULL_INPUT ((int_fast16_t)-104)
135 
139 #endif /* SHA2SW_COMMON_H_ */
Definition: sha2sw_common.h:55
Definition: sha2sw_common.h:62
SHA2SW_HashType
Enum for the hash types supported by the library.
Definition: sha2sw_common.h:53