CC23x0R5DriverLibrary
[tempdiode.h] High-accuracy temperature diode
Collaboration diagram for [tempdiode.h] High-accuracy temperature diode:

Functions

int32_t TempDiodeGetTemp (void)
 Reads temperature from high accuracy temperature diode. More...
 

Detailed Description

Function Documentation

§ TempDiodeGetTemp()

int32_t TempDiodeGetTemp ( void  )

Reads temperature from high accuracy temperature diode.

This function reads the temperature from the high-accuracy temperature diode The returned result contains 4 fractional bits. For example: 0x00000200 = +32.0000 degC 0x0000020C = +32.7500 degC 0xFFFFFEC3 = -19.8125 degC

Warning
This function uses the SoC ADC to measure the temperature. This function must not be called while the ADC driver is active, or the SoC ADC is open.
This function uses the internal test-bus (ATEST) to measure the temperature. The test-bus must not be used when calling this function.
Note
Due to long and repeated ADC sampling, this function takes roughly 8 milliseconds to execute.
Returns
Ambient temperature in degrees Celcius, with 4 fractional bits

References ADC_FIXED_REFERENCE_1V4, ADC_RESOLUTION_12_BIT, ADCAdjustValueForGain(), ADCEnableConversion(), ADCGetAdjustmentGain(), ADCReadResult(), ADCStartConversion(), ADCValueToMicrovolts(), CPUDelay(), enableADC(), IntDisableMaster(), IntEnableMaster(), and voltageToTemp().