CC23x0R5DriverLibrary
[spi.h] Serial Peripheral Interface
Collaboration diagram for [spi.h] Serial Peripheral Interface:

Macros

#define SPI_DMA_DONE_TX   SPI_IMASK_DMATX
 DMA Done 1 event for TX event mask. More...
 
#define SPI_DMA_DONE_RX   SPI_IMASK_DMARX
 DMA Done 1 event for RX event mask. More...
 
#define SPI_IDLE   SPI_IMASK_IDLE
 SPI Idle event mask. More...
 
#define SPI_TXEMPTY   SPI_IMASK_TXEMPTY
 Transmit FIFO Empty event mask. More...
 
#define SPI_TX   SPI_IMASK_TX
 Transmit FIFO event mask. More...
 
#define SPI_RX   SPI_IMASK_RX
 Receive FIFO event. This interrupt is set if the selected Receive FIFO level has been reached. More...
 
#define SPI_RTOUT   SPI_IMASK_RTOUT
 Enable SPI Receive Time-Out event mask. More...
 
#define SPI_PER   SPI_IMASK_PER
 Parity error event mask. More...
 
#define SPI_RXFIFO_OVF   SPI_IMASK_RXOVF
 RXFIFO overflow event mask. More...
 
#define SPI_BUSY   SPI_STA_BUSY_ACTIVE
 Busy. More...
 
#define SPI_RX_NOT_FULL   SPI_STA_RNF_NOT_FULL
 Receive FIFO not full. More...
 
#define SPI_RX_EMPTY   SPI_STA_RFE_EMPTY
 Receive FIFO empty. More...
 
#define SPI_TX_NOT_FULL   SPI_STA_TNF_NOT_FULL
 Transmit FIFO not full. More...
 
#define SPI_TX_EMPTY   SPI_STA_TFE_EMPTY
 Transmit FIFO empty. More...
 
#define SPI_STATUS_MASK   0x0000001F
 Mask for bits above. More...
 
#define SPI_FRF_MOTO_MODE_0   (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_FIRST)
 Motorola format 3-wire, polarity 0, phase 0. More...
 
#define SPI_FRF_MOTO_MODE_1   (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_SECOND)
 Motorola format 3-wire, polarity 0, phase 1. More...
 
#define SPI_FRF_MOTO_MODE_2   (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_FIRST)
 Motorola format 3-wire, polarity 1, phase 0. More...
 
#define SPI_FRF_MOTO_MODE_3   (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_SECOND)
 Motorola format 3-wire, polarity 1, phase 1. More...
 
#define SPI_FRF_MOTO_MODE_4   (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_FIRST)
 Motorola format 4-wire, polarity 0, phase 0. More...
 
#define SPI_FRF_MOTO_MODE_5   (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_SECOND)
 Motorola format 4-wire, polarity 0, phase 1. More...
 
#define SPI_FRF_MOTO_MODE_6   (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_FIRST)
 Motorola format 4-wire, polarity 1, phase 0. More...
 
#define SPI_FRF_MOTO_MODE_7   (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_SECOND)
 Motorola format 4-wire, polarity 1, phase 1. More...
 
#define SPI_FRF_TI   SPI_CTL0_FRF_TI_SYNC
 TI Sync frame format. More...
 
#define SPI_FRF_NMW   SPI_CTL0_FRF_MIRCOWIRE
 MicroWire frame format. More...
 
#define SPI_MODE_CONTROLLER   SPI_CTL1_MS_CONTROLLER
 SPI controller. More...
 
#define SPI_MODE_PERIPHERAL   SPI_CTL1_MS_PERIPHERAL
 SPI peripheral. More...
 
#define SPI_MODE_PERIPHERAL_OD   SPI_CTL1_SOD_ENABLE
 output disabled More...
 
#define SPI_DMA_TX   SPI_DMACR_TXEN
 Enable DMA for transmit. More...
 
#define SPI_DMA_RX   SPI_DMACR_RXEN
 Enable DMA for receive. More...
 

Functions

void SPIConfigSetExpClk (uint32_t base, uint32_t spiClk, uint32_t protocol, uint32_t mode, uint32_t bitRate, uint32_t dataWidth)
 Configures the serial peripheral port. More...
 
__STATIC_INLINE void SPIEnable (uint32_t base)
 Enables the serial peripheral port. More...
 
__STATIC_INLINE void SPIDisable (uint32_t base)
 Disables the serial peripheral port. More...
 
void SPIPutData (uint32_t base, uint32_t data)
 Puts a data element into the SPI transmit FIFO. More...
 
int32_t SPIPutDataNonBlocking (uint32_t base, uint32_t data)
 Puts a data element into the SPI transmit FIFO. More...
 
void SPIGetData (uint32_t base, uint32_t *data)
 Gets a data element from the SPI receive FIFO. More...
 
int32_t SPIGetDataNonBlocking (uint32_t base, uint32_t *data)
 Gets a data element from the SPI receive FIFO. More...
 
__STATIC_INLINE bool SPIBusy (uint32_t base)
 Determines whether the SPI transmitter is busy or not. More...
 
__STATIC_INLINE uint32_t SPIStatus (uint32_t base)
 Get the status of the SPI data buffers. More...
 
void SPIRegisterInt (uint32_t base, void(*pfnHandler)(void))
 Registers an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
 
void SPIUnregisterInt (uint32_t base)
 Unregisters an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
 
__STATIC_INLINE void SPIEnableInt (uint32_t base, uint32_t intFlags)
 Enables individual SPI interrupt sources. More...
 
__STATIC_INLINE void SPIDisableInt (uint32_t base, uint32_t intFlags)
 Disables individual SPI interrupt sources. More...
 
__STATIC_INLINE void SPIClearInt (uint32_t base, uint32_t intFlags)
 Clears SPI interrupt sources. More...
 
__STATIC_INLINE uint32_t SPIIntStatus (uint32_t base, bool isMasked)
 Gets the current interrupt status. More...
 
__STATIC_INLINE void SPIEnableDMA (uint32_t base, uint32_t dmaFlags)
 Enable SPI DMA operation. More...
 
__STATIC_INLINE void SPIDisableDMA (uint32_t base, uint32_t dmaFlags)
 Disable SPI DMA operation. More...
 

Detailed Description

Macro Definition Documentation

§ SPI_DMA_DONE_TX

#define SPI_DMA_DONE_TX   SPI_IMASK_DMATX

DMA Done 1 event for TX event mask.

§ SPI_DMA_DONE_RX

#define SPI_DMA_DONE_RX   SPI_IMASK_DMARX

DMA Done 1 event for RX event mask.

§ SPI_IDLE

#define SPI_IDLE   SPI_IMASK_IDLE

SPI Idle event mask.

§ SPI_TXEMPTY

#define SPI_TXEMPTY   SPI_IMASK_TXEMPTY

Transmit FIFO Empty event mask.

§ SPI_TX

#define SPI_TX   SPI_IMASK_TX

Transmit FIFO event mask.

§ SPI_RX

#define SPI_RX   SPI_IMASK_RX

Receive FIFO event. This interrupt is set if the selected Receive FIFO level has been reached.

§ SPI_RTOUT

#define SPI_RTOUT   SPI_IMASK_RTOUT

Enable SPI Receive Time-Out event mask.

§ SPI_PER

#define SPI_PER   SPI_IMASK_PER

Parity error event mask.

§ SPI_RXFIFO_OVF

#define SPI_RXFIFO_OVF   SPI_IMASK_RXOVF

RXFIFO overflow event mask.

§ SPI_BUSY

#define SPI_BUSY   SPI_STA_BUSY_ACTIVE

Busy.

§ SPI_RX_NOT_FULL

#define SPI_RX_NOT_FULL   SPI_STA_RNF_NOT_FULL

Receive FIFO not full.

§ SPI_RX_EMPTY

#define SPI_RX_EMPTY   SPI_STA_RFE_EMPTY

Receive FIFO empty.

§ SPI_TX_NOT_FULL

#define SPI_TX_NOT_FULL   SPI_STA_TNF_NOT_FULL

Transmit FIFO not full.

§ SPI_TX_EMPTY

#define SPI_TX_EMPTY   SPI_STA_TFE_EMPTY

Transmit FIFO empty.

§ SPI_STATUS_MASK

#define SPI_STATUS_MASK   0x0000001F

Mask for bits above.

Referenced by SPIStatus().

§ SPI_FRF_MOTO_MODE_0

#define SPI_FRF_MOTO_MODE_0   (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_FIRST)

Motorola format 3-wire, polarity 0, phase 0.

§ SPI_FRF_MOTO_MODE_1

#define SPI_FRF_MOTO_MODE_1   (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_SECOND)

Motorola format 3-wire, polarity 0, phase 1.

§ SPI_FRF_MOTO_MODE_2

#define SPI_FRF_MOTO_MODE_2   (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_FIRST)

Motorola format 3-wire, polarity 1, phase 0.

§ SPI_FRF_MOTO_MODE_3

#define SPI_FRF_MOTO_MODE_3   (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_SECOND)

Motorola format 3-wire, polarity 1, phase 1.

§ SPI_FRF_MOTO_MODE_4

#define SPI_FRF_MOTO_MODE_4   (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_FIRST)

Motorola format 4-wire, polarity 0, phase 0.

§ SPI_FRF_MOTO_MODE_5

#define SPI_FRF_MOTO_MODE_5   (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_SECOND)

Motorola format 4-wire, polarity 0, phase 1.

§ SPI_FRF_MOTO_MODE_6

#define SPI_FRF_MOTO_MODE_6   (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_FIRST)

Motorola format 4-wire, polarity 1, phase 0.

§ SPI_FRF_MOTO_MODE_7

#define SPI_FRF_MOTO_MODE_7   (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_SECOND)

Motorola format 4-wire, polarity 1, phase 1.

§ SPI_FRF_TI

#define SPI_FRF_TI   SPI_CTL0_FRF_TI_SYNC

TI Sync frame format.

§ SPI_FRF_NMW

#define SPI_FRF_NMW   SPI_CTL0_FRF_MIRCOWIRE

MicroWire frame format.

§ SPI_MODE_CONTROLLER

#define SPI_MODE_CONTROLLER   SPI_CTL1_MS_CONTROLLER

SPI controller.

§ SPI_MODE_PERIPHERAL

#define SPI_MODE_PERIPHERAL   SPI_CTL1_MS_PERIPHERAL

SPI peripheral.

§ SPI_MODE_PERIPHERAL_OD

#define SPI_MODE_PERIPHERAL_OD   SPI_CTL1_SOD_ENABLE

output disabled

SPI peripheral with POCI

§ SPI_DMA_TX

#define SPI_DMA_TX   SPI_DMACR_TXEN

Enable DMA for transmit.

§ SPI_DMA_RX

#define SPI_DMA_RX   SPI_DMACR_RXEN

Enable DMA for receive.

Function Documentation

§ SPIConfigSetExpClk()

void SPIConfigSetExpClk ( uint32_t  base,
uint32_t  spiClk,
uint32_t  protocol,
uint32_t  mode,
uint32_t  bitRate,
uint32_t  dataWidth 
)

Configures the serial peripheral port.

This function configures the serial peripheral port. It sets the SPI protocol, mode of operation, bit rate, and data width.

The protocol parameter defines the data frame format. The Motorola frame formats imply the following polarity and phase configurations:

Polarity Phase   Motorola Protocol                  Mode
  0       0           3-wire                SPI_FRF_MOTO_MODE_0
  0       1           3-wire                SPI_FRF_MOTO_MODE_1
  1       0           3-wire                SPI_FRF_MOTO_MODE_2
  1       1           3-wire                SPI_FRF_MOTO_MODE_3
  0       0           4-wire                SPI_FRF_MOTO_MODE_4
  0       1           4-wire                SPI_FRF_MOTO_MODE_5
  1       0           4-wire                SPI_FRF_MOTO_MODE_6
  1       1           4-wire                SPI_FRF_MOTO_MODE_7

The mode parameter defines the operating mode of the SPI module. The SPI module can operate as a controller or peripheral; if a peripheral, the SPI can be configured to disable output on its serial output line.

The bitRate parameter defines the bit rate for the SPI.

The dataWidth parameter defines the width of the data transfers, and can be a value between 4 and 32, for controller mode, and 7 to 32, in peripheral mode.

Note
The peripheral clock is not necessarily the same as the processor clock. The frequency of the peripheral clock is set by the system control.
Parameters
basespecifies the SPI module base address.
spiClkis the rate of the clock supplied to the SPI module.
protocolspecifies the data transfer protocol. The parameter can be one of the following values:
modespecifies the mode of operation. The parameter can be one of the following values:
bitRatespecifies the clock rate.
dataWidthspecifies number of bits transferred per frame. Must be a value between 4 and 16 for controller mode, and 7 to 16 in peripheral mode.
Returns
None

References ASSERT, DSAMPLE_HIGH_BITRATE, DSAMPLE_MED_BITRATE, and SPIConfig().

§ SPIEnable()

__STATIC_INLINE void SPIEnable ( uint32_t  base)

Enables the serial peripheral port.

This function enables operation of the serial peripheral port. The serial peripheral port must be configured before it is enabled.

Parameters
basespecifies the SPI module base address.
Returns
None

References ASSERT.

§ SPIDisable()

__STATIC_INLINE void SPIDisable ( uint32_t  base)

Disables the serial peripheral port.

This function disables operation of the serial peripheral port.

Parameters
basespecifies the SPI module base address.
Returns
None

References ASSERT, SPIGetData(), SPIGetDataNonBlocking(), SPIPutData(), and SPIPutDataNonBlocking().

§ SPIPutData()

void SPIPutData ( uint32_t  base,
uint32_t  data 
)

Puts a data element into the SPI transmit FIFO.

This function places the supplied data into the transmit FIFO of the specified SPI module.

Note
The upper 32 - N bits of the data are discarded by the hardware, where N is the data width as configured by SPIConfigSetExpClk(). For example, if the interface is configured for 8-bit data width, the upper 24 bits of data are discarded.
Parameters
basespecifies the SPI module base address.
datais the data to be transmitted over the SPI interface.
Returns
None

References ASSERT.

Referenced by SPIDisable().

§ SPIPutDataNonBlocking()

int32_t SPIPutDataNonBlocking ( uint32_t  base,
uint32_t  data 
)

Puts a data element into the SPI transmit FIFO.

This function places the supplied data into the transmit FIFO of the specified SPI module. If there is no space in the FIFO, then this function returns a zero.

Note
The upper 32 - N bits of the data are discarded by the hardware, where N is the data width as configured by SPIConfigSetExpClk(). For example, if the interface is configured for 8-bit data width, the upper 24 bits of data are discarded.
Parameters
basespecifies the SPI module base address.
datais the data to be transmitted over the SPI interface.
Returns
Returns the number of elements written to the SPI transmit FIFO.

References ASSERT.

Referenced by SPIDisable().

§ SPIGetData()

void SPIGetData ( uint32_t  base,
uint32_t *  data 
)

Gets a data element from the SPI receive FIFO.

This function gets received data from the receive FIFO of the specified SPI module and places that data into the location specified by the data parameter.

Note
Only the lower N bits of the value written to data contain valid data, where N is the data width as configured by SPIConfigSetExpClk(). For example, if the interface is configured for 8-bit data width, only the lower 8 bits of the value written to data contain valid data.
Parameters
basespecifies the SPI module base address.
datais a pointer to a storage location for data that was received over the SPI interface.
Returns
None

References ASSERT.

Referenced by SPIDisable().

§ SPIGetDataNonBlocking()

int32_t SPIGetDataNonBlocking ( uint32_t  base,
uint32_t *  data 
)

Gets a data element from the SPI receive FIFO.

This function gets received data from the receive FIFO of the specified SPI module and places that data into the location specified by the data parameter. If there is no data in the FIFO, then this function returns a zero.

Note
Only the lower N bits of the value written to data contain valid data, where N is the data width as configured by SPIConfigSetExpClk(). For example, if the interface is configured for 8-bit data width, only the lower 8 bits of the value written to data contain valid data.
Parameters
basespecifies the SPI module base address.
datais a pointer to a storage location for data that was received over the SPI interface.
Returns
Returns the number of elements read from the SPI receive FIFO.

References ASSERT.

Referenced by SPIDisable().

§ SPIBusy()

__STATIC_INLINE bool SPIBusy ( uint32_t  base)

Determines whether the SPI transmitter is busy or not.

Allows the caller to determine whether all transmitted bytes have cleared the transmitter hardware. If false is returned, then the transmit FIFO is empty and all bits of the last transmitted word have left the hardware shift register.

Parameters
baseis the base address of the SPI port.
Returns
Returns status of the SPI transmit buffer.
  • true : SPI is transmitting.
  • false : SPI transmissions are complete.

References ASSERT.

§ SPIStatus()

__STATIC_INLINE uint32_t SPIStatus ( uint32_t  base)

Get the status of the SPI data buffers.

This function is used to poll the status of the internal FIFOs in the SPI module. The status of both TX and RX FIFO is returned.

Parameters
basespecifies the SPI module base address.
Returns
Returns the current status of the internal SPI data buffers. The status is a bitwise OR'ed combination of:

References ASSERT, SPI_STATUS_MASK, SPIRegisterInt(), and SPIUnregisterInt().

§ SPIRegisterInt()

void SPIRegisterInt ( uint32_t  base,
void(*)(void)  pfnHandler 
)

Registers an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table.

Note
Only use this function if you want to use the dynamic vector table (in SRAM)!

This function registers a function as the interrupt handler for a specific interrupt and enables the corresponding interrupt in the interrupt controller.

Specific SPI interrupts must be enabled via SPIEnableInt(). If necessary, it is the interrupt handler's responsibility to clear the interrupt source via SPIClearInt().

Parameters
basespecifies the SPI module base address.
pfnHandleris a pointer to the function to be called when the serial peripheral port interrupt occurs.
Returns
None
See also
IntRegister() for important information about registering interrupt handlers.

References ASSERT, IntEnable(), and IntRegister().

Referenced by SPIStatus().

§ SPIUnregisterInt()

void SPIUnregisterInt ( uint32_t  base)

Unregisters an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table.

This function will clear the handler to be called when a SPI interrupt occurs. This will also mask off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

Parameters
basespecifies the SPI module base address.
Returns
None
See also
IntRegister() for important information about registering interrupt handlers.

References ASSERT, IntDisable(), and IntUnregister().

Referenced by SPIStatus().

§ SPIEnableInt()

__STATIC_INLINE void SPIEnableInt ( uint32_t  base,
uint32_t  intFlags 
)

Enables individual SPI interrupt sources.

Enables the indicated SPI interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
basespecifies the SPI module base address.
intFlagsis a bit mask of the interrupt sources to be enabled.
Returns
None

References ASSERT.

§ SPIDisableInt()

__STATIC_INLINE void SPIDisableInt ( uint32_t  base,
uint32_t  intFlags 
)

Disables individual SPI interrupt sources.

Disables the indicated SPI interrupt sources.

Parameters
basespecifies the SPI module base address.
intFlagsis a bit mask of the interrupt sources to be disabled.
Returns
None

References ASSERT.

§ SPIClearInt()

__STATIC_INLINE void SPIClearInt ( uint32_t  base,
uint32_t  intFlags 
)

Clears SPI interrupt sources.

The specified SPI interrupt sources are cleared so that they no longer assert. This function must be called in the interrupt handler to keep the interrupts from being recognized again immediately upon exit.

Note
Due to write buffers and synchronizers in the system it may take several clock cycles from a register write clearing an event in a module and until the event is actually cleared in the NVIC of the system CPU. It is recommended to clear the event source early in the interrupt service routine (ISR) to allow the event clear to propagate to the NVIC before returning from the ISR. At the same time, an early event clear allows new events of the same type to be pended instead of ignored if the event is cleared later in the ISR. It is the responsibility of the programmer to make sure that enough time has passed before returning from the ISR to avoid false re-triggering of the cleared event. A simple, although not necessarily optimal, way of clearing an event before returning from the ISR is:
  1. Write to clear event (interrupt source). (buffered write)
  2. Dummy read from the event source module. (making sure the write has propagated)
  3. Wait two system CPU clock cycles (user code or two NOPs), (allowing cleared event to propagate through any synchronizers)
Parameters
basespecifies the SPI module base address.
intFlagsis a bit mask of the interrupt sources to be cleared. The parameter can consist of either or both of:
Returns
None

References ASSERT.

§ SPIIntStatus()

__STATIC_INLINE uint32_t SPIIntStatus ( uint32_t  base,
bool  isMasked 
)

Gets the current interrupt status.

This function returns the interrupt status for the SPI module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.

Parameters
basespecifies the SPI module base address.
isMaskedselects either raw or masked interrupt. false : Raw interrupt status is required. true : Masked interrupt status is required.
Returns
Returns the current interrupt status as an OR'ed combination of:

References ASSERT.

§ SPIEnableDMA()

__STATIC_INLINE void SPIEnableDMA ( uint32_t  base,
uint32_t  dmaFlags 
)

Enable SPI DMA operation.

The specified SPI DMA features are enabled. The SPI can be configured to use DMA for transmit and/or receive data transfers.

Note
The uDMA controller must also be set up before DMA can be used with the SPI.
Parameters
baseis the base address of the SPI port.
dmaFlagsis a bit mask of the DMA features to enable. The parameter is the bitwise OR of any of the following values:
Returns
None

References ASSERT.

§ SPIDisableDMA()

__STATIC_INLINE void SPIDisableDMA ( uint32_t  base,
uint32_t  dmaFlags 
)

Disable SPI DMA operation.

This function is used to disable SPI DMA features that were enabled by SPIEnableDMA(). The specified SPI DMA features are disabled.

Parameters
baseis the base address of the SPI port.
dmaFlagsis a bit mask of the DMA features to disable. The parameter is the bitwise OR of any of the following values:
Returns
None

References ASSERT.