CC23x0R5DriverLibrary
adc.c File Reference
#include "adc.h"
#include "debug.h"
Include dependency graph for adc.c:

Functions

void ADCSetSampleDuration (uint32_t clkDiv, uint16_t clkCycles)
 Sets the clock-divider value, and sample duration. More...
 
void ADCSetResolution (uint32_t resolution)
 Sets the ADC bit resolution. More...
 
void ADCSetInput (uint32_t reference, uint8_t channel, uint32_t index)
 Sets the ADC reference source and input channel. More...
 
void ADCSetSamplingMode (uint32_t samplingMode)
 Set ADC sampling mode. More...
 
void ADCSetTriggerSource (uint32_t triggerSource)
 Set ADC trigger source. More...
 
void ADCSetTriggerPolicy (uint32_t triggerPolicy, uint32_t index)
 Set ADC trigger policy. More...
 
void ADCSetMemctlRange (uint32_t start, uint32_t stop)
 Set start and stop control registers. More...
 
void ADCSetPowerDownPolicy (uint32_t powerDownPolicy)
 Set power down policy. More...
 
void ADCSetSequence (uint32_t sequence)
 Set conversion sequence. More...
 
uint32_t ADCAdjustValueForGain (uint32_t adcValue, uint32_t bitResolution, uint16_t gain)
 Performs ADC value gain adjustment. More...
 
uint32_t ADCValueToMicrovolts (uint32_t adcCode, uint32_t bitResolution, uint32_t referenceVoltageMicroVolt)
 Convert ADC code to microvolts. More...
 
uint16_t ADCGetAdjustmentGain (uint32_t reference)
 Returns ADC gain value for given reference. More...
 
void ADCSetAdjustmentOffset (uint32_t reference)
 Write correct offset value to ADC-peripheral trim register. More...