![]() |
![]() |
|
CC23x0r2DriverLibrary
|
Definitions common across all SHA2 SW modules.
============================================================================
Provides top-level general purpose SHA2 SW definitions such as error return codes and enumerations.


Go to the source code of this file.
Macros | |
| #define | SHA2SW_224_OR_256_ROUNDS ((uint8_t)64u) |
| Number of rounds used in the SHA2 224 and 256 algorithms. More... | |
| #define | SHA2SW_384_OR_512_ROUNDS ((uint8_t)80u) |
| Number of rounds used in the SHA2 384 and 512 algorithms. More... | |
| #define | SHA2SW_224_OR_256_BLOCK_SIZE ((uint8_t)64u) |
| Number of bytes in the block of the SHA2 224 and 256 algorithms. More... | |
| #define | SHA2SW_384_OR_512_BLOCK_SIZE ((uint8_t)128u) |
| Number of bytes in the block of the SHA2 384 and 512 algorithms. More... | |
| #define | SHA2SW_MAX_MESSAGE_BIT_LENGTH ((uint32_t)0x20000000u) |
| The maximum number of bits this implementation supports in the input message/data. More... | |
| #define | SHA2SW_STATUS_SUCCESS ((int_fast16_t)0) |
| Successful status code. More... | |
| #define | SHA2SW_STATUS_ERROR ((int_fast16_t)-100) |
| Generic error status code. More... | |
| #define | SHA2SW_STATUS_UNSUPPORTED ((int_fast16_t)-102) |
| Requested operation is not supported. More... | |
| #define | SHA2SW_STATUS_LENGTH_TOO_LARGE ((int_fast16_t)-103) |
| Too many data bytes have been requested to be hashed. More... | |
| #define | SHA2SW_STATUS_NULL_INPUT ((int_fast16_t)-104) |
| Input value was NULL. More... | |
Enumerations | |
| enum | SHA2SW_HashType { SHA2SW_HASH_TYPE_256 = 0, SHA2SW_HASH_TYPE_512 = 3 } |
| Enum for the hash types supported by the library. More... | |
| #define SHA2SW_224_OR_256_ROUNDS ((uint8_t)64u) |
Number of rounds used in the SHA2 224 and 256 algorithms.
| #define SHA2SW_384_OR_512_ROUNDS ((uint8_t)80u) |
Number of rounds used in the SHA2 384 and 512 algorithms.
| #define SHA2SW_224_OR_256_BLOCK_SIZE ((uint8_t)64u) |
Number of bytes in the block of the SHA2 224 and 256 algorithms.
| #define SHA2SW_384_OR_512_BLOCK_SIZE ((uint8_t)128u) |
Number of bytes in the block of the SHA2 384 and 512 algorithms.
| #define SHA2SW_MAX_MESSAGE_BIT_LENGTH ((uint32_t)0x20000000u) |
The maximum number of bits this implementation supports in the input message/data.
| enum SHA2SW_HashType |