![]() |
![]() |
|
CC23x0r2DriverLibrary
|
#include "interrupt.h"#include "cpu.h"#include "debug.h"#include "../inc/hw_ints.h"#include "../inc/hw_types.h"#include "../cmsis/core/core_cm0plus.h"
Functions | |
| static void | IntDefaultHandler (void) |
| The default interrupt handler. More... | |
| static | __attribute__ ((section(".ramVecs"), aligned(256))) |
| Global pointer to the (dynamic) interrupt vector table when placed in SRAM. More... | |
| void | IntUnregister (uint32_t intNum) |
| Unregisters an interrupt handler in the dynamic vector table. More... | |
| void | IntSetPriority (uint32_t intNum, uint8_t priority) |
| Sets the priority of an interrupt. More... | |
| int32_t | IntGetPriority (uint32_t intNum) |
| Gets the priority of an interrupt. More... | |
| bool | IntIsEnabled (uint32_t intNum) |
| Check whether an interrupt is enabled. More... | |
| void | IntEnable (uint32_t intNum) |
| Enables an interrupt or system exception. More... | |
| void | IntDisable (uint32_t intNum) |
| Disables an interrupt or system exception. More... | |
| void | IntSetPend (uint32_t intNum) |
| Pends an interrupt. More... | |
| bool | IntGetPend (uint32_t intNum) |
| Checks if an interrupt is pending. More... | |
| void | IntClearPend (uint32_t intNum) |
| Unpends an interrupt. More... | |
|
static |
The default interrupt handler.
This is the default interrupt handler for all interrupts. It simply loops forever so that the system state is preserved for observation by a debugger. Since interrupts should be disabled before unregistering the corresponding handler, this should never be called.
References __attribute__().
Referenced by IntUnregister().
|
static |
Global pointer to the (dynamic) interrupt vector table when placed in SRAM.
Interrupt vector table is placed at ".ramVecs" defined in the linker file provided by Texas Instruments.
interrupt.c for compiler specific implementation! Referenced by IntDefaultHandler().