![]() |
![]() |
|
CC23x0r2DriverLibrary
|
|
Functions | |
| void | I2CControllerInitExpClk (uint32_t base, bool fast) |
| Initializes the I2C Controller module. More... | |
| __STATIC_INLINE void | I2CControllerCommand (uint32_t base, uint32_t cmd) |
| Controls the state of the I2C Controller module. More... | |
| __STATIC_INLINE void | I2CControllerSetTargetAddr (uint32_t base, uint8_t targetAddr, bool receive) |
| Sets the address that the I2C Controller will place on the bus. More... | |
| __STATIC_INLINE void | I2CControllerEnable (uint32_t base) |
| Enables the I2C Controller module. More... | |
| __STATIC_INLINE void | I2CControllerDisable (uint32_t base) |
| Disables the I2C controller module. More... | |
| __STATIC_INLINE bool | I2CControllerBusy (uint32_t base) |
| Indicates whether or not the I2C Controller is busy. More... | |
| __STATIC_INLINE bool | I2CControllerBusBusy (uint32_t base) |
| Indicates whether or not the I2C bus is busy. More... | |
| __STATIC_INLINE uint32_t | I2CControllerGetData (uint32_t base) |
| Receives a byte that has been sent to the I2C Controller. More... | |
| __STATIC_INLINE void | I2CControllerPutData (uint32_t base, uint8_t data) |
| Transmits a byte from the I2C Controller. More... | |
| uint32_t | I2CControllerError (uint32_t base) |
| Gets the error status of the I2C Controller module. More... | |
| __STATIC_INLINE void | I2CControllerEnableInt (uint32_t base) |
| Enables the I2C Controller interrupt. More... | |
| __STATIC_INLINE void | I2CControllerDisableInt (uint32_t base) |
| Disables the I2C Controller interrupt. More... | |
| __STATIC_INLINE void | I2CControllerClearInt (uint32_t base) |
| Clears I2C Controller interrupt sources. More... | |
| __STATIC_INLINE bool | I2CControllerIntStatus (uint32_t base, bool masked) |
| Gets the current I2C Controller interrupt status. More... | |
| __STATIC_INLINE void | I2CTargetEnable (uint32_t base) |
| Enables the I2C Target module. More... | |
| __STATIC_INLINE void | I2CTargetInit (uint32_t base, uint8_t targetAddr) |
| Initializes the I2C Target module. More... | |
| __STATIC_INLINE void | I2CTargetSetAddress (uint32_t base, uint8_t targetAddr) |
| Sets the I2C target address. More... | |
| __STATIC_INLINE void | I2CTargetDisable (uint32_t base) |
| Disables the I2C target module. More... | |
| __STATIC_INLINE uint32_t | I2CTargetStatus (uint32_t base) |
| Gets the I2C Target module status. More... | |
| __STATIC_INLINE uint32_t | I2CTargetGetData (uint32_t base) |
| Receives a byte that has been sent to the I2C Target. More... | |
| __STATIC_INLINE void | I2CTargetPutData (uint32_t base, uint8_t data) |
| Transmits a byte from the I2C Target. More... | |
| __STATIC_INLINE void | I2CTargetEnableInt (uint32_t base, uint32_t intFlags) |
| Enables individual I2C Target interrupt sources. More... | |
| __STATIC_INLINE void | I2CTargetDisableInt (uint32_t base, uint32_t intFlags) |
| Disables individual I2C Target interrupt sources. More... | |
| __STATIC_INLINE void | I2CTargetClearInt (uint32_t base, uint32_t intFlags) |
| Clears I2C Target interrupt sources. More... | |
| __STATIC_INLINE uint32_t | I2CTargetIntStatus (uint32_t base, bool masked) |
| Gets the current I2C Target interrupt status. More... | |
| #define I2C_CONTROLLER_CMD_SINGLE_SEND 0x00000007 |
Referenced by I2CControllerCommand().
| #define I2C_CONTROLLER_CMD_SINGLE_RECEIVE 0x00000007 |
| #define I2C_CONTROLLER_CMD_BURST_SEND_START 0x00000003 |
Referenced by I2CControllerCommand().
| #define I2C_CONTROLLER_CMD_BURST_SEND_CONT 0x00000001 |
Referenced by I2CControllerCommand().
| #define I2C_CONTROLLER_CMD_BURST_SEND_FINISH 0x00000005 |
Referenced by I2CControllerCommand().
| #define I2C_CONTROLLER_CMD_BURST_SEND_ERROR_STOP 0x00000004 |
Referenced by I2CControllerCommand().
| #define I2C_CONTROLLER_CMD_BURST_RECEIVE_START 0x0000000b |
Referenced by I2CControllerCommand().
| #define I2C_CONTROLLER_CMD_BURST_RECEIVE_CONT 0x00000009 |
Referenced by I2CControllerCommand().
| #define I2C_CONTROLLER_CMD_BURST_RECEIVE_FINISH 0x00000005 |
Referenced by I2CControllerCommand().
| #define I2C_CONTROLLER_CMD_BURST_RECEIVE_ERROR_STOP 0x00000004 |
Referenced by I2CControllerCommand().
| #define I2C_CONTROLLER_ERR_NONE 0 |
Referenced by I2CControllerError().
| #define I2C_CONTROLLER_ERR_ADDR_ACK 0x00000004 |
| #define I2C_CONTROLLER_ERR_DATA_ACK 0x00000008 |
| #define I2C_CONTROLLER_ERR_ARB_LOST 0x00000010 |
| #define I2C_TARGET_ACT_NONE 0 |
| #define I2C_TARGET_ACT_RREQ 0x00000001 |
| #define I2C_TARGET_ACT_TREQ 0x00000002 |
| #define I2C_TARGET_ACT_RREQ_FBR 0x00000005 |
| #define I2C_TARGET_INT_STOP 0x00000004 |
Referenced by I2CTargetDisableInt(), and I2CTargetEnableInt().
| #define I2C_TARGET_INT_START 0x00000002 |
Referenced by I2CTargetDisableInt(), and I2CTargetEnableInt().
| #define I2C_TARGET_INT_DATA 0x00000001 |
Referenced by I2CTargetDisableInt(), and I2CTargetEnableInt().
| #define I2C_CLK_FREQ 48000000 |
Referenced by I2CControllerInitExpClk().
| void I2CControllerInitExpClk | ( | uint32_t | base, |
| bool | fast | ||
| ) |
Initializes the I2C Controller module.
This function initializes operation of the I2C Controller module. Upon successful initialization of the I2C module, this function will have set the bus speed for the controller, and will have enabled the I2C Controller module.
If the parameter fast is true, then the controller module will be set up to transfer data at 400 kbps; otherwise, it will be set up to transfer data at 100 kbps.
| base | is the base address of the I2C module. |
| fast | set up for fast data transfers. |
References ASSERT, I2C_CLK_FREQ, and I2CControllerEnable().
| __STATIC_INLINE void I2CControllerCommand | ( | uint32_t | base, |
| uint32_t | cmd | ||
| ) |
Controls the state of the I2C Controller module.
This function is used to control the state of the Controller module send and receive operations.
| base | is the base address of the I2C module. |
| cmd | is the command to be issued by the I2C Controller module The parameter can be one of the following values:
|
References ASSERT, CPUDelay(), I2C_CONTROLLER_CMD_BURST_RECEIVE_CONT, I2C_CONTROLLER_CMD_BURST_RECEIVE_ERROR_STOP, I2C_CONTROLLER_CMD_BURST_RECEIVE_FINISH, I2C_CONTROLLER_CMD_BURST_RECEIVE_START, I2C_CONTROLLER_CMD_BURST_SEND_CONT, I2C_CONTROLLER_CMD_BURST_SEND_ERROR_STOP, I2C_CONTROLLER_CMD_BURST_SEND_FINISH, I2C_CONTROLLER_CMD_BURST_SEND_START, and I2C_CONTROLLER_CMD_SINGLE_SEND.
| __STATIC_INLINE void I2CControllerSetTargetAddr | ( | uint32_t | base, |
| uint8_t | targetAddr, | ||
| bool | receive | ||
| ) |
Sets the address that the I2C Controller will place on the bus.
This function will set the address that the I2C Controller will place on the bus when initiating a transaction. When the receive parameter is set to true, the address will indicate that the I2C Controller is initiating a read from the target; otherwise the address will indicate that the I2C Controller is initiating a write to the target.
| base | is the base address of the I2C module. |
| targetAddr | is a 7-bit target address |
| receive | flag indicates the type of communication with the target.
|
References ASSERT.
| __STATIC_INLINE void I2CControllerEnable | ( | uint32_t | base | ) |
Enables the I2C Controller module.
This will enable operation of the I2C Controller module.
| base | is the base address of the I2C module. |
References ASSERT.
Referenced by I2CControllerInitExpClk().
| __STATIC_INLINE void I2CControllerDisable | ( | uint32_t | base | ) |
Disables the I2C controller module.
This will disable operation of the I2C controller module.
| base | is the base address of the I2C module. |
References ASSERT.
| __STATIC_INLINE bool I2CControllerBusy | ( | uint32_t | base | ) |
Indicates whether or not the I2C Controller is busy.
This function returns an indication of whether or not the I2C Controller is busy transmitting or receiving data.
| base | is the base address of the I2C module. |
true : I2C Controller is busy.false : I2C Controller is not busy. References ASSERT.
| __STATIC_INLINE bool I2CControllerBusBusy | ( | uint32_t | base | ) |
Indicates whether or not the I2C bus is busy.
This function returns an indication of whether or not the I2C bus is busy. This function can be used in a multi-controller environment to determine if another controller is currently using the bus.
| base | is the base address of the I2C module. |
true : I2C bus is busy.false : I2C bus is not busy. References ASSERT.
| __STATIC_INLINE uint32_t I2CControllerGetData | ( | uint32_t | base | ) |
Receives a byte that has been sent to the I2C Controller.
This function reads a byte of data from the I2C Controller Data Register.
| base | is the base address of the I2C module. |
References ASSERT.
| __STATIC_INLINE void I2CControllerPutData | ( | uint32_t | base, |
| uint8_t | data | ||
| ) |
Transmits a byte from the I2C Controller.
This function will place the supplied data into I2C Controller Data Register.
| base | is the base address of the I2C module. |
| data | is the data to be transmitted by the I2C Controller |
References ASSERT, and I2CControllerError().
| uint32_t I2CControllerError | ( | uint32_t | base | ) |
Gets the error status of the I2C Controller module.
This function is used to obtain the error status of the Controller module send and receive operations.
| base | is the base address of the I2C module. |
References ASSERT, and I2C_CONTROLLER_ERR_NONE.
Referenced by I2CControllerPutData().
| __STATIC_INLINE void I2CControllerEnableInt | ( | uint32_t | base | ) |
Enables the I2C Controller interrupt.
Enables the I2C Controller interrupt source.
| base | is the base address of the I2C module. |
References ASSERT.
| __STATIC_INLINE void I2CControllerDisableInt | ( | uint32_t | base | ) |
Disables the I2C Controller interrupt.
Disables the I2C Controller interrupt source.
| base | is the base address of the I2C module. |
References ASSERT.
| __STATIC_INLINE void I2CControllerClearInt | ( | uint32_t | base | ) |
Clears I2C Controller interrupt sources.
The I2C Controller interrupt source is cleared, so that it no longer asserts. This must be done in the interrupt handler to keep it from being called again immediately upon exit.
| base | is the base address of the I2C module. |
References ASSERT.
| __STATIC_INLINE bool I2CControllerIntStatus | ( | uint32_t | base, |
| bool | masked | ||
| ) |
Gets the current I2C Controller interrupt status.
This returns the interrupt status for the I2C Controller module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
| base | is the base address of the I2C Controller module. |
| masked | selects either raw or masked interrupt status.
|
true : Active.false : Not active. References ASSERT.
| __STATIC_INLINE void I2CTargetEnable | ( | uint32_t | base | ) |
Enables the I2C Target module.
This will enable operation of the I2C Target module.
| base | is the base address of the I2C Target module. |
References ASSERT.
Referenced by I2CTargetInit().
| __STATIC_INLINE void I2CTargetInit | ( | uint32_t | base, |
| uint8_t | targetAddr | ||
| ) |
Initializes the I2C Target module.
This function initializes operation of the I2C Target module. Upon successful initialization of the I2C module, this function will have set the target address and have enabled the I2C Target module.
The parameter targetAddr is the value that will be compared against the target address sent by an I2C controller.
| base | is the base address of the I2C Target module. |
| targetAddr | is the 7-bit target address. |
References ASSERT, and I2CTargetEnable().
| __STATIC_INLINE void I2CTargetSetAddress | ( | uint32_t | base, |
| uint8_t | targetAddr | ||
| ) |
Sets the I2C target address.
This function writes the specified target address.
| base | is the base address of the I2C Target module. |
| targetAddr | is the 7-bit target address |
References ASSERT.
| __STATIC_INLINE void I2CTargetDisable | ( | uint32_t | base | ) |
Disables the I2C target module.
This will disable operation of the I2C target module.
| base | is the base address of the I2C Target module. |
References ASSERT.
| __STATIC_INLINE uint32_t I2CTargetStatus | ( | uint32_t | base | ) |
Gets the I2C Target module status.
This function will return the action requested from a controller, if any.
| base | is the base address of the I2C Target module. |
References ASSERT.
| __STATIC_INLINE uint32_t I2CTargetGetData | ( | uint32_t | base | ) |
Receives a byte that has been sent to the I2C Target.
This function reads a byte of data from the I2C Target Data Register.
| base | is the base address of the I2C Target module. |
References ASSERT.
| __STATIC_INLINE void I2CTargetPutData | ( | uint32_t | base, |
| uint8_t | data | ||
| ) |
Transmits a byte from the I2C Target.
This function will place the supplied data into I2C Target Data Register.
| base | is the base address of the I2C Target module. |
| data | data to be transmitted from the I2C Target. |
References ASSERT.
| __STATIC_INLINE void I2CTargetEnableInt | ( | uint32_t | base, |
| uint32_t | intFlags | ||
| ) |
Enables individual I2C Target interrupt sources.
Enables the indicated I2C Target interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| base | is the base address of the I2C module. |
| intFlags | is the bit mask of the target interrupt sources to be enabled. The parameter is the bitwise OR of any of the following: |
References ASSERT, I2C_TARGET_INT_DATA, I2C_TARGET_INT_START, and I2C_TARGET_INT_STOP.
| __STATIC_INLINE void I2CTargetDisableInt | ( | uint32_t | base, |
| uint32_t | intFlags | ||
| ) |
Disables individual I2C Target interrupt sources.
Disables the indicated I2C Target interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| base | is the base address of the I2C Target module. |
| intFlags | is the bit mask of the interrupt sources to be disabled. The parameter is the bitwise OR of any of the following: |
References ASSERT, I2C_TARGET_INT_DATA, I2C_TARGET_INT_START, and I2C_TARGET_INT_STOP.
| __STATIC_INLINE void I2CTargetClearInt | ( | uint32_t | base, |
| uint32_t | intFlags | ||
| ) |
Clears I2C Target interrupt sources.
The specified I2C Target interrupt sources are cleared, so that they no longer assert. This must be done in the interrupt handler to keep it from being called again immediately upon exit.
| base | is the base address of the I2C module. |
| intFlags | is a bit mask of the interrupt sources to be cleared. The parameter is the bitwise OR of any of the following: |
References ASSERT.
| __STATIC_INLINE uint32_t I2CTargetIntStatus | ( | uint32_t | base, |
| bool | masked | ||
| ) |
Gets the current I2C Target interrupt status.
This returns the interrupt status for the I2C Target module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
| base | is the base address of the I2C Target module. |
| masked | selects either raw or masked interrupt status.
|
References ASSERT.