CC23x0r2DriverLibrary

Functions that manage interrupts and exceptions via the NVIC. More...

Collaboration diagram for NVIC Functions:

Macros

#define NVIC_SetPriorityGrouping   __NVIC_SetPriorityGrouping
 
#define NVIC_GetPriorityGrouping   __NVIC_GetPriorityGrouping
 
#define NVIC_EnableIRQ   __NVIC_EnableIRQ
 
#define NVIC_GetEnableIRQ   __NVIC_GetEnableIRQ
 
#define NVIC_DisableIRQ   __NVIC_DisableIRQ
 
#define NVIC_GetPendingIRQ   __NVIC_GetPendingIRQ
 
#define NVIC_SetPendingIRQ   __NVIC_SetPendingIRQ
 
#define NVIC_ClearPendingIRQ   __NVIC_ClearPendingIRQ
 
#define NVIC_SetPriority   __NVIC_SetPriority
 
#define NVIC_GetPriority   __NVIC_GetPriority
 
#define NVIC_SystemReset   __NVIC_SystemReset
 
#define NVIC_SetVector   __NVIC_SetVector
 
#define NVIC_GetVector   __NVIC_GetVector
 
#define NVIC_USER_IRQ_OFFSET   16
 
#define EXC_RETURN_HANDLER   (0xFFFFFFF1UL) /* return to Handler mode, uses MSP after return */
 
#define EXC_RETURN_THREAD_MSP   (0xFFFFFFF9UL) /* return to Thread mode, uses MSP after return */
 
#define EXC_RETURN_THREAD_PSP   (0xFFFFFFFDUL) /* return to Thread mode, uses PSP after return */
 
#define _BIT_SHIFT(IRQn)   ( ((((uint32_t)(int32_t)(IRQn)) ) & 0x03UL) * 8UL)
 
#define _SHP_IDX(IRQn)   ( (((((uint32_t)(int32_t)(IRQn)) & 0x0FUL)-8UL) >> 2UL) )
 
#define _IP_IDX(IRQn)   ( (((uint32_t)(int32_t)(IRQn)) >> 2UL) )
 
#define __NVIC_SetPriorityGrouping(X)   (void)(X)
 
#define __NVIC_GetPriorityGrouping()   (0U)
 

Functions

__STATIC_INLINE void __NVIC_EnableIRQ (IRQn_Type IRQn)
 Enable Interrupt. More...
 
__STATIC_INLINE uint32_t __NVIC_GetEnableIRQ (IRQn_Type IRQn)
 Get Interrupt Enable status. More...
 
__STATIC_INLINE void __NVIC_DisableIRQ (IRQn_Type IRQn)
 Disable Interrupt. More...
 
__STATIC_INLINE uint32_t __NVIC_GetPendingIRQ (IRQn_Type IRQn)
 Get Pending Interrupt. More...
 
__STATIC_INLINE void __NVIC_SetPendingIRQ (IRQn_Type IRQn)
 Set Pending Interrupt. More...
 
__STATIC_INLINE void __NVIC_ClearPendingIRQ (IRQn_Type IRQn)
 Clear Pending Interrupt. More...
 
__STATIC_INLINE void __NVIC_SetPriority (IRQn_Type IRQn, uint32_t priority)
 Set Interrupt Priority. More...
 
__STATIC_INLINE uint32_t __NVIC_GetPriority (IRQn_Type IRQn)
 Get Interrupt Priority. More...
 
__STATIC_INLINE uint32_t NVIC_EncodePriority (uint32_t PriorityGroup, uint32_t PreemptPriority, uint32_t SubPriority)
 Encode Priority. More...
 
__STATIC_INLINE void NVIC_DecodePriority (uint32_t Priority, uint32_t PriorityGroup, uint32_t *const pPreemptPriority, uint32_t *const pSubPriority)
 Decode Priority. More...
 
__STATIC_INLINE void __NVIC_SetVector (IRQn_Type IRQn, uint32_t vector)
 Set Interrupt Vector. More...
 
__STATIC_INLINE uint32_t __NVIC_GetVector (IRQn_Type IRQn)
 Get Interrupt Vector. More...
 
__NO_RETURN __STATIC_INLINE void __NVIC_SystemReset (void)
 System Reset. More...
 

Detailed Description

Functions that manage interrupts and exceptions via the NVIC.

Macro Definition Documentation

§ NVIC_SetPriorityGrouping

#define NVIC_SetPriorityGrouping   __NVIC_SetPriorityGrouping

§ NVIC_GetPriorityGrouping

#define NVIC_GetPriorityGrouping   __NVIC_GetPriorityGrouping

§ NVIC_EnableIRQ

#define NVIC_EnableIRQ   __NVIC_EnableIRQ

§ NVIC_GetEnableIRQ

#define NVIC_GetEnableIRQ   __NVIC_GetEnableIRQ

§ NVIC_DisableIRQ

#define NVIC_DisableIRQ   __NVIC_DisableIRQ

§ NVIC_GetPendingIRQ

#define NVIC_GetPendingIRQ   __NVIC_GetPendingIRQ

§ NVIC_SetPendingIRQ

#define NVIC_SetPendingIRQ   __NVIC_SetPendingIRQ

§ NVIC_ClearPendingIRQ

#define NVIC_ClearPendingIRQ   __NVIC_ClearPendingIRQ

§ NVIC_SetPriority

#define NVIC_SetPriority   __NVIC_SetPriority

Referenced by SCB_GetFPUType().

§ NVIC_GetPriority

#define NVIC_GetPriority   __NVIC_GetPriority

§ NVIC_SystemReset

#define NVIC_SystemReset   __NVIC_SystemReset

§ NVIC_SetVector

#define NVIC_SetVector   __NVIC_SetVector

§ NVIC_GetVector

#define NVIC_GetVector   __NVIC_GetVector

§ NVIC_USER_IRQ_OFFSET

#define NVIC_USER_IRQ_OFFSET   16

§ EXC_RETURN_HANDLER

#define EXC_RETURN_HANDLER   (0xFFFFFFF1UL) /* return to Handler mode, uses MSP after return */

§ EXC_RETURN_THREAD_MSP

#define EXC_RETURN_THREAD_MSP   (0xFFFFFFF9UL) /* return to Thread mode, uses MSP after return */

§ EXC_RETURN_THREAD_PSP

#define EXC_RETURN_THREAD_PSP   (0xFFFFFFFDUL) /* return to Thread mode, uses PSP after return */

§ _BIT_SHIFT

#define _BIT_SHIFT (   IRQn)    ( ((((uint32_t)(int32_t)(IRQn)) ) & 0x03UL) * 8UL)

§ _SHP_IDX

#define _SHP_IDX (   IRQn)    ( (((((uint32_t)(int32_t)(IRQn)) & 0x0FUL)-8UL) >> 2UL) )

§ _IP_IDX

#define _IP_IDX (   IRQn)    ( (((uint32_t)(int32_t)(IRQn)) >> 2UL) )

§ __NVIC_SetPriorityGrouping

#define __NVIC_SetPriorityGrouping (   X)    (void)(X)

§ __NVIC_GetPriorityGrouping

#define __NVIC_GetPriorityGrouping ( )    (0U)

Function Documentation

§ __NVIC_EnableIRQ()

__STATIC_INLINE void __NVIC_EnableIRQ ( IRQn_Type  IRQn)

Enable Interrupt.

Enables a device specific interrupt in the NVIC interrupt controller.

Parameters
[in]IRQnDevice specific interrupt number.
Note
IRQn must not be negative.

References __COMPILER_BARRIER, and NVIC.

§ __NVIC_GetEnableIRQ()

__STATIC_INLINE uint32_t __NVIC_GetEnableIRQ ( IRQn_Type  IRQn)

Get Interrupt Enable status.

Returns a device specific interrupt enable status from the NVIC interrupt controller.

Parameters
[in]IRQnDevice specific interrupt number.
Returns
0 Interrupt is not enabled.
1 Interrupt is enabled.
Note
IRQn must not be negative.

References NVIC.

§ __NVIC_DisableIRQ()

__STATIC_INLINE void __NVIC_DisableIRQ ( IRQn_Type  IRQn)

Disable Interrupt.

Disables a device specific interrupt in the NVIC interrupt controller.

Parameters
[in]IRQnDevice specific interrupt number.
Note
IRQn must not be negative.

References __DSB(), __ISB(), and NVIC.

§ __NVIC_GetPendingIRQ()

__STATIC_INLINE uint32_t __NVIC_GetPendingIRQ ( IRQn_Type  IRQn)

Get Pending Interrupt.

Reads the NVIC pending register and returns the pending bit for the specified device specific interrupt.

Parameters
[in]IRQnDevice specific interrupt number.
Returns
0 Interrupt status is not pending.
1 Interrupt status is pending.
Note
IRQn must not be negative.

References NVIC.

§ __NVIC_SetPendingIRQ()

__STATIC_INLINE void __NVIC_SetPendingIRQ ( IRQn_Type  IRQn)

Set Pending Interrupt.

Sets the pending bit of a device specific interrupt in the NVIC pending register.

Parameters
[in]IRQnDevice specific interrupt number.
Note
IRQn must not be negative.

References NVIC.

§ __NVIC_ClearPendingIRQ()

__STATIC_INLINE void __NVIC_ClearPendingIRQ ( IRQn_Type  IRQn)

Clear Pending Interrupt.

Clears the pending bit of a device specific interrupt in the NVIC pending register.

Parameters
[in]IRQnDevice specific interrupt number.
Note
IRQn must not be negative.

References NVIC.

§ __NVIC_SetPriority()

__STATIC_INLINE void __NVIC_SetPriority ( IRQn_Type  IRQn,
uint32_t  priority 
)

Set Interrupt Priority.

Sets the priority of a device specific interrupt or a processor exception. The interrupt number can be positive to specify a device specific interrupt, or negative to specify a processor exception.

Parameters
[in]IRQnInterrupt number.
[in]priorityPriority to set.
Note
The priority cannot be set for every processor exception.

References __NVIC_PRIO_BITS, _BIT_SHIFT, _IP_IDX, _SHP_IDX, NVIC, and SCB.

§ __NVIC_GetPriority()

__STATIC_INLINE uint32_t __NVIC_GetPriority ( IRQn_Type  IRQn)

Get Interrupt Priority.

Reads the priority of a device specific interrupt or a processor exception. The interrupt number can be positive to specify a device specific interrupt, or negative to specify a processor exception.

Parameters
[in]IRQnInterrupt number.
Returns
Interrupt Priority. Value is aligned automatically to the implemented priority bits of the microcontroller.

References __NVIC_PRIO_BITS, _BIT_SHIFT, _IP_IDX, _SHP_IDX, NVIC, and SCB.

§ NVIC_EncodePriority()

__STATIC_INLINE uint32_t NVIC_EncodePriority ( uint32_t  PriorityGroup,
uint32_t  PreemptPriority,
uint32_t  SubPriority 
)

Encode Priority.

Encodes the priority for an interrupt with the given priority group, preemptive priority value, and subpriority value. In case of a conflict between priority grouping and available priority bits (__NVIC_PRIO_BITS), the smallest possible priority group is set.

Parameters
[in]PriorityGroupUsed priority group.
[in]PreemptPriorityPreemptive priority value (starting from 0).
[in]SubPrioritySubpriority value (starting from 0).
Returns
Encoded priority. Value can be used in the function NVIC_SetPriority().

References __NVIC_PRIO_BITS.

§ NVIC_DecodePriority()

__STATIC_INLINE void NVIC_DecodePriority ( uint32_t  Priority,
uint32_t  PriorityGroup,
uint32_t *const  pPreemptPriority,
uint32_t *const  pSubPriority 
)

Decode Priority.

Decodes an interrupt priority value with a given priority group to preemptive priority value and subpriority value. In case of a conflict between priority grouping and available priority bits (__NVIC_PRIO_BITS) the smallest possible priority group is set.

Parameters
[in]PriorityPriority value, which can be retrieved with the function NVIC_GetPriority().
[in]PriorityGroupUsed priority group.
[out]pPreemptPriorityPreemptive priority value (starting from 0).
[out]pSubPrioritySubpriority value (starting from 0).

References __NVIC_PRIO_BITS.

§ __NVIC_SetVector()

__STATIC_INLINE void __NVIC_SetVector ( IRQn_Type  IRQn,
uint32_t  vector 
)

Set Interrupt Vector.

Sets an interrupt vector in SRAM based interrupt vector table. The interrupt number can be positive to specify a device specific interrupt, or negative to specify a processor exception. VTOR must been relocated to SRAM before. If VTOR is not present address 0 must be mapped to SRAM.

Parameters
[in]IRQnInterrupt number
[in]vectorAddress of interrupt handler function

References NVIC_USER_IRQ_OFFSET, and SCB.

§ __NVIC_GetVector()

__STATIC_INLINE uint32_t __NVIC_GetVector ( IRQn_Type  IRQn)

Get Interrupt Vector.

Reads an interrupt vector from interrupt vector table. The interrupt number can be positive to specify a device specific interrupt, or negative to specify a processor exception.

Parameters
[in]IRQnInterrupt number.
Returns
Address of interrupt handler function

References NVIC_USER_IRQ_OFFSET, and SCB.

§ __NVIC_SystemReset()

__NO_RETURN __STATIC_INLINE void __NVIC_SystemReset ( void  )

System Reset.

Initiates a system reset request to reset the MCU.

References __DSB(), __NOP, SCB, SCB_AIRCR_SYSRESETREQ_Msk, and SCB_AIRCR_VECTKEY_Pos.