![]() |
![]() |
|
CC23x0r2DriverLibrary
|
#include <stdint.h>#include "../inc/hw_adc.h"#include "../inc/hw_fcfg.h"#include "../inc/hw_memmap.h"#include "../inc/hw_sys0.h"#include "../inc/hw_types.h"

Go to the source code of this file.
Macros | |
| #define | ADC_CLOCK_DIVIDER_1 ADC_CTL0_SCLKDIV_DIV_BY_1 |
| Set ADC clock to system clock divided by 1. More... | |
| #define | ADC_CLOCK_DIVIDER_2 ADC_CTL0_SCLKDIV_DIV_BY_2 |
| Set ADC clock to system clock divided by 2. More... | |
| #define | ADC_CLOCK_DIVIDER_4 ADC_CTL0_SCLKDIV_DIV_BY_4 |
| Set ADC clock to system clock divided by 4. More... | |
| #define | ADC_CLOCK_DIVIDER_8 ADC_CTL0_SCLKDIV_DIV_BY_8 |
| Set ADC clock to system clock divided by 8. More... | |
| #define | ADC_CLOCK_DIVIDER_16 ADC_CTL0_SCLKDIV_DIV_BY_16 |
| Set ADC clock to system clock divided by 16. More... | |
| #define | ADC_CLOCK_DIVIDER_24 ADC_CTL0_SCLKDIV_DIV_BY_24 |
| Set ADC clock to system clock divided by 24. More... | |
| #define | ADC_CLOCK_DIVIDER_32 ADC_CTL0_SCLKDIV_DIV_BY_32 |
| Set ADC clock to system clock divided by 32. More... | |
| #define | ADC_CLOCK_DIVIDER_48 ADC_CTL0_SCLKDIV_DIV_BY_48 |
| Set ADC clock to system clock divided by 48. More... | |
| #define | ADC_RESOLUTION_12_BIT ADC_CTL2_RES_BIT_12 |
| Set resolution of ADC conversion to 12 bit (unsigned) More... | |
| #define | ADC_RESOLUTION_10_BIT ADC_CTL2_RES_BIT_10 |
| Set resolution of ADC conversion to 10 bit (unsigned) More... | |
| #define | ADC_RESOLUTION_8_BIT ADC_CTL2_RES_BIT_8 |
| Set resolution of ADC conversion to 8 bit (unsigned) More... | |
| #define | ADC_FIXED_REFERENCE_1V4 0 |
| Set ADC reference to internal fixed 1.4V. More... | |
| #define | ADC_FIXED_REFERENCE_2V5 1 |
| Set ADC reference to internal fixed 2.5V. More... | |
| #define | ADC_EXTERNAL_REFERENCE 2 |
| Set ADC reference to external analog pin A1. More... | |
| #define | ADC_VDDS_REFERENCE 3 |
| Set ADC reference to VDDS. More... | |
| #define | ADC_POWER_DOWN_POLICY_AUTO ADC_CTL0_PWRDN_AUTO |
| ADC is powered down on completion of a conversion if there is no pending trigger. To be used with ADCSetPowerDownPolicy() More... | |
| #define | ADC_POWER_DOWN_POLICY_MANUAL ADC_CTL0_PWRDN_MANUAL |
| ADC remains powered on as long as the power mode it set to manual. To be used with ADCSetPowerDownPolicy() More... | |
| #define | ADC_SEQUENCE_REPEATSEQUENCE ADC_CTL1_CONSEQ_REPEATSEQUENCE |
| Set ADC conversion sequence to repeat control registers defined by start and stop address, as set by ADCSetMemctlRange. More... | |
| #define | ADC_SEQUENCE_REPEATSINGLE ADC_CTL1_CONSEQ_REPEATSINGLE |
| Set ADC conversion sequence to repeat control register defined by start as set by ADCSetMemctlRange. More... | |
| #define | ADC_SEQUENCE_SEQUENCE ADC_CTL1_CONSEQ_SEQUENCE |
| Set ADC conversion sequence to a single pass of control registers defined by start and stop address, as set by ADCSetMemctlRange. More... | |
| #define | ADC_SEQUENCE_SINGLE ADC_CTL1_CONSEQ_SINGLE |
| Set ADC conversion sequence to do a single conversion of control register defined by start, as set by ADCSetMemctlRange. More... | |
| #define | ADC_SAMPLE_MODE_AUTO ADC_CTL1_SAMPMODE_AUTO |
| Sample duration is controlled by values set using ADCSetSampleDuration() More... | |
| #define | ADC_SAMPLE_MODE_MANUAL ADC_CTL1_SAMPMODE_MANUAL |
| Sample phase is manually started using ADCStartConversion() and manually stopped using ADCStopConversion() More... | |
| #define | ADC_TRIGGER_SOURCE_EVENT ADC_CTL1_TRIGSRC_EVENT |
| The ADC trigger source is a hardware event. More... | |
| #define | ADC_TRIGGER_SOURCE_SOFTWARE ADC_CTL1_TRIGSRC_SOFTWARE |
| The ADC trigger source is software. More... | |
| #define | ADC_TRIGGER_POLICY_AUTO_NEXT ADC_MEMCTL0_TRG_AUTO_NEXT |
| The next conversion is automatically started after the completion of the previous conversion. More... | |
| #define | ADC_TRIGGER_POLICY_TRIGGER_NEXT ADC_MEMCTL0_TRG_TRIGGER_NEXT |
| The next conversion requires a trigger. More... | |
| #define | ADC_INT_MEMRES_23 ADC_IMASK0_MEMRESIFG23 |
| Result ready in memory result register 23. More... | |
| #define | ADC_INT_MEMRES_22 ADC_IMASK0_MEMRESIFG22 |
| Result ready in memory result register 22. More... | |
| #define | ADC_INT_MEMRES_21 ADC_IMASK0_MEMRESIFG21 |
| Result ready in memory result register 21. More... | |
| #define | ADC_INT_MEMRES_20 ADC_IMASK0_MEMRESIFG20 |
| Result ready in memory result register 20. More... | |
| #define | ADC_INT_MEMRES_19 ADC_IMASK0_MEMRESIFG19 |
| Result ready in memory result register 19. More... | |
| #define | ADC_INT_MEMRES_18 ADC_IMASK0_MEMRESIFG18 |
| Result ready in memory result register 18. More... | |
| #define | ADC_INT_MEMRES_17 ADC_IMASK0_MEMRESIFG17 |
| Result ready in memory result register 17. More... | |
| #define | ADC_INT_MEMRES_16 ADC_IMASK0_MEMRESIFG16 |
| Result ready in memory result register 16. More... | |
| #define | ADC_INT_MEMRES_15 ADC_IMASK0_MEMRESIFG15 |
| Result ready in memory result register 15. More... | |
| #define | ADC_INT_MEMRES_14 ADC_IMASK0_MEMRESIFG14 |
| Result ready in memory result register 14. More... | |
| #define | ADC_INT_MEMRES_13 ADC_IMASK0_MEMRESIFG13 |
| Result ready in memory result register 13. More... | |
| #define | ADC_INT_MEMRES_12 ADC_IMASK0_MEMRESIFG12 |
| Result ready in memory result register 12. More... | |
| #define | ADC_INT_MEMRES_11 ADC_IMASK0_MEMRESIFG11 |
| Result ready in memory result register 11. More... | |
| #define | ADC_INT_MEMRES_10 ADC_IMASK0_MEMRESIFG10 |
| Result ready in memory result register 10. More... | |
| #define | ADC_INT_MEMRES_09 ADC_IMASK0_MEMRESIFG9 |
| Result ready in memory result register 9. More... | |
| #define | ADC_INT_MEMRES_08 ADC_IMASK0_MEMRESIFG8 |
| Result ready in memory result register 8. More... | |
| #define | ADC_INT_MEMRES_07 ADC_IMASK0_MEMRESIFG7 |
| Result ready in memory result register 7. More... | |
| #define | ADC_INT_MEMRES_06 ADC_IMASK0_MEMRESIFG6 |
| Result ready in memory result register 6. More... | |
| #define | ADC_INT_MEMRES_05 ADC_IMASK0_MEMRESIFG5 |
| Result ready in memory result register 5. More... | |
| #define | ADC_INT_MEMRES_04 ADC_IMASK0_MEMRESIFG4 |
| Result ready in memory result register 4. More... | |
| #define | ADC_INT_MEMRES_03 ADC_IMASK0_MEMRESIFG3 |
| Result ready in memory result register 3. More... | |
| #define | ADC_INT_MEMRES_02 ADC_IMASK0_MEMRESIFG2 |
| Result ready in memory result register 2. More... | |
| #define | ADC_INT_MEMRES_01 ADC_IMASK0_MEMRESIFG1 |
| Result ready in memory result register 1. More... | |
| #define | ADC_INT_MEMRES_00 ADC_IMASK0_MEMRESIFG0 |
| Result ready in memory result register 0. More... | |
| #define | ADC_INT_ASCDONE ADC_IMASK0_ASCDONE |
| Ad-Hoc single conversion done. More... | |
| #define | ADC_INT_UVIFG ADC_IMASK0_UVIFG |
| Conversion underflow. More... | |
| #define | ADC_INT_DMADONE ADC_IMASK0_DMADONE |
| DMA transaction done. More... | |
| #define | ADC_INT_INIFG ADC_IMASK0_INIFG |
| ADC result is inside window comparator range. More... | |
| #define | ADC_INT_LOWIFG ADC_IMASK0_LOWIFG |
| ADC result is below window comparator range. More... | |
| #define | ADC_INT_HIGHIFG ADC_IMASK0_HIGHIFG |
| ADC result is above window comparator range. More... | |
| #define | ADC_INT_TOVIFG ADC_IMASK0_TOVIFG |
| Sequence conversion timeout overflow. More... | |
| #define | ADC_INT_OVIFG ADC_IMASK0_OVIFG |
| Conversion overflow. More... | |
Functions | |
| void | ADCSetSampleDuration (uint32_t clkDiv, uint16_t clkCycles) |
| Sets the clock-divider value, and sample duration. More... | |
| void | ADCSetResolution (uint32_t resolution) |
| Sets the ADC bit resolution. More... | |
| void | ADCSetInput (uint32_t reference, uint8_t channel, uint32_t index) |
| Sets the ADC reference source and input channel. More... | |
| void | ADCSetMemctlRange (uint32_t start, uint32_t stop) |
| Set start and stop control registers. More... | |
| void | ADCSetPowerDownPolicy (uint32_t powerDownPolicy) |
| Set power down policy. More... | |
| void | ADCSetSequence (uint32_t sequence) |
| Set conversion sequence. More... | |
| void | ADCSetSamplingMode (uint32_t samplingMode) |
| Set ADC sampling mode. More... | |
| void | ADCSetTriggerSource (uint32_t triggerSource) |
| Set ADC trigger source. More... | |
| void | ADCSetTriggerPolicy (uint32_t triggerPolicy, uint32_t index) |
| Set ADC trigger policy. More... | |
| __STATIC_INLINE void | ADCStartConversion (void) |
| Start conversion. More... | |
| __STATIC_INLINE void | ADCStopConversion (void) |
| Stop sample phase of a conversion. More... | |
| __STATIC_INLINE void | ADCEnableConversion (void) |
| Enable conversion. More... | |
| __STATIC_INLINE void | ADCDisableConversion (void) |
| Disable conversion. More... | |
| __STATIC_INLINE void | ADCEnableDmaTrigger (void) |
| Enable DMA trigger for data transfer. More... | |
| __STATIC_INLINE void | ADCDisableDmaTrigger (void) |
| Disable DMA trigger for data transfer. More... | |
| __STATIC_INLINE uint32_t | ADCReadResult (uint32_t index) |
| Read conversion result from ADC. More... | |
| __STATIC_INLINE bool | ADCIsBusy (void) |
| Check if ADC is busy. More... | |
| __STATIC_INLINE uint32_t | ADCReadResultNonBlocking (uint32_t index) |
| Read conversion result from ADC. More... | |
| uint32_t | ADCValueToMicrovolts (uint32_t adcCode, uint32_t bitResolution, uint32_t referenceVoltageMicroVolt) |
| Convert ADC code to microvolts. More... | |
| __STATIC_INLINE void | ADCEnableInterrupt (uint32_t intFlags) |
| Enables individual ADC interrupt sources. More... | |
| __STATIC_INLINE void | ADCDisableInterrupt (uint32_t intFlags) |
| Disables individual ADC interrupt sources. More... | |
| __STATIC_INLINE uint32_t | ADCRawInterruptStatus (void) |
| Gets the current raw interrupt status. More... | |
| __STATIC_INLINE uint32_t | ADCMaskedInterruptStatus (void) |
| Gets the current masked interrupt status. More... | |
| __STATIC_INLINE void | ADCClearInterrupt (uint32_t intFlags) |
| Clears ADC interrupt sources. More... | |
| uint16_t | ADCGetAdjustmentGain (uint32_t reference) |
| Returns ADC gain value for given reference. More... | |
| void | ADCSetAdjustmentOffset (uint32_t reference) |
| Write correct offset value to ADC-peripheral trim register. More... | |
| uint32_t | ADCAdjustValueForGain (uint32_t adcValue, uint32_t bitResolution, uint16_t gain) |
| Performs ADC value gain adjustment. More... | |