UTIL_NV_Read¶
- Opcode:
0xFE81
- Command Description:
Send this command to read an NV parameter.
Command Parameters
- nvID:
- Size:
2 byte(s)
- Default:
0
- Range:
Any 2-byte value
- nvLen:
- Size:
1 byte(s)
- Default:
0
- Range:
Any 1-byte value
Events Generated
When this command is received, the host will send the CommandStatus Event.
UTIL_NV_Write¶
- Opcode:
0xFE82
- Command Description:
Send this command to write an NV parameter.
Command Parameters
- nvID:
- Size:
2 byte(s)
- Default:
0
- Range:
Any 2-byte value
- nvDataLen:
Size of NV data
- Size:
1 byte(s)
- Value:
size(nvData)
- nvData:
NV Data Field. Structure can be different for each NV item
- Size:
input byte(s)
- Default:
“00”
- Range:
Any 1-byte value
Events Generated
When this command is received, the host will send the CommandStatus Event.
UTIL_ForceBoot¶
- Opcode:
0xFE83
- Command Description:
Force the boot loader to run.
Events Generated
When this command is received, the device resets if the boot loader is present. Otherwise, the host will send the CommandStatus Event.
UTIL_BuildRevision¶
- Opcode:
0xFE84
- Command Description:
This command is used to read the build revision information of the BLE stack software.
Events Generated
When this command is received, the host will send the CommandStatus Event.
Additional Command Status Return Parameters
- dataLen:
- Size:
1 byte(s)
- Range:
- stk ver (mj/mn/ph):
- Condition:
( StatStatus==0x00)
- Size:
3 byte(s)
- Range:
- bld ver:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- stk info:
- Condition:
( StatStatus==0x00)
- Size:
1 byte(s)
- Range:
Value
Description
0x01
IARProject
0x02
CCSProject
0x10
IARLibrary
0x80
ROMBuild
- ctrl info:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
Value
Description
0x01
ADV_NCONN
0x02
ADV_CONN
0x04
SCAN
0x08
INIT
0x10
PING
0x20
SLV_FEAT_EXCHG
0x40
CONN_PARAM_REQ
- host info:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
Value
Description
0x01
BROADCASTER
0x02
OBSERVER
0x04
PERIPHERAL
0x08
CENTRAL
UTIL_GetMemStats¶
- Opcode:
0xFE87
- Command Description:
Get memory statistics
Command Parameters
- command ID:
- Size:
1 byte(s)
- Default:
2
- Range:
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
Events Generated
When this command is received, the host will send the CommandStatus Event.
Additional Command Status Return Parameters
- dataLen:
- Size:
1 byte(s)
- Range:
:all cmdID receive :
- Size:
1 byte(s)
- Range:
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- cmdID:
- Condition:
( (cmdID & 0x01) == 0x01)
- Size:
1 byte(s)
- Range:
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- Heap Size:
- Condition:
( (cmdID & 0x01) == 0x01)
- Size:
4 byte(s)
- Range:
- Heap Size Free:
- Condition:
( (cmdID & 0x01) == 0x01)
- Size:
4 byte(s)
- Range:
- Biggest free buffer Available:
- Condition:
( (cmdID & 0x01) == 0x01)
- Size:
4 byte(s)
- Range:
- cmdID:
- Condition:
( (cmdID & 0x02) == 0x02)
- Size:
1 byte(s)
- Range:
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- Heap Fail number:
- Condition:
( (cmdID & 0x02) == 0x02)
- Size:
2 byte(s)
- Range:
- Heap Allocated:
- Condition:
( (cmdID & 0x02) == 0x02)
- Size:
4 byte(s)
- Range:
- Heap Max Allocated:
- Condition:
( (cmdID & 0x02) == 0x02)
- Size:
4 byte(s)
- Range:
- cmdID:
- Condition:
( (cmdID & 0x04) ==0x04)
- Size:
1 byte(s)
- Range:
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- Number of Thread:
- Condition:
( (cmdID & 0x04) ==0x04)
- Size:
1 byte(s)
- Range:
An array of size “Count” will be returned containing the parameters starting here:
- Priority:
- Condition:
( (cmdID & 0x04) ==0x04)
- Size:
1 byte(s)
- Range:
- Handle:
- Condition:
( (cmdID & 0x04) ==0x04)
- Size:
2 byte(s)
- Range:
- max Stack used:
- Condition:
( (cmdID & 0x04) ==0x04)
- Size:
2 byte(s)
- Range:
- stack size:
- Condition:
( (cmdID & 0x04) ==0x04)
- Size:
2 byte(s)
- Range:
The array of parameters ends here.