GAP_DeviceInit

Opcode:

0xFE00

Command Description:

This command is used to setup the device. Can only be called once per reset. In order to change the address mode / random address, it is necessary to reset the device and call this API again. In the case where the address mode or random address is different than it was for the last initialization, all bonds and local information stored in NV will be erased.

Command Parameters

profileRole:

Bit Mask - GAP Profile Roles

Size:

1 byte(s)

Default:

8

Range:

Value

Description

0x01

GAP_PROFILE_BROADCASTER

0x02

GAP_PROFILE_OBSERVER

0x04

GAP_PROFILE_PERIPHERAL

0x08

GAP_PROFILE_CENTRAL

addrMode:

Address Mode

Size:

1 byte(s)

Default:

2

Range:

Value

Description

0x00

ADDRMODE_PUBLIC

0x01

ADDRMODE_RANDOM

0x02

ADDRMODE_RP_WITH_PUBLIC_ID

0x03

ADDRMODE_RP_WITH_RANDOM_ID

ramdomAddr:

Address Mode

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value

Events Generated

When this command is received, the host will send the CommandStatus Event.When initialization task is complete, the host will send the GAP_DeviceInitDone event.

GAP_TerminateLinkReq

Opcode:

0xFE0A

Command Description:

Send this command to terminate a connection link or all active connections.

Command Parameters

connectionHandle:

Connection handle of link to terminate.

Size:

2 byte(s)

Default:

0

Range:

0 - 0xFFFD to terminate a connection, 0xFFFF to terminate all connections

reason:

Error Code to send over the air in the termination request.

Size:

1 byte(s)

Default:

0x13

Range:

Value

Description

0x05

Authentication Failure

0x13

Remote User Terminated Connection

0x14

Remote Device Terminated Connection Due To Low Resources

0x15

Remote Device Terminated Connection due to Power Off

0x1A

Unsupported Remote Feature

0x29

Pairing With Unit Key Not Supported

0x3B

Unacceptable Connection Interval

Events Generated

When this command is received, the host will send the CommandStatus Event. When the connection is terminated, the GAP_LinkTerminated Event will be generated.

GAP_Authenticate

Opcode:

0xFE0B

Command Description:

Send this command to initiate the pairing process (if Central device), wait for the pairing process (if Peripheral device), or accept a pairing request (if Peripheral device).

Command Parameters

Connection Handle:

Identifies the connection.

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x0EFF

secReq_ioCaps:

Defines the values which are used when exchanging IO capabilities

Size:

1 byte(s)

Default:

3

Range:

Value

Description

0x00

DisplayOnly

0x01

DisplayYesNo

0x02

KeyboardOnly

0x03

NoInputNoOutput

0x04

KeyboardDisplay

secReq_oobAvailable:

“Enable” if Out-of-band key available.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Disable

1

Enable

secReq_oob:

OOB data - Initial TK value for the pairing process.

Size:

16 byte(s)

Default:

“4d:9f:88:5a:6e:03:12:fe:00:00:00:00:00:00:00:00”

Range:

Any 16 byte value

secReq_oobConfirm:

OOB data Confirm value. Secure Connection only.

Size:

16 byte(s)

Default:

“00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00”

Range:

Any 16 byte value

secReq_localOobAvailable:

Secure Connections Local OOB data available

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

Locally generated OOB data is NOT available

0x01

Local generated OOB data is available

secReq_localOob:

Secure Connections local OOB value - 16 bytes in length.

Size:

16 byte(s)

Default:

“00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00”

Range:

Any 16 byte value

secReq_isSCOnlyMode:

Type of pairing to allow

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

Legacy Pairing allowed

0x01

Only Secure Connections pairing allowed

secReq_eccKeys_isUsed:

1 if ECC Keys are specified, 0 for internal generation.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

Stack chooses ECC keys.

0x01

Use application provided ECC keys.

secReq_eccKeys_sK:

P-256 ECC Private Key.

Size:

32 byte(s)

Default:

“BD:1A:3C:CD:A6:B8:99:58:99:B7:40:EB:7B:60:FF:4A:50:3F:10:D2:E3:B3:C9:74:38:5F:C5:A3:D4:F6:49:3F”

Range:

Any 32 byte value

secReq_eccKeys_pK_x:

P-256 ECC Public Key X-Coordinate.

Size:

32 byte(s)

Default:

“E6:9D:35:0E:48:01:03:CC:DB:FD:F4:AC:11:91:F4:EF:B9:A5:F9:E9:A7:83:2C:5E:2C:BE:97:F2:D2:03:B0:20”

Range:

Any 32 byte value

secReq_eccKeys_pK_y:

P-256 ECC Public Key Y-Coordinate.

Size:

32 byte(s)

Default:

“8B:D2:89:15:D0:8E:1C:74:24:30:ED:8F:C2:45:63:76:5C:15:52:5A:BF:9A:32:63:6D:EB:2A:65:49:9C:80:DC”

Range:

Any 32 byte value

secReq_authReq:

A bit field that indicates the requested security properties for STK and GAP bonding information.

Size:

1 byte(s)

Default:

1

Range:

Value

Description

0x01

Bonding

0x04

MITM

0x08

SC

0x10

KP

0x20

CT2

secReq_maxEncKeySize:

This value defines the maximum encryption key size in octets that the device can support.

Size:

1 byte(s)

Default:

16

Range:

7-16

secReq_keyDist:

The Key Distribution field indicates which keys will be distributed.

Size:

1 byte(s)

Default:

119

Range:

Value

Description

0x01

GAPBOND_KEYDIST_PENCKEY

0x02

GAPBOND_KEYDIST_PIDKEY

0x04

GAPBOND_KEYDIST_PSIGN

0x08

GAPBOND_KEYDIST_PLINK

0x10

GAPBOND_KEYDIST_CENCKEY

0x20

GAPBOND_KEYDIST_CIDKEY

0x40

GAPBOND_KEYDIST_CSIGN

0x80

GAPBOND_KEYDIST_CLINK

pairReq_Enable:

“Enable” if Pairing Request has already been received and to respond with a Pairing Response. This should only be used in a Peripheral device.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Disable

1

Enable

pairReq_ioCaps:

Defines the values which are used when exchanging IO capabilities

Size:

1 byte(s)

Default:

3

Range:

Value

Description

0x00

DisplayOnly

0x01

DisplayYesNo

0x02

KeyboardOnly

0x03

NoInputNoOutput

0x04

KeyboardDisplay

pairReq_oobDataFlag:

“Enable” if OOB key is available.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Disable

1

Enable

pairReq_authReq:

A bit field that indicates the requested security properties for STK and GAP bonding information.

Size:

1 byte(s)

Default:

1

Range:

Value

Description

0x01

Bonding

0x04

MITM

0x08

SC

0x10

KP

0x20

CT2

pairReq_maxEncKeySize:

This value defines the maximum encryption key size in octets that the device can support.

Size:

1 byte(s)

Default:

16

Range:

7-16

pairReq_keyDist:

The Key Distribution field indicates which keys will be distributed.

Size:

1 byte(s)

Default:

119

Range:

Value

Description

0x01

GAPBOND_KEYDIST_PENCKEY

0x02

GAPBOND_KEYDIST_PIDKEY

0x04

GAPBOND_KEYDIST_PSIGN

0x08

GAPBOND_KEYDIST_PLINK

0x10

GAPBOND_KEYDIST_CENCKEY

0x20

GAPBOND_KEYDIST_CIDKEY

0x40

GAPBOND_KEYDIST_CSIGN

0x80

GAPBOND_KEYDIST_CLINK

Events Generated

When this command is received, the host will send the CommandStatus Event. When the pairing process is complete (either SUCCESS or Failure), a GAP_AuthenticationComplete will be generated. If a passkey is needed, a GAP_PasskeyNeeded will be generated.

GAP_TerminateAuth

Opcode:

0xFE10

Command Description:

Send this command to terminate a pairing process.

Command Parameters

Connection Handle:

Identifies the connection.

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x0EFF

reason:

Pairing Failed Message reason field.

Size:

1 byte(s)

Default:

3

Range:

Value

Description

0x00

SUCCESS

0x01

SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED

0x02

SMP_PAIRING_FAILED_OOB_NOT_AVAIL

0x03

SMP_PAIRING_FAILED_AUTH_REQ

0x04

SMP_PAIRING_FAILED_CONFIRM_VALUE

0x05

SMP_PAIRING_FAILED_NOT_SUPPORTED

0x06

SMP_PAIRING_FAILED_ENC_KEY_SIZE

0x07

SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED

0x08

SMP_PAIRING_FAILED_UNSPECIFIED

0x09

SMP_PAIRING_FAILED_REPEATED_ATTEMPTS

0x0A

SMP_PAIRING_FAILED_INVALID_PARAMETERS

0x0B

SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED

0x0C

SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED

0x0D

SMP_PAIRING_FAILED_BREDR_PAIR_IN_PROGRESS

0x0E

SMP_PAIRING_FAILED_CT_KEYDER_NOT_ALLOWED

0x0F

SMP_PAIRING_FAILED_KEY_REJECTED

0x10

Command Disallowed

0x11

Unsupported Feature Or Parameter Value

0x12

Invalid HCI Command Parameters

0x17

bleTimeout

Events Generated

When this command is received, the host will send the CommandStatus Event. When the existing pairing had ended, the GAP_AuthenticationComplete with be generated.

GAP_UpdateLinkParamReq

Opcode:

0xFE11

Command Description:

Send this command to change the Link Layer connection parameters of a connection. This command can only be used when the local devices role is Central or peripheral.

Command Parameters

Connection Handle:

Identifies the connection.

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0xFFFD

intervalMin:

Minimum value (* 1.25 ms) for the connection event interval. This shall be less than or equal to intervalMax.

Size:

2 byte(s)

Default:

80

Range:

6 - 3200

intervalMax:

Maximum value (* 1.25 ms) for the connection event interval. This shall be greater than or equal to intervalMin./

Size:

2 byte(s)

Default:

160

Range:

6 - 3200

connLatency:

The desired peripheral latency for the connection in number of connection events.

Size:

2 byte(s)

Default:

0

Range:

0 - 499

connTimeout:

The desired supervision timeout (* 10 ms)

Size:

2 byte(s)

Default:

1000

Range:

10 - 3200

Events Generated

When this command is received, the host will send the CommandStatus Event. When the connection parameters have been applied by the Controller, the GAP_LinkParamUpdate Event will be generated.

GAP_UpdateLinkParamReqReply

Opcode:

0xFE12

Command Description:

Reply to a GAP_LinkParamUpdateRequest that was received from a remote device

Command Parameters

Connection Handle:

Identifies the connection.

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0xFFFD

intervalMin:

Minimum value (* 1.25 ms) for the connection event interval. This shall be less than or equal to intervalMax.

Size:

2 byte(s)

Default:

80

Range:

6 - 3200

intervalMax:

Maximum value (* 1.25 ms) for the connection event interval. This shall be greater than or equal to intervalMin./

Size:

2 byte(s)

Default:

160

Range:

6 - 3200

connLatency:

The desired peripheral latency for the connection in number of connection events.

Size:

2 byte(s)

Default:

0

Range:

0 - 499

connTimeout:

The desired supervision timeout (* 10 ms)

Size:

2 byte(s)

Default:

1000

Range:

10 - 3200

signalIdentifier:

Signal ID for L2CAP Connection Parameter Update Request. 0 for LL Connection Parameter Request. This must match the signal ID provided by the corresponding update request.

Size:

1 byte(s)

Default:

1

Range:

0 - 255

accepted:

Yes to accept Parameter Update Request, No to reject it.

Size:

1 byte(s)

Default:

1

Range:

Value

Description

0x00

No

0x01

Yes

Events Generated

When this command is received, the host will send the CommandStatus Event. When the connection parameters have been applied by the Controller, the GAP_LinkParamUpdate Event will be generated.

Gap_RegisterConnEvent

Opcode:

0xFE13

Command Description:

Register/Unregister to receive connection event information.

Command Parameters

Action:

Whether to register or unregister.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

GAP_CB_REGISETER

0x01

GAP_CB_UNREGISTER

Connection Handle:

Identifies the connection. If 0xFFFF, apply to all connections. Else, apply only for a specific connection

Size:

2 byte(s)

Default:

0xFFFF

Range:

0x0000 to 0xFFFD

Event Type:

Which Event Type Information to register to. This will prevent the event from getting generated after each connection event, instead it will be generated in specific cases of the connection event.

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x01

GAP_CB_CONN_ESTABLISHED

0x02

GAP_CB_PHY_UPDATE

0x03

GAP_CB_CONN_ESTABLISHED | GAP_CB_PHY_UPDATE

0xFF

GAP_CB_CONN_EVENT_ALL

Events Generated

When this command is received, the host will send the CommandStatus Event. If successfully registers, the GAP_ConnectionEventNotice Event will be generated after each connection event or on specific instances.

GapAdv_SetPeriodicAdvParams

Opcode:

0xFE14

Command Description:

Create a periodic advertising set.

Command Parameters

Handle:

The extended advertising handle

Size:

1 byte(s)

Default:

0x00

Range:

0x00 to 0xEF

Interval Min:

Periodic interval minimum time = Min Interval * 1.25 ms

Size:

2 byte(s)

Default:

0x0006

Range:

0x0006 to 0xFFFF

Interval Max:

Periodic interval maximum time = Min Interval * 1.25 ms

Size:

2 byte(s)

Default:

0x0006

Range:

0x0006 to 0xFFFF

Properties:

Periodic advertising properties. Set 0x0040 to include TxPower in the advertising PDU

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 or 0x0040

Events Generated

When this command is received, the host will send the CommandStatus Event. If the host returns SUCCESS GapAdv_SetPeriodicAdvParams VS event will be received with the controller completion status

GapAdv_setPeriodicAdvData

Opcode:

0xFE15

Command Description:

Add data to a periodic advertising set.

Command Parameters

Handle:

The extended advertising handle

Size:

1 byte(s)

Default:

0x00

Range:

0x00 to 0xEF

Operation:

Type of operation used to send the payload in the controller

Size:

1 byte(s)

Default:

0x03

Range:

Value

Description

0x00

Intermediate fragment of data

0x01

First fragment of fragmented data

0x02

Last fragment of fragmented data

0x03

Complete data

Payload Length:
Size:

1 byte(s)

Value:

size(dataLen)

Data:

Periodic advertising data up to 252

Size:

input byte(s)

Default:

“00:11:22:33”

Range:

0 to 252

Events Generated

When this command is received, the host will send the CommandStatus Event. If the host returns SUCCESS GAPAdv_SetPeriodicAdvData VS event will be received with the controller completion status

GapAdv_SetPeriodicAdvEnable

Opcode:

0xFE16

Command Description:

Enable a periodic advertising set

Command Parameters

Enable:

Enable or disable the periodic adverising set

Size:

1 byte(s)

Default:

0x00

Range:

0x00 to 0x01

Handle:

The extended advertising handle

Size:

1 byte(s)

Default:

0x00

Range:

0x00 to 0xEF

Events Generated

When this command is received, the host will send the CommandStatus Event. If the host returns SUCCESS GAPAdv_SetPeriodicAdvEnable VS event will be received with the controller completion status

GapScan_PeriodicAdvCreateSync

Opcode:

0xFE17

Command Description:

Set sync parameters for periodic scanning

Command Parameters

advSID:

Persiodic Advertising SID

Size:

1 byte(s)

Default:

0x00

Range:

0x00 to 0x0F

options:

Use periodic list and/or enable/disable periodic report

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x01

Use Periodic Advertiser List

0x02

Disable Periodic Advertising Report

advAddrType:

Advertiser Address Type

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID

0x01

PEER_ADDRTYPE_RANDOM_OR_RANDOM_ID

advAddress:

Advertiser Address

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value

skip:

Periodic Advertising events that can be skipped after a successful receive

Size:

2 byte(s)

Default:

0

Range:

0x0000 to 0x01F3

syncTimeout:

Synchronization timeout for the periodic advertising train

Size:

2 byte(s)

Default:

0x000A

Range:

0x000A-0x4000

syncCteType:

Select cte type for syncing periodic train (bit mask)

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x01

Do not sync to packets with AoA

0x02

Do not sync to packets with 1us AoD

0x04

Do not sync to packets with 2us AoD

0x08

not in use

0x10

Do not sync to packets without CTE

Events Generated

When this command is received, the host will send the CommandStatus Event. If the host returns SUCCESS GAPScan_PeriodicAdvCreateSync VS event will be received with the controller completion status

GapScan_PeriodicAdvCreateSyncCancel

Opcode:

0xFE18

Command Description:

Cancel the ongoing scanner’s synchronizing state

Events Generated

The host will send the CommandComplete Event to indicate whether the cancel was completed and periodic Advertising Sync Establish with status “Operation Cancelled by Host”

GapScan_PeriodicAdvTerminateSync

Opcode:

0xFE19

Command Description:

Used by the scanner to stop reception of the periodic advertising train identified by the syncHandle parameter

Command Parameters

syncHandle:

Periodic Advertising train identifier

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x0EFF

Events Generated

When this command is received, the host will send the CommandStatus Event. If the host returns SUCCESS GAPScan_PeriodicAdvTerminateSync VS event will be received with the controller completion status

GapScan_SetPeriodicAdvReceiveEnable

Opcode:

0xFE1A

Command Description:

Used by the scanner to enabling or diabling the periodic advertising reports

Command Parameters

syncHandle:

Periodic Advertising train identifier

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x0EFF

Enable:

Enable or disable reports

Size:

1 byte(s)

Default:

1

Range:

0 to 1

Events Generated

When this command is received, the host will send the CommandStatus Event. If the host returns SUCCESS GAPScan_SetPeriodicAdvReceiveEnable VS event will be received with the controller completion status

GapScan_AddDeviceToPeriodicAdvList

Opcode:

0xFE1B

Command Description:

Adding device to the periodic advertiser list

Command Parameters

advAddrType:

Advertiser Address Type

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID

0x01

PEER_ADDRTYPE_RANDOM_OR_RANDOM_ID

advAddress:

Advertiser Address

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value

advSID:

Persiodic Advertising SID

Size:

1 byte(s)

Default:

0x00

Range:

0x00 to 0x0F

Events Generated

When this command is received, the host will send the CommandStatus Event. If the host returns SUCCESS GAPScan_AddDeviceToPeriodicAdvList VS event will be received with the controller completion status

GapScan_RemoveDeviceFromPeriodicAdvList

Opcode:

0xFE1C

Command Description:

Removing device to the periodic advertiser list

Command Parameters

advAddrType:

Advertiser Address Type

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID

0x01

PEER_ADDRTYPE_RANDOM_OR_RANDOM_ID

advAddress:

Advertiser Address

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value

advSID:

Persiodic Advertising SID

Size:

1 byte(s)

Default:

0x00

Range:

0x00 to 0x0F

Events Generated

When this command is received, the host will send the CommandStatus Event. If the host returns SUCCESS GAPScan_RemoveDeviceFromPeriodicAdvList VS event will be received with the controller completion status

GapScan_ReadPeriodicAdvListSize

Opcode:

0xFE1D

Command Description:

Read the advertisers list size

Events Generated

When this command is received, the host will send the CommandStatus Event. After GAPScan_ReadPeriodicAdvListSize with the advertisers list size will be received

GapScan_ClearPeriodicAdvList

Opcode:

0xFE1E

Command Description:

Clear the advertisers list size

Events Generated

When this command is received, the host will send the CommandStatus Event. If the host returns SUCCESS GAPScan_ClearPeriodicAdvList VS event will be received with the controller completion status

GAP_Bond

Opcode:

0xFE0F

Command Description:

Send this command for a connected and bound device to load the encryption key.

Command Parameters

Connection Handle:

Identifies the connection.

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0xFFFD

authenticated:

1 if authenticated. 0 if not.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

No

0x01

Yes

secureConnections:

1 if Secure Connections. 0 if not.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

No

0x01

Yes

secInfo.LTK:

Long Term Key

Size:

16 byte(s)

Default:

“4d:9f:88:5a:6e:03:12:fe:00:00:00:00:00:00:00:00”

Range:

Any 16 byte value

secInfo.DIV:

Diversifier

Size:

2 byte(s)

Default:

0x1111

Range:

Any 16-bit value

secInfo.rand:

LTK Rand pairing

Size:

8 byte(s)

Default:

“11:22:33:44:55:66:77:88”

Range:

Any 8-byte value

secInfo.LTKsize:

LTK Key size (bytes)

Size:

1 byte(s)

Default:

16

Range:

7-16

Events Generated

When this command is received, the host will send the CommandStatus Event. When both connected devices have setup encryption, the GAP_BondComplete is generated.

GAP_Signable

Opcode:

0xFE0E

Command Description:

Send this command for a connected and bound device to enable signed data.

Command Parameters

connectionHandle:

Used to identify the connection

Size:

2 byte(s)

Default:

0

Range:

0 - 0xFFFD

authenticated:

“1 if the signing information was authenticated; 0 otherwise

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

No

0x01

Yes

CSRK:

Connection Signature Resolving Key for the connected device

Size:

16 byte(s)

Default:

0

Range:

Any 16 byte value

signCounter:

Sign Counter for the connected device

Size:

4 byte(s)

Default:

0

Range:

Any 4 byte value

Events Generated

When this command is received, the host will send the CommandStatus Event.

GAP_PasskeyUpdate

Opcode:

0xFE0C

Command Description:

Send this command when the GAP Passkey Needed Event is received. This command sends a passkey needed during the Pairing Process.

Command Parameters

connectionHandle:

Used to identify the connection

Size:

2 byte(s)

Default:

0

Range:

0 - 0xFFFD

Passkey:

6 character ASCII string of numbers (ex. 019655? )

Size:

6 byte(s)

Default:

“019655”

Range:

Any 6 character string

Events Generated

When this command is received, the host will send the CommandStatus Event.

GAP_PeripheralSecurityRequest

Opcode:

0xFE0D

Command Description:

Send this command, Peripheral Role only, to initiate security from a peripheral device. This message is also sent, by the Peripheral, to upgrade security (Pairing) to “Authenticated”, make sure to ask for Man-In-The-Middle (MITM) protection in the “authReq” field.

Command Parameters

connectionHandle:

Used to identify the connection

Size:

2 byte(s)

Default:

0

Range:

0 - 0xFFFD

authReq:

A bit field that indicates the requested security properties for STK and GAP bonding information.

Size:

1 byte(s)

Default:

5

Range:

Value

Description

0x01

Bonding

0x04

MITM

0x08

SC

0x10

KP

0x20

CT2

Events Generated

When this command is received, the host will send the CommandStatus Event.

GapConfig_SetParameter

Opcode:

0xFE2F

Command Description:

Set a configuration parameter (IRK or SRK)

Command Parameters

paramID:

Parameter ID

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

GAP_CONFIG_PARAM_IRK

1

GAP_CONFIG_PARAM_SRK

2

GAP_CONFIG_PARAM_IRK_UPDATE_IMMED

paramValue:

Key to set the parameter with

Size:

16 byte(s)

Default:

“00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00”

Range:

Any 16-byte value

Events Generated

When this command is received, the host will send the CommandStatus Event.

GAP_SetParamValue

Opcode:

0xFE30

Command Description:

Set a GAP Parameter. See the respective parameter for more information

Command Parameters

paramID:

Parameter to Set

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

GAP_PARAM_LINK_UPDATE_DECISION

1

GAP_PARAM_CONN_PARAM_TIMEOUT

2

GAP_PARAM_PRIVATE_ADDR_INT

3

GAP_PARAM_SM_TIMEOUT

4

GAP_PARAM_SM_MIN_KEY_LEN

5

GAP_PARAM_SM_MAX_KEY_LEN

6

GAP_PARAM_AUTH_TASK_ID

7

GAP_PARAM_VERIFY_CAR

8

GAP_PARAM_GGS_PARAMS

9

GAP_PARAM_GAP_TESTCODE

10

GAP_PARAM_SM_TESTCODE

11

GAP_PARAM_GATT_TESTCODE

12

GAP_PARAM_ATT_TESTCODE

13

GAP_PARAM_L2CAP_TESTCODE

14

GAP_PARAM_SET_SCAN_CHAN

GAP_PARAM_LINK_UPDATE_DECISION:

Action to take upon receiving a parameter update request

Condition:

( paramID == 0)

Size:

2 byte(s)

Default:

0x02

Range:

Value

Description

0x00

GAP_UPDATE_REQ_ACCEPT_ALL

0x01

GAP_UPDATE_REQ_DENY_ALL

0x02

GAP_UPDATE_REQ_PASS_TO_APP

GAP_PARAM_CONN_PARAM_TIMEOUT:

Minimum time after an L2CAP Connection Parameter Update Response has been received that a L2CAP Connection Parameter Update Request can be sent. See section Version 5.0 Vol 3, Part C, Section 9.3.9.2 of the BT Core Spec

Condition:

( paramID == 1)

Size:

2 byte(s)

Default:

30000

Range:

1-65535

GAP_PARAM_PRIVATE_ADDR_INT:

Minimum Time Interval between private (resolvable) address changes (in minutes)

Condition:

( paramID == 2)

Size:

2 byte(s)

Default:

15

Range:

1-65535

GAP_PARAM_SM_TIMEOUT:

Time to wait for security manager response before returning bleTimeout (in ms)

Condition:

( paramID == 3)

Size:

2 byte(s)

Default:

30000

Range:

1-65535

GAP_PARAM_SM_MIN_KEY_LEN:

SM Minimum Key Length supported

Condition:

( paramID == 4)

Size:

2 byte(s)

Default:

7

Range:

1-65535

GAP_PARAM_SM_MAX_KEY_LEN:

SM Maximum Key Length supported

Condition:

( paramID == 5)

Size:

2 byte(s)

Default:

16

Range:

1-65535

GAP_PARAM_AUTH_TASK_ID:

For TestMode Only

Condition:

( paramID == 6)

Size:

2 byte(s)

Default:

0xFF

Range:

Any 2 byte value

GAP_PARAM_VERIFY_CAR:

Verify the Central Address Resolution (CAR) characteristic is set before sending directed advertisements using RPA

Condition:

( paramID == 7)

Size:

2 byte(s)

Default:

1

Range:

Value

Description

0x00

No

0x01

Yes

GAP_PARAM_GGS_PARAMS:

For TestMode Only

Condition:

( paramID == 8)

Size:

2 byte(s)

Default:

30720

Range:

For TestMode Only

GAP_PARAM_GAP_TESTCODE:

For TestMode Only

Condition:

( paramID == 9)

Size:

2 byte(s)

Default:

30720

Range:

For TestMode Only

GAP_PARAM_SM_TESTCODE:

For TestMode Only

Condition:

( paramID == 10)

Size:

2 byte(s)

Default:

30720

Range:

For TestMode Only

GAP_PARAM_GATT_TESTCODE:

For TestMode Only

Condition:

( paramID == 11)

Size:

2 byte(s)

Default:

30720

Range:

For TestMode Only

GAP_PARAM_ATT_TESTCODE:

For TestMode Only

Condition:

( paramID == 12)

Size:

2 byte(s)

Default:

30720

Range:

For TestMode Only

GAP_PARAM_L2CAP_TESTCODE:

For TestMode Only

Condition:

( paramID == 13)

Size:

2 byte(s)

Default:

30720

Range:

For TestMode Only

GAP_PARAM_SET_SCAN_CHAN:

Set the Scan Channels Mapping

Condition:

( paramID == 14)

Size:

2 byte(s)

Default:

0x7

Range:

1-7

Events Generated

When this command is received, the host will send the CommandStatus Event.

GAP_GetParamValue

Opcode:

0xFE31

Command Description:

Get a Parameter value.

Command Parameters

paramID:

Parameter to get

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

GAP_PARAM_LINK_UPDATE_DECISION

1

GAP_PARAM_CONN_PARAM_TIMEOUT

2

GAP_PARAM_PRIVATE_ADDR_INT

3

GAP_PARAM_SM_TIMEOUT

4

GAP_PARAM_SM_MIN_KEY_LEN

5

GAP_PARAM_SM_MAX_KEY_LEN

6

GAP_PARAM_AUTH_TASK_ID

7

GAP_PARAM_VERIFY_CAR

8

GAP_PARAM_GGS_PARAMS

9

GAP_PARAM_GAP_TESTCODE

10

GAP_PARAM_SM_TESTCODE

11

GAP_PARAM_GATT_TESTCODE

12

GAP_PARAM_ATT_TESTCODE

13

GAP_PARAM_L2CAP_TESTCODE

14

GAP_PARAM_SET_SCAN_CHAN

Events Generated

When this command is received, the host will send the CommandStatus Event.

GapAdv_create

Opcode:

0xFE3E

Command Description:

Create an advertising set.

Command Parameters

Properties:

Advertising Event Properties bit field

Size:

2 byte(s)

Default:

0x0013

Range:

Value

Description

0x0001

GAP_ADV_PROP_CONNECTABLE

0x0002

GAP_ADV_PROP_SCANNABLE

0x0004

GAP_ADV_PROP_DIRECTED

0x0008

GAP_ADV_PROP_HDC

0x0010

GAP_ADV_PROP_LEGACY

0x0020

GAP_ADV_PROP_ANONYMOUS

0x0040

GAP_ADV_PROP_TX_POWER

Interval Min:
Size:

3 byte(s)

Default:

160

Range:

20 ms to 10,485.759375 s

Interval Max:
Size:

3 byte(s)

Default:

160

Range:

ms to 10,485.759375 s

Primary channel map:
Size:

1 byte(s)

Default:

0x07

Range:

Value

Description

0x01

GAP_ADV_CHAN_37

0x02

GAP_ADV_CHAN_38

0x04

GAP_ADV_CHAN_39

Peer address type:
Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID

0x01

PEER_ADDRTYPE_RANDOM_OR_RANDOM_ID

Peer Address:

Address of the peer. Only applicable for directed advertising.

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value.

Filter Policy:
Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

GAP_ADV_AL_POLICY_ANY_REQ

0x01

GAP_ADV_AL_POLICY_AL_SCAN_REQ

0x02

GAP_ADV_AL_POLICY_AL_CONNECT_IND

0x03

GAP_ADV_AL_POLICY_AL_ALL_REQ

Tx Power:
Size:

1 byte(s)

Default:

127

Range:

0 - 127

Primary PHY:
Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x01

GAP_ADV_PRIM_PHY_1_MBPS

0x03

GAP_ADV_PRIM_PHY_CODED_S8

0x83

GAP_ADV_PRIM_PHY_CODED_S2

Secoondary PHY:
Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x01

GAP_ADV_SEC_PHY_1_MBPS

0x02

GAP_ADV_SEC_PHY_2_MBPS

0x03

GAP_ADV_SEC_PHY_CODED_S8

0x83

GAP_ADV_SEC_PHY_CODED_S2

sid:
Size:

1 byte(s)

Default:

0

Range:

0-15

Events Generated

The host will send the CommandStatus Event to indicate the advertising handle that is associated with this set.

Additional Command Status Return Parameters

length:

Length of data

Size:

1 byte(s)

Range:

handle:

Advertising handle

Size:

1 byte(s)

Range:

GapAdv_enable

Opcode:

0xFE3F

Command Description:

This will attempt to enable advertising for a set identified by the handle. The advertising set must first be created with GapAdv_create.

Command Parameters

handle:

handle of the advertisement set

Size:

1 byte(s)

Default:

0x00

Range:

0x00 - 0xFE

enable options:

Whether to use the max possible duration for advertising, a user specified duration, or a user specified maximum number of events. Note that if the max possible duration is used, the maxEvent parameter is not applicable.

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

GAP_ADV_ENABLE_OPTIONS_USE_MAX

0x01

GAP_ADV_ENABLE_OPTIONS_USE_DURATION

0x02

GAP_ADV_ENABLE_OPTIONS_USE_MAX_EVENTS

duration or max event:
Size:

2 byte(s)

Default:

0x00

Range:

10 ms to 655,540 ms.

Events Generated

The host will send the CommandStatus Event to indicate the advertising handle that is associated with this set. Also, if enabled by GapAdv_setEventMask, GAP_Advertiser/Scanner_Event events with the following event ID’s can be received: GAP_EVT_ADV_START_AFTER_ENABLE after advertising is enabled, GAP_EVT_ADV_START after each advertising set starts, GAP_EVT_ADV_END after each advertising set ends, GAP_EVT_SCAN_REQ_RECEIVED after received scan requests

GapAdv_disable

Opcode:

0xFE40

Command Description:

Disable an active advertising set.

Command Parameters

handle:

handle of the advertisement

Size:

1 byte(s)

Default:

0x00

Range:

0x00 - 0xFE

Events Generated

When this command is received, the host will send the CommandStatus Event to indicate advertising has been disabled.

GapAdv_setParam

Opcode:

0xFE42

Command Description:

Set a parameter for an advertising set by advertising handle.

Command Parameters

handle:

handle of the advertisement set

Size:

1 byte(s)

Default:

0x00

Range:

0x00 - 0x0FE

ParamID:

identification of the data to set

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0

GAP_ADV_PARAM_PROPS

1

GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN

2

GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX

3

GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP

4

GAP_ADV_PARAM_PEER_ADDRESS_TYPE

5

GAP_ADV_PARAM_PEER_ADDRESS

6

GAP_ADV_PARAM_FILTER_POLICY

7

GAP_ADV_PARAM_TX_POWER

8

GAP_ADV_PARAM_PRIMARY_PHY

9

GAP_ADV_PARAM_SECONDARY_PHY

10

GAP_ADV_PARAM_SID

11

GAP_ADV_PARAM_OWN_ADDRESS_TYPE

12

GAP_ADV_PARAM_ZERODELAY

Properties:

Advertising Event Properties bit field

Condition:

( paramID == 0x0)

Size:

2 byte(s)

Default:

0x0013

Range:

Value

Description

0x0001

GAP_ADV_PROP_CONNECTABLE

0x0002

GAP_ADV_PROP_SCANNABLE

0x0004

GAP_ADV_PROP_DIRECTED

0x0008

GAP_ADV_PROP_HDC

0x0010

GAP_ADV_PROP_LEGACY

0x0020

GAP_ADV_PROP_ANONYMOUS

0x0040

GAP_ADV_PROP_TX_POWER

Interval Min:

Minimum advertising interval (n * 0.625 ms)

Condition:

( paramID == 0x1)

Size:

3 byte(s)

Default:

160

Range:

20 ms to 10,485.759375 s

Interval Max:

Maximum advertising interval (n * 0.625 ms). This is currently ignored; the minimum advertising interval will always be used.

Condition:

( paramID == 0x2)

Size:

3 byte(s)

Default:

160

Range:

20 ms to 10,485.759375 s

Primary channel map:

A bit field that indicates the advertising channels that shall be used when transmitting advertising packets on primary channels

Condition:

( paramID == 0x3)

Size:

1 byte(s)

Default:

7

Range:

Value

Description

0x01

GAP_ADV_CHAN_37

0x02

GAP_ADV_CHAN_38

0x04

GAP_ADV_CHAN_39

Peer address type:

Address type of the peer. Only applicable for directed advertising.

Condition:

( paramID == 0x4)

Size:

1 byte(s)

Default:

Public

Range:

Value

Description

0x00

PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID

0x01

PEER_ADDRTYPE_RANDOM_OR_RANDOM_ID

Peer address:

The Peer address for directed advertising.

Condition:

( paramID == 0x5)

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value

Filter Policy:

Advertising filter policy.

Condition:

( paramID == 0x6)

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

GAP_ADV_AL_POLICY_ANY_REQ

0x01

GAP_ADV_AL_POLICY_AL_SCAN_REQ

0x02

GAP_ADV_AL_POLICY_AL_CONNECT_IND

0x03

GAP_ADV_AL_POLICY_AL_ALL_REQ

Tx power:

The maximum power level at which the advertising packets are to be transmitted on the advertising channels. The Controller will choose a power level lower than or equal to this. The range is 0 - 126 or 127 if there is no preference.

Condition:

( paramID == 0x7)

Size:

1 byte(s)

Default:

127

Range:

0-127

Primary PHY:

The PHY on which the advertising packets are transmitted on the primary advertising channels.

Condition:

( paramID == 0x8)

Size:

1 byte(s)

Default:

1

Range:

Value

Description

0x01

GAP_ADV_PRIM_PHY_1_MBPS

0x03

GAP_ADV_PRIM_PHY_CODED_S8

0x83

GAP_ADV_PRIM_PHY_CODED_S2

Secondary PHY:

The PHY on which the advertising packets are transmitted on the secondary advertising channels.

Condition:

( paramID == 0x9)

Size:

1 byte(s)

Default:

1

Range:

Value

Description

0x01

GAP_ADV_SEC_PHY_1_MBPS

0x02

GAP_ADV_SEC_PHY_2_MBPS

0x03

GAP_ADV_SEC_PHY_CODED_S8

0x83

GAP_ADV_SEC_PHY_CODED_S2

SID:

This is the value to be transmitted in the Advertising SID subfield of the ADI field of the Extended Header of those advertising channel PDUs that have an ADI field. If the advertising set only uses PDUs that do not contain an ADI field, this parameter is ignored. The range is 0-15.

Condition:

( paramID == 0xA)

Size:

1 byte(s)

Default:

0

Range:

0-15

addrMode:

Address Mode

Condition:

( paramID == 0xB)

Size:

1 byte(s)

Default:

2

Range:

Value

Description

0x00

ADDRMODE_PUBLIC

0x01

ADDRMODE_RANDOM

0x02

ADDRMODE_RP_WITH_PUBLIC_ID

0x03

ADDRMODE_RP_WITH_RANDOM_ID

zeroDelay:

This is the condition which determines if an extra random delay between advertising sets will be generated. if 0, a delay will be generated. if 1, there will be no extra delay. default - 0.

Condition:

( paramID == 0xC)

Size:

1 byte(s)

Default:

0x0

Range:

Value

Description

0

Disable

1

Enable

Events Generated

The host will send the CommandStatus Event to indicate the parameter has been set.

GapAdv_destroy

Opcode:

0xFE41

Command Description:

Delete an advertising set. This will free any memory associated with the advertising set.

Command Parameters

handle:

handle of the advertisement set to handle

Size:

1 byte(s)

Default:

0x00

Range:

0x00-0xFE

Events Generated

The host will send the CommandStatus Event to indicate the set has been destroyed.

GapAdv_getParam

Opcode:

0xFE43

Command Description:

Get an advertising parameter for an advertising set.

Command Parameters

handle:

handle of the advertisement set to handle

Size:

1 byte(s)

Default:

0x00

Range:

0x00 - 0xFE

paramId:

parameter ID to get

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0

GAP_ADV_PARAM_PROPS

1

GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN

2

GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX

3

GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP

4

GAP_ADV_PARAM_PEER_ADDRESS_TYPE

5

GAP_ADV_PARAM_PEER_ADDRESS

6

GAP_ADV_PARAM_FILTER_POLICY

7

GAP_ADV_PARAM_TX_POWER

8

GAP_ADV_PARAM_PRIMARY_PHY

9

GAP_ADV_PARAM_SECONDARY_PHY

10

GAP_ADV_PARAM_SID

11

GAP_ADV_PARAM_OWN_ADDRESS_TYPE

12

GAP_ADV_PARAM_ZERODELAY

Events Generated

The host will send the CommandStatus Event to return the parameter value in question.

Additional Command Status Return Parameters

length:
Size:

1 byte(s)

Range:

paramId:
Condition:

( StatStatus==0x00)

Size:

1 byte(s)

Range:

Value

Description

0

GAP_ADV_PARAM_PROPS

1

GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN

2

GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX

3

GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP

4

GAP_ADV_PARAM_PEER_ADDRESS_TYPE

5

GAP_ADV_PARAM_PEER_ADDRESS

6

GAP_ADV_PARAM_FILTER_POLICY

7

GAP_ADV_PARAM_TX_POWER

8

GAP_ADV_PARAM_PRIMARY_PHY

9

GAP_ADV_PARAM_SECONDARY_PHY

10

GAP_ADV_PARAM_SID

11

GAP_ADV_PARAM_OWN_ADDRESS_TYPE

12

GAP_ADV_PARAM_ZERODELAY

GAP_ADV_PARAM_PROPS:
Condition:

( StatStatus==0x00 paramId==0x00)

Size:

2 byte(s)

Range:

Value

Description

0x0001

GAP_ADV_PROP_CONNECTABLE

0x0002

GAP_ADV_PROP_SCANNABLE

0x0004

GAP_ADV_PROP_DIRECTED

0x0008

GAP_ADV_PROP_HDC

0x0010

GAP_ADV_PROP_LEGACY

0x0020

GAP_ADV_PROP_ANONYMOUS

0x0040

GAP_ADV_PROP_TX_POWER

GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN:
Condition:

( StatStatus==0x00 paramId==0x01)

Size:

3 byte(s)

Range:

GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX:
Condition:

( StatStatus==0x00 paramId==0x02)

Size:

3 byte(s)

Range:

GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP:
Condition:

( StatStatus==0x00 paramId==0x03)

Size:

1 byte(s)

Range:

Value

Description

0x01

GAP_ADV_CHAN_37

0x02

GAP_ADV_CHAN_38

0x04

GAP_ADV_CHAN_39

GAP_ADV_PARAM_PEER_ADDRESS_TYPE:
Condition:

( StatStatus==0x00 paramId==0x04)

Size:

1 byte(s)

Range:

GAP_ADV_PARAM_PEER_ADDRESS:

Note! The value is byte-reversed.

Condition:

( StatStatus==0x00 paramId==0x05)

Size:

6 byte(s)

Range:

GAP_ADV_PARAM_FILTER_POLICY:
Condition:

( StatStatus==0x00 paramId==0x06)

Size:

1 byte(s)

Range:

Value

Description

0x00

GAP_ADV_AL_POLICY_ANY_REQ

0x01

GAP_ADV_AL_POLICY_AL_SCAN_REQ

0x02

GAP_ADV_AL_POLICY_AL_CONNECT_IND

0x03

GAP_ADV_AL_POLICY_AL_ALL_REQ

GAP_ADV_PARAM_TX_POWER:
Condition:

( StatStatus==0x00 paramId==0x07)

Size:

1 byte(s)

Range:

GAP_ADV_PARAM_PRIMARY_PHY:
Condition:

( StatStatus==0x00 paramId==0x08)

Size:

1 byte(s)

Range:

Value

Description

0x01

GAP_ADV_PRIM_PHY_1_MBPS

0x03

GAP_ADV_PRIM_PHY_CODED_S8

0x83

GAP_ADV_PRIM_PHY_CODED_S2

GAP_ADV_PARAM_SECONDARY_PHY:
Condition:

( StatStatus==0x00 paramId==0x09)

Size:

1 byte(s)

Range:

Value

Description

0x01

GAP_ADV_SEC_PHY_1_MBPS

0x02

GAP_ADV_SEC_PHY_2_MBPS

0x03

GAP_ADV_SEC_PHY_CODED_S8

0x83

GAP_ADV_SEC_PHY_CODED_S2

GAP_ADV_PARAM_SID:
Condition:

( StatStatus==0x00 paramId==0x0A)

Size:

1 byte(s)

Range:

GAP_ADV_PARAM_OWN_ADDRESS_TYPE:
Condition:

( StatStatus==0x00 paramId==0x0B)

Size:

1 byte(s)

Range:

GAP_ADV_PARAM_ZERODELAY:
Condition:

( StatStatus==0x00 paramId==0x0C)

Size:

1 byte(s)

Range:

Value

Description

0

Disable

1

Enable

GapAdv_loadData

Opcode:

0xFE44

Command Description:

Load advertising or scan response data to an advertising set by handle.

Command Parameters

Layer:
Size:

1 byte(s)

Value:

9

Event Opcode:
Size:

2 byte(s)

Value:

0xFE44

Payload Length:
Size:

2 byte(s)

Value:

size(HandleLen)+size(type)+size(LengthLen)+size(dataLen)

Handle:

Handle of the advertisement set

Size:

1 byte(s)

Default:

0x00

Range:

0x00 - 0xFE

type:

Type of Data to Load

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0

GAP_ADV_DATA_TYPE_ADV

1

GAP_ADV_DATA_TYPE_SCAN_RSP

Data length:

The number of bytesthe Advertising Data parameter

Size:

2 byte(s)

Default:

16

Range:

0-251

Adv Data:

Data

Size:

input byte(s)

Default:

“00:01:02:03:04:05:06:07:08:09:0A:0B:0C:0D:0E:0F”

Range:

This parameter has a variable length.

Events Generated

The host will send the CommandStatus Event to indicate the data has been loaded.

GapAdv_setEventMask

Opcode:

0xFE45

Command Description:

Set the per-advertising set event mask to select which events are sent

Command Parameters

handle:

handle of the advertisement set to handle

Size:

1 byte(s)

Default:

0x00

Range:

0x00 - 0xFE

Event Mask:

Bitfield to enable / disable callback events:

Size:

2 byte(s)

Default:

0x0000

Range:

Value

Description

0x01

GAP_EVT_SCAN_REQ_RECEIVED

0x02

GAP_EVT_ADV_SET_TERMINATED

0x10

GAP_EVT_ADV_START_AFTER_ENABLE

0x20

GAP_EVT_ADV_START

0x40

GAP_EVT_ADV_END

0x80

GAP_EVT_ADV_END_AFTER_DISABLE

Events Generated

The host will send the CommandStatus Event to indicate the event mask has been set.

GapAdv_setVirtualAdvAddr

Opcode:

0xFE4B

Command Description:

Set the advertiser’s virtual public address. This api shuold be used after a handle was created using GapAdv_create and before enabling the advertise set using GapAdv_enable. Setting virtual address is allowed only for Legacy Non-Connectable and Non-Scanable PDUs.

Command Parameters

Handle:

Adv handle to which address will be assigned

Size:

1 byte(s)

Default:

“0”

Range:

From 0 to 20 sets

BDADDR:

Advertiser’s virtual public address

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value

Events Generated

The host will send the CommandStatus Event to indicate that the virtual address was associated

GapScan_enable

Opcode:

0xFE51

Command Description:

Start scanning.

Command Parameters

period:

scan period in 1.28 sec. Ignore if duration is 0

Size:

2 byte(s)

Default:

0

Range:

1-65535

duration:

scan duration in 10 ms. If 0, scanning will not end until GapScan_disable is called. the time of scan duration shall be greater than the time of scan window.

Size:

2 byte(s)

Default:

500

Range:

1-65535

max number of records:

if non-zero, up to this number of adv reports will be recoreded during scanning

Size:

1 byte(s)

Default:

40

Range:

1-65535 or until the heap is exhausted

Events Generated

The host will send the CommandStatus Event to indicate the scan has started

GapScan_disable

Opcode:

0xFE52

Command Description:

Stop the currently running scanning operation.

Events Generated

The host will send the CommandStatus Event to indicate the scan has ended.

GapScan_setPhyParams

Opcode:

0xFE53

Command Description:

Set parameters dependent on PHY. Note that if primPhys contains more than one PHY, the same parameters of those PHYs will be set with the same values.

Command Parameters

primPhy:

PHY(s) to use on primary advertising channels

Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x01

SCAN_PRIM_PHY_1M

0x04

SCAN_PRIM_PHY_CODED

type:

scan type

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

SCAN_TYPE_PASSIVE

0x01

SCAN_TYPE_ACTIVE

interval:

scan interval in 625-us unit. shall be equal to or greater than window.

Size:

2 byte(s)

Default:

800

Range:

4-16384

window:

scan window in 625-us unit

Size:

2 byte(s)

Default:

800

Range:

4-16384

Events Generated

The host will send the CommandStatus Event to indicate the phy parameters have been set.

GapScan_getPhyParams

Opcode:

0xFE54

Command Description:

Get parameters of the specified PHY. Note that primPhy shall indicate only one PHY.

Command Parameters

primPhy:

PHY to retrieve parameters relevant to

Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x01

SCAN_PRIM_PHY_1M

0x04

SCAN_PRIM_PHY_CODED

Events Generated

The host will send the CommandStatus Event to return the parameter value in question.

Additional Command Status Return Parameters

length:

Length of data

Size:

1 byte(s)

Range:

type:

Scan type

Size:

1 byte(s)

Range:

Value

Description

0x00

SCAN_TYPE_PASSIVE

0x01

SCAN_TYPE_ACTIVE

interval:

Scan Interval

Size:

2 byte(s)

Range:

window:

Scan window

Size:

2 byte(s)

Range:

GapScan_setParam

Opcode:

0xFE55

Command Description:

Set a scan parameter.

Command Parameters

paramID:

Parameter ID

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

SCAN_PARAM_RPT_FIELDS

0x01

SCAN_PARAM_PRIM_PHYS

0x02

SCAN_PARAM_FLT_POLICY

0x03

SCAN_PARAM_FLT_PDU_TYPE

0x04

SCAN_PARAM_FLT_MIN_RSSI

0x05

SCAN_PARAM_FLT_DISC_MODE

0x06

SCAN_PARAM_FLT_DUP

0x07

SCAN_PARAM_NUM_ADV_RPT (Read-only)

SCAN_PARAM_RPT_FIELDS:

Fields of advertising report to keep in the list

Condition:

( paramID == 0x0)

Size:

2 byte(s)

Default:

0x08a7

Range:

Value

Description

0x0001

SCAN_ADVRPT_FLD_EVENTTYPE

0x0002

SCAN_ADVRPT_FLD_ADDRTYPE

0x0004

SCAN_ADVRPT_FLD_ADDRESS

0x0008

SCAN_ADVRPT_FLD_PRIMPHY

0x0010

SCAN_ADVRPT_FLD_SECPHY

0x0020

SCAN_ADVRPT_FLD_ADVSID

0x0040

SCAN_ADVRPT_FLD_TXPOWER

0x0080

SCAN_ADVRPT_FLD_RSSI

0x0100

SCAN_ADVRPT_FLD_DIRADDRTYPE

0x0200

SCAN_ADVRPT_FLD_DIRADDRESS

0x0400

SCAN_ADVRPT_FLD_PRDADVINTERVAL

0x0800

SCAN_ADVRPT_FLD_DATALEN

SCAN_PARAM_PRIM_PHYS:

PHY to scan for on the primary channels

Condition:

( paramID == 0x1)

Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x01

SCAN_PRIM_PHY_1M

0x04

SCAN_PRIM_PHY_CODED

SCAN_PARAM_FLT_POLICY:

Acceptlist filter policy

Condition:

( paramID == 0x2)

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

SCAN_FLT_POLICY_ALL

0x01

SCAN_FLT_POLICY_AL

0x02

SCAN_FLT_POLICY_ALL_RPA

0x03

SCAN_FLT_POLICY_AL_RPA

SCAN_PARAM_FLT_PDU_TYPE:

Filter by PDU types

Condition:

( paramID == 0x3)

Size:

2 byte(s)

Default:

0x0800

Range:

Value

Description

0x0001

SCAN_FLT_PDU_NONCONNECTABLE_ONLY

0x0002

SCAN_FLT_PDU_CONNECTABLE_ONLY

0x0004

SCAN_FLT_PDU_NONSCANNABLE_ONLY

0x0008

SCAN_FLT_PDU_SCANNABLE_ONLY

0x0010

SCAN_FLT_PDU_UNDIRECTED_ONLY

0x0020

SCAN_FLT_PDU_DIRECTED_ONLY

0x0040

SCAN_FLT_PDU_ADV_ONLY

0x0080

SCAN_FLT_PDU_SCANRSP_ONLY

0x0100

SCAN_FLT_PDU_EXTENDED_ONLY

0x0200

SCAN_FLT_PDU_LEGACY_ONLY

0x0400

SCAN_FLT_PDU_TRUNCATED_ONLY

0x0800

SCAN_FLT_PDU_COMPLETE_ONLY

SCAN_PARAM_FLT_MIN_RSSI:

Filter by RSSI. Note this is a signed one-byte value.

Condition:

( paramID == 0x4)

Size:

1 byte(s)

Default:

-128

Range:

-128 - 127

SCAN_PARAM_FLT_DISC_MODE:

Filter by discoverable mode

Condition:

( paramID == 0x5)

Size:

1 byte(s)

Default:

0x04

Range:

Value

Description

0x00

SCAN_FLT_DISC_NONE

0x01

SCAN_FLT_DISC_GENERAL

0x02

SCAN_FLT_DISC_LIMITED

0x03

SCAN_FLT_DISC_ALL

0x04

SCAN_FLT_DISC_DISABLE

SCAN_PARAM_FLT_DUP:

Duplicate Filter

Condition:

( paramID == 0x6)

Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x00

SCAN_FLT_DUP_DISABLE

0x01

SCAN_FLT_DUP_ENABLE

0x02

SCAN_FLT_DUP_RESET (Duplicate filtering enabled, reset for each scan period)

Events Generated

The host will send the CommandStatus Event to indicate the parameter has been set.

GapScan_getParam

Opcode:

0xFE56

Command Description:

Set a scan parameter.

Command Parameters

paramID:

Parameter ID

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

SCAN_PARAM_RPT_FIELDS

0x01

SCAN_PARAM_PRIM_PHYS

0x02

SCAN_PARAM_FLT_POLICY

0x03

SCAN_PARAM_FLT_PDU_TYPE

0x04

SCAN_PARAM_FLT_MIN_RSSI

0x05

SCAN_PARAM_FLT_DISC_MODE

0x06

SCAN_PARAM_FLT_DUP

0x07

SCAN_PARAM_NUM_ADV_RPT (Read-only)

Events Generated

The host will send the CommandStatus Event to return the parameter value in question.

Additional Command Status Return Parameters

length:

Length of data

Size:

1 byte(s)

Range:

paramId:
Condition:

( StatStatus==0x00)

Size:

1 byte(s)

Range:

Value

Description

0x00

SCAN_PARAM_RPT_FIELDS

0x01

SCAN_PARAM_PRIM_PHYS

0x02

SCAN_PARAM_FLT_POLICY

0x03

SCAN_PARAM_FLT_PDU_TYPE

0x04

SCAN_PARAM_FLT_MIN_RSSI

0x05

SCAN_PARAM_FLT_DISC_MODE

0x06

SCAN_PARAM_FLT_DUP

0x07

SCAN_PARAM_NUM_ADV_RPT (Read-only)

SCAN_PARAM_RPT_FIELDS:
Condition:

( StatStatus==0x00 paramId==0x00)

Size:

2 byte(s)

Range:

Value

Description

0x0001

SCAN_ADVRPT_FLD_EVENTTYPE

0x0002

SCAN_ADVRPT_FLD_ADDRTYPE

0x0004

SCAN_ADVRPT_FLD_ADDRESS

0x0008

SCAN_ADVRPT_FLD_PRIMPHY

0x0010

SCAN_ADVRPT_FLD_SECPHY

0x0020

SCAN_ADVRPT_FLD_ADVSID

0x0040

SCAN_ADVRPT_FLD_TXPOWER

0x0080

SCAN_ADVRPT_FLD_RSSI

0x0100

SCAN_ADVRPT_FLD_DIRADDRTYPE

0x0200

SCAN_ADVRPT_FLD_DIRADDRESS

0x0400

SCAN_ADVRPT_FLD_PRDADVINTERVAL

0x0800

SCAN_ADVRPT_FLD_DATALEN

SCAN_PARAM_PRIM_PHYS:
Condition:

( StatStatus==0x00 paramId==0x01)

Size:

1 byte(s)

Range:

Value

Description

0x01

SCAN_PRIM_PHY_1M

0x04

SCAN_PRIM_PHY_CODED

SCAN_PARAM_FLT_POLICY:
Condition:

( StatStatus==0x00 paramId==0x02)

Size:

1 byte(s)

Range:

Value

Description

0x00

SCAN_FLT_POLICY_ALL

0x01

SCAN_FLT_POLICY_AL

0x02

SCAN_FLT_POLICY_ALL_RPA

0x03

SCAN_FLT_POLICY_AL_RPA

SCAN_PARAM_FLT_PDU_TYPE:
Condition:

( StatStatus==0x00 paramId==0x03)

Size:

2 byte(s)

Range:

Value

Description

0x0001

SCAN_FLT_PDU_NONCONNECTABLE_ONLY

0x0002

SCAN_FLT_PDU_CONNECTABLE_ONLY

0x0004

SCAN_FLT_PDU_NONSCANNABLE_ONLY

0x0008

SCAN_FLT_PDU_SCANNABLE_ONLY

0x0010

SCAN_FLT_PDU_UNDIRECTED_ONLY

0x0020

SCAN_FLT_PDU_DIRECTED_ONLY

0x0040

SCAN_FLT_PDU_ADV_ONLY

0x0080

SCAN_FLT_PDU_SCANRSP_ONLY

0x0100

SCAN_FLT_PDU_EXTENDED_ONLY

0x0200

SCAN_FLT_PDU_LEGACY_ONLY

0x0400

SCAN_FLT_PDU_TRUNCATED_ONLY

0x0800

SCAN_FLT_PDU_COMPLETE_ONLY

SCAN_PARAM_FLT_MIN_RSSI:
Condition:

( StatStatus==0x00 paramId==0x04)

Size:

1 byte(s)

Range:

SCAN_PARAM_FLT_DISC_MODE:
Condition:

( StatStatus==0x00 paramId==0x05)

Size:

1 byte(s)

Range:

Value

Description

0x00

SCAN_FLT_DISC_NONE

0x01

SCAN_FLT_DISC_GENERAL

0x02

SCAN_FLT_DISC_LIMITED

0x03

SCAN_FLT_DISC_ALL

0x04

SCAN_FLT_DISC_DISABLE

SCAN_PARAM_FLT_DUP:
Condition:

( StatStatus==0x00 paramId==0x06)

Size:

1 byte(s)

Range:

Value

Description

0x00

SCAN_FLT_DUP_DISABLE

0x01

SCAN_FLT_DUP_ENABLE

0x02

SCAN_FLT_DUP_RESET (Duplicate filtering enabled, reset for each scan period)

SCAN_PARAM_NUM_ADV_RPT:
Condition:

( StatStatus==0x00 paramId==0x07)

Size:

1 byte(s)

Range:

GapScan_setEventMask

Opcode:

0xFE57

Command Description:

Set which events to receive through the callback. One bit per event. If a bit is set to 1, the callback provided by GapScan_registerCb() will be called upon corresponding event.

Command Parameters

eventMask:

The mask receive the wanted scan events

Size:

4 byte(s)

Default:

0x00C30000

Range:

Value

Description

0x00010000

GAP_EVT_SCAN_ENABLED

0x00020000

GAP_EVT_SCAN_DISABLED

0x00040000

GAP_EVT_SCAN_PRD_ENDED

0x00080000

GAP_EVT_SCAN_DUR_ENDED

0x00100000

GAP_EVT_SCAN_INT_ENDED

0x00200000

GAP_EVT_SCAN_WND_ENDED

0x00400000

GAP_EVT_ADV_REPORT

0x00800000

GAP_EVT_ADV_REPORT_FULL

0x01000000

GAP_EVT_PRD_ADV_SYNC_ESTABLISHED

0x02000000

GAP_EVT_PRD_ADV_REPORT

0x04000000

GAP_EVT_PRD_ADV_SYNC_LOST

Events Generated

The host will send the CommandStatus Event to indicate the event mask has been set.

GapScan_getAdvReport

Opcode:

0xFE58

Command Description:

Get a specific advertising report from the advertising report list. Only the fields specified by GapScan_setParam(SCAN_PARAM_RPT_FIELDS, ..) will be filled out. All other fields will be filled with 0s.

Command Parameters

rptIdx:

the index of the report to retrieve (number of reports available is returned by the GapScan_disable)

Size:

1 byte(s)

Default:

0

Range:

0-maxNumReport as set by GapScan_enable

Events Generated

The host will send the CommandStatus Event to return the advertising report.

Additional Command Status Return Parameters

length:

Length of data

Size:

1 byte(s)

Range:

evtType:
Size:

1 byte(s)

Range:

addrType:
Size:

1 byte(s)

Range:

Value

Description

0x00

ADDRTYPE_PUBLIC

0x01

ADDRTYPE_RANDOM

0x02

ADDRTYPE_PUBLIC_ID

0x03

ADDRTYPE_RANDOM_ID

0xFE

ADDRTYPE_RANDOM_NR

0xFF

ADDRTYPE_NONE

addr:
Size:

6 byte(s)

Range:

primPhy:
Size:

1 byte(s)

Range:

Value

Description

0x00

SCANNED_PHY_NONE

0x01

SCANNED_PHY_1M

0x02

SCANNED_PHY_2M

0x03

SCANNED_PHY_CODED

secPhy:
Size:

1 byte(s)

Range:

Value

Description

0x00

SCANNED_PHY_NONE

0x01

SCANNED_PHY_1M

0x02

SCANNED_PHY_2M

0x03

SCANNED_PHY_CODED

advSid:
Size:

1 byte(s)

Range:

txPower:
Size:

1 byte(s)

Range:

rssi:
Size:

1 byte(s)

Range:

directAddrType:
Size:

1 byte(s)

Range:

Value

Description

0x00

ADDRTYPE_PUBLIC

0x01

ADDRTYPE_RANDOM

0x02

ADDRTYPE_PUBLIC_ID

0x03

ADDRTYPE_RANDOM_ID

0xFE

ADDRTYPE_RANDOM_NR

0xFF

ADDRTYPE_NONE

directAddr:
Size:

6 byte(s)

Range:

GapInit_setPhyParam

Opcode:

0xFE60

Command Description:

Set parameters dependent on PHY. Note that if phys contains more than one PHY, the same parameter of those PHYs will be set with the same value.

Command Parameters

phy:

PHY(s) to set parameter of

Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x01

INIT_PHY_1M

0x02

INIT_PHY_2M

0x04

INIT_PHY_CODED

paramId:

parameter ID

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

INIT_PHYPARAM_SCAN_INTERVAL

0x01

INIT_PHYPARAM_SCAN_WINDOW

0x02

INIT_PHYPARAM_CONN_INT_MIN

0x03

INIT_PHYPARAM_CONN_INT_MAX

0x04

INIT_PHYPARAM_CONN_LATENCY

0x05

INIT_PHYPARAM_SUP_TIMEOUT

INIT_PHYPARAM_SCAN_INTERVAL:

scan interval in 625-us unit

Condition:

( paramID == 0x0)

Size:

2 byte(s)

Default:

16

Range:

4-16384

INIT_PHYPARAM_SCAN_WINDOW:

scan window in 625-us unit

Condition:

( paramID == 0x1)

Size:

2 byte(s)

Default:

16

Range:

4-16384

INIT_PHYPARAM_CONN_INT_MIN:

minimum connection interval in 1.25-ms unit

Condition:

( paramID == 0x2)

Size:

2 byte(s)

Default:

80

Range:

6-3200

INIT_PHYPARAM_CONN_INT_MAX:

maximum connection interval in 1.25-ms unit

Condition:

( paramID == 0x3)

Size:

2 byte(s)

Default:

80

Range:

0 - 499

INIT_PHYPARAM_CONN_LATENCY:

connection latency

Condition:

( paramID == 0x4)

Size:

2 byte(s)

Default:

0

Range:

10 - 3200

INIT_PHYPARAM_SUP_TIMEOUT:

supervision timeout in 10-ms unit

Condition:

( paramID == 0x5)

Size:

2 byte(s)

Default:

2000

Range:

0 - 0xFFFF

Events Generated

The host will send the CommandStatus Event to indicate the parameter has been set.

GapInit_getPhyParam

Opcode:

0xFE61

Command Description:

Get parameters of the specified PHY. Note that phy shall indicate only one PHY.

Command Parameters

phy:

PHY to get parameter of

Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x01

INIT_PHY_1M

0x02

INIT_PHY_2M

0x04

INIT_PHY_CODED

paramId:

Parameter ID

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

INIT_PHYPARAM_SCAN_INTERVAL

0x01

INIT_PHYPARAM_SCAN_WINDOW

0x02

INIT_PHYPARAM_CONN_INT_MIN

0x03

INIT_PHYPARAM_CONN_INT_MAX

0x04

INIT_PHYPARAM_CONN_LATENCY

0x05

INIT_PHYPARAM_SUP_TIMEOUT

Events Generated

The host will send the CommandStatus Event to return the parameter value in question.

Additional Command Status Return Parameters

length:

Length of data

Size:

1 byte(s)

Range:

paramId:

Parameter ID

Size:

1 byte(s)

Range:

Value

Description

0x00

INIT_PHYPARAM_SCAN_INTERVAL

0x01

INIT_PHYPARAM_SCAN_WINDOW

0x02

INIT_PHYPARAM_CONN_INT_MIN

0x03

INIT_PHYPARAM_CONN_INT_MAX

0x04

INIT_PHYPARAM_CONN_LATENCY

0x05

INIT_PHYPARAM_SUP_TIMEOUT

INIT_PHYPARAM_SCAN_INTERVAL:

Phy

Condition:

( paramId==0x00)

Size:

2 byte(s)

Range:

INIT_PHYPARAM_SCAN_WINDOW:
Condition:

( paramId==0x01)

Size:

2 byte(s)

Range:

INIT_PHYPARAM_CONN_INT_MIN:
Condition:

( paramId==0x02)

Size:

2 byte(s)

Range:

INIT_PHYPARAM_CONN_INT_MAX:
Condition:

( paramId==0x03)

Size:

2 byte(s)

Range:

INIT_PHYPARAM_CONN_LATENCY:
Condition:

( paramId==0x04)

Size:

2 byte(s)

Range:

INIT_PHYPARAM_SUP_TIMEOUT:
Condition:

( paramId==0x05)

Size:

2 byte(s)

Range:

GapInit_connect

Opcode:

0xFE62

Command Description:

Initiate connection with the specified peer device

Command Parameters

peerAddrType:

peer device’s address type

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID

0x01

PEER_ADDRTYPE_RANDOM_OR_RANDOM_ID

pPeerAddress:

peer device’s address

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value

phys:

PHY(s) to use for connection

Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x01

INIT_PHY_1M

0x02

INIT_PHY_2M

0x04

INIT_PHY_CODED

timeout:

initiating timeout in ms

Size:

2 byte(s)

Default:

0

Range:

Any 32-bit number

Events Generated

The host will send the CommandStatus Event to indicate whether the connect process has started successfully. If a connection is formed, the GAP_LinkEstablished event will be returned.

GapInit_connectAl

Opcode:

0xFE63

Command Description:

Initiate connection with a device in the acceptlist.

Command Parameters

phys:

PHY(s) to use for connection

Size:

1 byte(s)

Default:

0x01

Range:

Value

Description

0x01

INIT_PHY_1M

0x02

INIT_PHY_2M

0x04

INIT_PHY_CODED

timeout:

initiating timeout in ms

Size:

2 byte(s)

Default:

0

Range:

Any 32-bit number

Events Generated

The host will send the CommandStatus Event to indicate whether the connect process has started successfully. If a connection is formed, the GAP_LinkEstablished event will be returned

GapInit_cancelConnect

Opcode:

0xFE64

Command Description:

Cancel the ongoing connection process.

Events Generated

The host will send the CommandStatus Event to indicate whether the connect cancel process has started successfully. If the cancel completes, the GAP_ConnectingCancelled event will be returned.