TI BLE5-Stack 9.14.00 Release Notes

Table of Contents

Introduction

The BLE-Stack is a set of sample applications, tools, APIs and protocol stack libraries that enable engineers to develop Bluetooth ® LE standalone or network processor LE applications on the SimpleLink™ CC23xx family and the SimpleLink™ CC27xx family of wireless MCUs.

Key features overview of BLE-Stack 9.14.00:

BLE Features Support Status
Legacy advertising Supported
Connection using the LE 1M PHY Supported
Pairing and link encryption Supported
Bonding Supported
Accept list for advertiser Supported
Direct Test Mode (DTM) Supported
L2CAP Connection Oriented Channels (CoC) Supported
Extended advertising Supported
LE 2M and Coded PHYs Supported
Privacy Supported
Adjustable TX Power Supported
RSSI Reading Supported
Over The Air Download Supported
LE Secure Connection Supported
Data Length Extension (DLE) Supported
Periodic Advertising Supported
Periodic Scanning Supported
Adaptivity Supported (China MIIT and EU RED Regulation)
LE Power Control Preview (Not yet certified)
Channel Sounding Supported *
RAS/RAP Server/Client Preview (Not yet certified)
Direction Finding (AoA) Not Supported (Planned for a future release)

The BLE-Stack provides a set of basic examples designed to accelerate customer product development providing easy-to-use, out-of-the-box demonstrations of the full hardware capabilities.

Available Examples (CC23xx) Description
basic_ble Example project where the device can be configured to operate as a Bluetooth LE peripheral, central, or both.
basic_ble_extctrl Example that implements connection handover used to control a device running basic_ble device through external commands sent over UART.
basic_ble_oad_offchip Same as basic_ble with OAD off-chip functionality to enable wireless firmware updates.
basic_ble_oad_onchip Same as basic_ble with OAD on-chip functionality to enable wireless firmware updates.
basic_ble_profiles Same as basic_ble with additional custom profiles: Continuous Glucose Monitoring and Glucose Profile & Health Thermometer Profile.
basic_ble_ptm Same as basic_ble with Production Test Mode (PTM) functionality.
basic_dual_image Same as basic_ble with OAD dual image functionality.
basic_persistent Example project that implements OAD profile.
ble_controller Example project that implements the Bluetooth LE controller layer.
car_node Example project to support Channel Sounding, BLE Handover, and Connection Monitor Role only available for CC2340R53 device. Used with key_node example project.
data_stream Example project which implements data stream profile to enable UART over Bluetooth LE.
key_node Example project to support Channel Sounding, used with car_node example project.
host_test Example project which can be used with Bluetooth Tester through UART or SPI.
Available Examples (CC27xx) Description
basic_ble Example project where the device can be configured to operate as a Bluetooth LE peripheral, central, or both.
basic_ble_extctrl Example that implements connection handover used to control a device running basic_ble device through external commands sent over UART.
basic_ble_oad_onchip Same as basic_ble with OAD on-chip functionality to enable wireless firmware updates.
basic_ble_profiles Same as basic_ble with additional custom profiles: Continuous Glucose Monitoring and Glucose Profile & Health Thermometer Profile.
basic_ble_oad_dual_image Same as basic_ble with OAD dual image functionality.
basic_persistent Example project that implements OAD profile.
data_stream Example project which implements data stream profile to enable UART over Bluetooth LE.
ble_controller Example project that implements the Bluetooth LE controller layer.
car_node Example project to support Channel Sounding, BLE Handover, and Connection Monitor Role. Used with key_node example project.
key_node Example project to support Channel Sounding, used with car_node example project.
host_test Example project which can be used with Bluetooth Tester through UART or SPI.

Examples showcasing support for Apple® Find My® Network are available in the Find My Network Accessory Protocol (FMNAP) Plugin for SimpleLink devices (SIMPLELINK-LOWPOWER-FMNAP). Access to the plugin requires an MFi license and a myTI account. Access requests should be filled through the online request form.

Additional information about TI’s Bluetooth Low Energy solutions can be found at www.ti.com/ble

BLE-Stack Documentation

The SimpleLink™ Low Power F3 Software Development Kit (SDK) allows easier product development by combining TI-drivers and the Bluetooth LE protocol stack in one unified SDK. All BLE-Stack sample applications are based off the FreeRTOS Kernel. Key documents needed for Bluetooth LE application development include:

Installation and Usage

What’s New

ID Summary
BLE_LOKI-3603 Add support for LP-EM-C2755R10-BG for BLE examples
BLE_LOKI-3600 Allow Configuration of Number of Thread Priorities with BLE Thread Defaulting to Highest Priority
BLE_LOKI-1945 L2CAP to Signal application When Peer sends L2CAP Credits

Fixed Issues

ID Summary
BLE_LOKI-3773 ICALL Thread Task Priority Adjustment
BLE_LOKI-3768 Timer Double Abort Potential Issue within Car Node Example Project
BLE_LOKI-3757 Connection handover data size is abnormally large on SDK 9.14
BLE_LOKI-3755 Channel Sounding Repetition Termination Mechanism Fixes
BLE_LOKI-3723 Wrong Result Format due to Memory Corruption when using Channel Sounding Repeat Procedures
BLE_LOKI-3716 Channel Sounding Procedure Enable Fails for Coded Phy in all Modes
BLE_LOKI-3657 Unexpected Behavior in First Channel Sounding Distance Events Following Reconnection
BLE_LOKI-3330 Channel Sounding Procedure Repetition Termination is not supported
BLE_LOKI-3224 CS TPM is limited to 40us and offset is increased to 1.5ms
BLE_LOKI-3209 Potential Memory Leak while Running Fuzz Test with L2CAP Connection, Configuration and Disconnection Packets
BLE_LOKI-3172 L2CAP Channel is not established after connection is handed over backwards, when devices are not Paired
BLE_LOKI-3154 Channel Sounding Procedure Repetitions stops if connection event fails

Known Issues and Limitations

ID Summary
BLE_LOKI-3724 IAR Compiler Error when Compiling Basic_persistent on CC2340 Devices
BLE_LOKI-3676 Channel Sounding Timeout Distance Events for Mode 3 with 2x2 Antennas
BLE_LOKI-3536 If parameter update or channel map update w/ CSA#1 is from the past - Connection Monitor will terminate
BLE_LOKI-3535 Connection Monitor Cannot properly track connection on Coded PHY
BLE_LOKI-3473 IAR Compiled Car Node and Key Node Executing Channel Sounding in Loops Causes GAP Link Termination
BLE_LOKI-3429 No Distance is Received after 160 to 255 CS Procedures using RAS over Indications
BLE_LOKI-3389 CS procedure must be complete before starting the next one
BLE_LOKI-3236 Calling HCI_ResetCmd Causes Program to Crash
BLE_LOKI-3208 BLE Agent GUI not able to calculate time offset correctly when running connection handover demo which causes frequent unsuccessful handover sessions
BLE_LOKI-3177 [SWAT] Observer failed to receive GAP_EVT_SCAN_DISABLED event
BLE_LOKI-3097 After changing PHY both devices continue to send Power Reporting events
BLE_LOKI-2978 Connnection Handover AuthenticationComplete Event Received after Handover When Candidate Configured To Initiate Pairing Request
BLE_LOKI-2842 CC23XX and CC27XX family of devices rounds down Tx power values that are not in the power table
BLE_LOKI-2650 CC2745R10Q1 Central Role Fails to Switch Connection PHY to Coded While Holding 16 Connections
BLE_LOKI-2648 Connection may be unstable with Coded PHY when Access Address has high cross-correlation with the preamble
BLE_LOKI-2373 CC2340R5 MAX periodic adv list size is hard coded and can't be configure by SysConfig
BLE_LOKI-2358 CC2340R5 Basic MR printed peripheral initial RPA after bond and pair, instead of its Public Address
BLE_LOKI-2108 Specific smart phone doesn't find peer running extended ADV with secondary PHY of 1M
BLE_LOKI-1630 Extended Advertisement Reports Are Not Filtered When SCAN_PARAM_FLT_DUP is Enabled

Upgrade and Compatibility Information

No support for previous silicon revisions or LaunchPad™ development kits using earlier silicon revision. If you’re unsure of the revision number of your device, please see the Package Symbolization and Revision Identification section of the Errata Note.

The following compilers are supported (see the SDK release notes for specific version numbers):

Qualification

The applicable Design Number for this release is for CC23XX Design Number Q301991 and for CC27XX Design Number Q371076

Please take a look at the following application note for further details on How to Certify Your Bluetooth Product.

Dependencies

The correct dependencies for this SDK release must be used to ensure proper functionality of the software and compatibility with the hardware. Using incorrect dependencies will very likely lead to unintended and unexpected behavior. See top-level release notes for overall SDK dependencies.

Device Support

This release supports development of single-mode Bluetooth LE applications on 2.4 GHz wireless MCUs listed in the top-level SDK release.

Development Board Support

This release supports development of single-mode Bluetooth LE on 2.4 GHz wireless MCU development kits listed in the top-level SDK release notes.

Versioning

This product follows a version format, M.mm.pp.bb, where:

Product Security Vulnerabilities

Technical Support and Product Updates