BLE5-Stack SysConfig Features

Warning

SysConfig integration for BLE5-Stack examples is not yet complete. As such, certain configurations settings may be generated by SysConfig, but not used by the application. Please modify the application file sources directly as needed to work around this.

Checking if SysConfig is used for BLE

Projects that are using SysConfig to configure BLE will have a green check mark next to BLE as shown in the green rectangle.

../_images/ble5_sysconfig_enabled-cc23xx.png

Figure 221. Check for SysConfig enabled example applications

Note

Get started with SysConfig provides an overview of what Sysconfig is and how to get started with it. Please take a look at this if you have not already.

Get started with SysConfig enabled BLE5-Stack projects

After importing a SysConfig enabled BLE5-Stack project into CCS, by double clicking on the *.syscfg file, a GUI will appear where the project can be configured more easily. A number of BLE5-Stack configurable features are included in this GUI. Figure 222. shows what this looks like when importing the basic_ble example.

../_images/syscfg_after_import-basicble.png

Figure 222. After Import

Figure 222. Also shows many different configurable parameters for the project. The first few configurable options inside the Software -> BLE panel are as shown below. The generated file name for the BLE5-Stack feature is ti_build_config.opt.

../_images/ble5_sysconfig_stack_feature-cc23xx.png

Figure 223. Stack Feature

The Device Role configurable is an example of a drop down list where you can select the specific Device Role you wish to use. Device Role refers to the GAP Roles that the project operates as. This can be seen in Figure 224. There are many different options with different input methods available.

../_images/syscfg_role_combinations-cc23xx.png

Figure 224. Device Role

When you first open a SysConfig project all of the settings for that project will be at their default values that are known to work with that example. Providing this amount of quick and easy configuration for a project is powerful. However, as we know, with great power comes great responsibility. Any one specific example is not guaranteed to function properly with any and all permutations of the available configurable options. More specifically, BLE5-Stack projects are written to implement one (or more) specific Generic Access Profile (GAP) Role Combinations, so one should not switch this unless you know what you’re doing. As long as the files that are generated from your input compile, the project will build. Whether or not it performs to the same degree depends on what you changed the options to.

Furthermore, the options that are available to modify will depend on the GAP Roles that have been selected. Changing the Device Role may add or remove options below it. If changing the Device Role option is required, it is suggested to change this first so that you do not lose any work you have already done below.

Open the SysConfig output (see Viewing SysConfig Output). After selecting a file you will be able, in real-time, to identify how the changes in the GUI effect the generated files. This will help you review the relationship between the GUI and the code.

../_images/syscfg_code_review-cc23xx.png

Figure 225. Code Review

Note

Changes will appear as a diff in the code view. Changes will be applied when the project is rebuilt.

Additional Configuration Categories

Note

Remember that the following Configuration Categories will depend on the Role Combination (GAP Roles) you’ve chosen. Change Role Combination before changing any of the below options.

General Configurations

../_images/syscfg_general_configurations-cc23xx.png

Figure 226. General Configurations

Bond Manager

These settings control all the bond manager parameters and generate the function setBondManagerParameters() in ti_ble_config.c file. This function sets all the bond manager parameters as configured by SysConfig, and should be called from the main application.

../_images/syscfg_bond_manager_configurations-cc23xx.png

Figure 227. Bond Manager Configurations

Note

Currently, there is a limitation when using SysConfig to configure the number of bonds. SysConfig will only successfully configure up to 10 bonds. If the user configures more than 10 bonds in SysConfig, the first 10 connections will bond and pair successfully while the remaining connections will pair successfully, but fail bonding. Please refer to GAPBondMgr and NV for information on how to configure more than 10 bonds.

Advanced Settings

In this category you will find settings that configure the application such as Power Management. You can also configure whether to use RCOSC and/or PTM mode. You will also find ICall options. More information:

  1. Power Management

  2. HAL Assert Handling

  3. Extended Stack Settings, see Link Layer (LL)

  4. GAPBondMgr and NV

  5. Production and Direct Test Mode (PTM, DTM)

  6. ICall, see: Creating Additional ICall Enabled Tasks

  7. sec-adaptivity-using-daa

Central Configuration

../_images/syscfg_central_configurations.png

Figure 228. Central Configurations

Observer Configuration

../_images/syscfg_observer_configurations-cc23xx.png

Figure 229. Observer Configurations

Peripheral Configuration

../_images/syscfg_peripheral_configurations-cc23xx.png

Figure 230. Peripheral Configurations

Broadcaster Configuration

  1. GAP Roles

  2. Advertisements

    For each advertisement set, the advertisement parameters (Advertisment Type, Channels, TX Power…), the advertisement data and the scan response can be set. The TX Power parameter will not affect Legacy Advertisement sets.

../_images/syscfg_broadcaster_configurations-cc23xx.png

Figure 231. Broadcaster Configurations

Device Configuration

The Device Configuration pannel located in the Software -> BLE panel is as shown below. This pannel let you choose the LF Clock Source between LF XOSC or LF RCOSC.

Voltage regulator DC-DC or GLDO can also be selected.

../_images/syscfg_device_configuration.png