Connection Monitoring - The Feature

The Connection Monitoring feature is a proprietary feature of the BLE-stack provided through TI’s Simplelink ® SDK. The purpose of this feature is to enable a CC23xx or CC27xx to monitor an active Bluetooth LE connection between any two devices , provided the connection parameters are provided to the CC23xx or CC27xx. This feature can be used in applications like locationing, tracking connection status and more. This section will cover the what, why, when and who for the connection monitor. In other words, the following will be covered in this section:

  • When can the connection monitor be enabled?

  • Who can the connection monitor track in active connections?

  • What data is needed for enabling the connection monitor on an ongoing connection, and what is the output from the Connection Monitor.

  • How does the connection monitor work, and how to debug the connection monitor?

Enabling the Connection Monitoring Feature

This section talks about when the Connection Monitor feature can be enabled. The process for enabling the Connection Monitor feature starts much before writing code for it in the application layer. In order to enable the connection monitoring feature in your application, you will need to start by enabling the Connection Monitor feature in SysConfig.

../_images/Enable_CMR.png

Figure 130. Enabling the Connection Monitor feature of the TI BLE stack.

This is very important, as the aforementioned compiler macro is used by the compiler to include/exclude code from the SDK.

Warning

If the Connection Monitor check-box is not checked, it will cause the compiler macro to not be defined in turn leading to the compilation errors, incurring hard-faults in the system, or getting incorrect size of memory blocks allocated for various purposes!

For a connection monitor device, referred to as candidate node in this document, to start monitoring a connection, the candidate node needs to receive the connection parameters for that connection. This can be provided directly by one of the devices involved in the connection, i.e. the peripheral or the central. The device that provides the connection information will hence be called the serving side, and the APIs that have the prefix CMS will pertain to the serving side. It is worthwhile noting that since the connection monitor does not actively participate in a connection, not all of the connection information is relevant for the connection monitor. In effect this means that when the serving side, is preparing to send the connection information to the candidate node, only a sub-set of the connection information needs to be provided.

The API cmErrorCodes_e CMS_GetConnData(uint16_t connHandle, cmsConnDataParams_t *pData) can be called from the application layer on the serving side, where the connHandle is the connection handle of the connection you want to get connection parameters for, and pData is a pointer to a data structure of type cmsConnDataParams_t to store information required by the connection monitor. This struct contains two elements, one that tracks the length of the connection information data it has been populated with, and the other is a pointer to a memory block which shall contain the information needed by the candidate node. It is the application’s responsibility to make sure that a memory block has been allocated to be used for storing connection parameters. The application should also ensure that the memory block allocated for storing connection parameters is word aligned (4-byte aligned). If the memory block is not properly aligned, it could lead to a hard fault occurring due to unaligned access.

The aforementioned API CMS_GetConnData(), will uniquely identify the connection using the provided connection handle, it will then find the pointer to the connection information for that connection. From the connection parameters, it will then populate the memory block, the pointer to which is provided as a parameter to CMS_GetConnData(), with the relevant information needed by the candidate node. This information then needs to be sent to the candidate node, which will then setup for monitoring the connection on it’s side.

There is no limitation around when, during the lifetime of a connection, can a connection monitoring session be started. This means that the serving side can choose to trigger the monitoring of a connection right after it’s establishment. It can, alternatively, also choose to start monitoring the connection at any other point in time. The important thing to note here is that the connection information which will be provided to the candidate node must always be “fresh”. This means that the connection parameters must be what are valid at that instant in time, and not what was previously valid. This is especially true if the connection that the candidate node needs to monitor has recently gotten a parameter update to change the connection interval, the PHY, or the channel map. If the aforementioned data is incorrect, the candidate node will not be able to track the connection. It is as such recommended to call CMS_GetConnData() on the connHandle of interest to ensure that the connection parameters that the application layer has access to have not become stale since last use.

Tracking a connection

When the candidate node has received connection information from a serving node, and a command to start monitoring a connection, the candidate node will try to establish a monitoring session. Without getting into the details of how this is done just yet, upon successful establishment of the connection monitoring session, the candidate node can now sniff packets sent between the central and the peripheral every connection event. The connection monitor is designed such that it expects to sniff two connection event packets from every connection event. The first being from the central to the peripheral, and the second being the peripheral’s response to the central. For each packet that is successfully sniffed by the candidate node, a connection monitor report message is sent up to the application layer.

The application layer receives information like the RSSI value of the last packet that was received, the origin of the packet (if it was from the central or the peripheral), the channel number that the packet was received on, and more. The connection monitor report cannot be filtered by role, and all RSSI reports will be forwarded to the application. It is possible to configure each connection monitoring session uniquely, and independently, to allow for using session specific connection role masks. This allows the application to only receive the connection monitor report from a certain role. For instance, if a connection monitoring session is set up to only report successfully sniffed packets from the peripheral to the central, the application layer will receive a message every time the candidate node has successfully received that packet, but no message for successfully sniffing the central to peripheral packet. Implementing connection role masks may also help with minimizing the amount of message traffic from the stack to the application layer.

For as long as the connection parameters do not change, the candidate node can manage to continuously monitor a connection. When the connection parameters/channel map changes on the serving node’s side, the candidate node must also immediately receive the parameter update so that the monitoring session can be updated. If this does not happen, then the candidate node may no longer be able to track the connection, resulting in the failure of that monitoring session. The serving node will then need to restart the process for starting a connection monitoring session.

Inner Workings of the Connection Monitor

The connection monitor feature presents itself to the application designer as a black-box, since the connection monitoring feature is not standardized by the BLE specification. This can make it harder to understand how the connection monitor works, what kind of timing requirements are necessary from a system level, and how the application designer can go about debugging the feature, should that ever become relevant. Through this section, using a logic trace for the PA (Radio TX), and LNA (Radio RX) pins from the candidate node, the central and the peripheral, the application designer will become more familiar with what to look for to ensure that everything works as expected, and if it doesn’t, how to go about fixing it.

When running the connection monitor from the Simplelink ® SDK, the user has access to three forms of outputs from the demo:

  • UART print to the terminal (Powershell, Command Prompt, etc): Enabled out-of-Box

  • Log statements saved to a .txt file: Enabled out-of-Box

  • RF Observables (visualize the activity of the radio, and timing): Not enabled out-of-Box, sysconfig changes required to enable this. Refer to the Loading FW Images section in the Connection Monitor Overview document on how to do this.

The UART prints to the terminal capture live state of the demo, printing RSSI reports in realtime, and showing the different BLE events occuring. The .txt logs are more technical and contain raw UART data that is transferred between the candidate and serving nodes. The log file output can come in handy when trying to examine the exchanged data, and extracting and understanding the flow of information between the host PC, candidate and serving nodes.

../_images/example_output_CMR_demo_connRoleMask.png

Figure 131. Example output when running the out-of-box Connection Monitor Demo

In the example output presented above, the prints showcase that the com-ports to the candidate node, and the serving node have been opened. It shows the serving node, referred to as the Car Node, scanning for advertisement from the Key Node (peripheral device). Upon discovering the advertising report from Key Node, the serving node initiates a connection, and a pairing request. When these succeed, the connection parameters, and information is forwarded to the candidate node to start monitoring the connection. Upon successfully starting a connection monitor session, the reports are printed containing RSSI, and more information.

Note

In the image above, the connection role Mask is set to central. This is why the reports from the candidate node only show the central in the connection role field of the report.

When the connection role mask is set to both central + peripheral, the report from the candidate node, look like this:

../_images/example_output_CMR_demo.png

Figure 132. Example output with connection role mask set to central plus peripheral

RF observables and the Connection Monitor Demo

In this sub-section, a logic trace of the RF Observables is shown which will help demonstrate the manner in which the connection monitor works. Important terminology for this section:

  • Key Node: Advertising peripheral, with advertising interval set to 1s

  • Car Node: The serving node. Scanning for advertising from a device called “Key Node”. When it finds this device, it will initiate a connection, and sub-sequently initiate a pairing request.

    • This is a multi-role device. It means that it is possible to connect to the car node device with the phone acting as a central. The connection parameters for the connection between the phone and the car node will then be sent to The candidate node for monitoring.

  • CMR Node: The candidate node. This node will wait to receive connection parameters, and connection monitor start/stop commands from the serving node. In addition to monitoring the connection that has been forwarded from the serving node, the CMR node can also maintain a connection in parallel as a peripheral.

  • PA: Power Amplifier RF Observable, active-high when the radio is transmitting.

  • LNA: Low-Noise Amplifier RF Observable, active-high when the radio is scanning.

The following figure visualizes advertising from the key node:

../_images/Key_Node_advInterval_1s.png

Figure 133. Key Node advertising with a 1s adv. interval

When the out-of-box demo is started, the Car Node will start scanning to find advertising from the Key Node. The scan window, which is equal to the scan interval here is set to be 10ms. This means that every 10ms the Car Node will switch to a different BLE advertising channel, always starting on channel 37, then moving to 38, then 39 and so on. This is depicted in the following image:

../_images/CarNode_infinite_scan_start.png

Figure 134. Car Node scanning with scan interval = scan window = 10ms

When the Car Node manages to successfully receive an advertising packet on the channel it is scanning on, it will initiate a connection establishment. This is showcased in the following figure:

../_images/link_establishment_CN_KN.png

Figure 135. Car Node initiating a connection with the Key Node.

The image above showcases an overlap between the PA of the Key Node, and the LNA of the Car Node (marker 0). Since the Key Node advertises with connectable advertising, right after emitting the advertising packet, it opens a receive window which is when the Car Node sends the Connection Indication Packet. This marks the creation of a link. At the next connection interval, the Car Node sends a packet first, followed by the Key Node sending a packet. This marks the establishment of the connection. The connection event for the connection between the Car Node and the Key Node is set to 30ms. This is shown in the following image.

../_images/connEvents.png

Figure 136. Connection Events spaced 30ms apart.

The out-of-Box demo gets the connection information, and sends it to the CMR node when the link established event is received by the application layer. Following this, the Car Node then sends the information to the CMR Node. From the received connection information, and the information about the transmission delay between the Car Node, and the CMR node, the CMR node will calculate which channel to listen on for the next connection event between the Car Node and the Key Node device. It will then open scan windows hoping to catch this event, for a maximum number of attempts, as defined in the CM_StartMonitor() API. Initially the CMR node will open the first scan window slightly before the start of the connection event. It does this to ensure that the connection event is not missed, and that packets between the central and the peripheral are both received correctly. The wide scan windows are opened for a fixed number of windows as defined in software by the adjustment tries. After these adjustment tries, the CMR will fine tune the opening of the scan windows such that it exactly, only covers the connection event. The connection monitor now enters the adjustment mode again if there are multiple missing packets (which can be caused by bad RSSI values for example). The start of the monitoring session is captured in the image below.

../_images/CMR_start_monitoring.png

Figure 137. CMR starts monitoring the connection between the Car and Key Node.

The scan window fine tuning by the CMR is captured in the following image. In the out-of-Box demo, the maximum number of adjustment tries is set to 5, which means that after the first 5 scan windows, the CMR node will fine tune the timing of the scan windows. Notice the sharper timing from marker 5 in the image below.

../_images/scan_window_timing_improvement_CMR.png

Figure 138. CMR fine tunes the timing of the scan window.

This concludes the section describing the expected behavior for the RF observables from the out-of-box demo.

Note

When the connection monitor role is in adjustment mode, the connection monitor will report an UNDETERMINED status, since the CMR is unable to determine the identity of the packet.