Porting and Migration Guides

Migration Guides

Migration guides are used to migrate major changes, e.g. from one device to another device or from one configuration to another.

Note

The F3 SDK 8.40 introduces the RNG Health Check functionality: the RNG driver random number generation APIs will now perform an entropy check and not generate any output if the entropy is not within acceptable ranges; in such case random number generation should be re-attempted. This could cause existing implementations of RNG to not work as expected.

Listing 203. Code snippet for checking RNG
for(int i = 0; i < n; i++) //n should be set to at least 5 or 10
{
    rclStatus = RCL_AdcNoise_get_samples_blocking(localNoiseInput, RNGLPF3RF_noiseInputWordLen);

    // Initialize the RNG driver noise input pointer with global noise input array from user //
    rclStatus = RNGLPF3RF_conditionNoiseToGenerateSeed(localNoiseInput);

    if(rclStatus = 0)
    {
    //RNG driver has succeeded generating a number
    break;
    }

    else if(i == (n-1))
    {
    //error handling, report error here
    }
}