API Documentation  9.14.00
Data Fields
PDMCC26XX_I2S_Config Struct Reference

The PDMCC26XX_I2S_Config structure contains a set of pointers used to characterize the PDMCC26XX_I2S driver implementation. More...

Data Fields

void const * hwAttrs
 
void * object
 

Detailed Description

The PDMCC26XX_I2S_Config structure contains a set of pointers used to characterize the PDMCC26XX_I2S driver implementation.

Field Documentation

§ hwAttrs

void const* PDMCC26XX_I2S_Config::hwAttrs

Pointer to a driver specific hardware attributes structure

§ object

void* PDMCC26XX_I2S_Config::object

Pointer to a driver specific data object


The documentation for this struct was generated from the following file: