|
API Documentation
9.14.00
|
DisplayUart2 Attributes. More...
Data Fields | |
| unsigned int | baudRate |
| unsigned int | mutexTimeout |
| char * | strBuf |
| uint16_t | strBufLen |
| unsigned int | uartIdx |
DisplayUart2 Attributes.
The DisplayUart2 driver uses a buffer for formatting messages, which is then passed to UART2_write(). The location and size of the buffer are specified in a DisplayUart2_HWAttrs structure. Access to the buffer is synchronized by a semaphore. The timeout for acquiring the semaphore is specified in the attributes.
| unsigned int DisplayUart2_HWAttrs::baudRate |
Baud rate for uart
| unsigned int DisplayUart2_HWAttrs::mutexTimeout |
Timeout for acquiring semaphore
| char* DisplayUart2_HWAttrs::strBuf |
Buffer for formatting messages
| uint16_t DisplayUart2_HWAttrs::strBufLen |
Size of buffer
| unsigned int DisplayUart2_HWAttrs::uartIdx |
Index of uart in UART_config[]
1.8.12