|
API Documentation
9.14.00
|
ADCBuf parameters used with ADCBuf_open(). More...
Data Fields | |
| uint32_t | blockingTimeout |
| ADCBuf_Callback | callbackFxn |
| void * | custom |
| ADCBuf_Recurrence_Mode | recurrenceMode |
| ADCBuf_Return_Mode | returnMode |
| uint32_t | samplingFrequency |
ADCBuf parameters used with ADCBuf_open().
ADCBuf_Params_init() must be called prior to setting fields in this structure.
| uint32_t ADCBuf_Params::blockingTimeout |
Timeout in system clock ticks. This value is only valid when using ADCBuf_RETURN_MODE_BLOCKING. A call to ADCBuf_convert() will block for a duration up to blockingTimeout ticks. The call to ADCBuf_convert() will return prior if the requested number of samples in ADCBuf_Conversion.samplesRequestedCount are completed. The blockingTimeout should be large enough to allow for ADCBuf_Conversion.samplesRequestedCount samples to be collected given the ADCBuf_Params.samplingFrequency.
| ADCBuf_Callback ADCBuf_Params::callbackFxn |
Pointer to a ADCBuf_Callback function to be invoked after a conversion completes when operating in ADCBuf_RETURN_MODE_CALLBACK.
| void* ADCBuf_Params::custom |
Pointer to a device specific extension of the ADCBuf_Params
| ADCBuf_Recurrence_Mode ADCBuf_Params::recurrenceMode |
ADCBuf_Recurrence_Mode for all conversions.
| ADCBuf_Return_Mode ADCBuf_Params::returnMode |
ADCBuf_Return_Mode for all conversions.
| uint32_t ADCBuf_Params::samplingFrequency |
The frequency at which the ADC will sample in Hertz (Hz). After a call to ADCBuf_convert(), the ADC will perform samplingFrequency samples per second.
1.8.12