API Documentation  9.14.00
Data Structures
I2CCC26XX.h File Reference

I2C driver implementation for a CC26XX I2C controller. More...

Go to the source code of this file.

Data Structures

struct  I2CCC26XX_HWAttrsV1
 I2CCC26XX Hardware attributes. More...
 
struct  I2CCC26XX_I2CPinCfg
 I2CCC26XX Pin Configuration. More...
 
struct  I2CCC26XX_Object
 I2CCC26XX Object. More...
 

Detailed Description

I2C driver implementation for a CC26XX I2C controller.


Driver Include

The I2C header file should be included in an application as follows:

Refer to I2C.h for a complete description of APIs.

Overview

Refer to I2C.h for a complete description of APIs.

General Behavior

Before using the I2C in CC26XX:

The following is true for receive operation:

The following apply for transmit operation:

After I2C operation has ended:

Known Issue

Warning
The I2C will transmit a single data byte in the event that the I2C target address is not acknowledged (NACK'd). This is due to a known hardware bug.

Error handling

If an error occurs during operation:

Power Management

The I2CCC26XX driver sets a power constraint during transactions to keep the device out of standby; so when all tasks are blocked, the device will enter idle mode instead of standby. When the transactions have finished, the power constraint to prohibit standby is released. The following statements are valid:

Supported Functions

Generic API Function Description
I2C_init() Initialize I2C driver
I2C_Params_init() Initialize an I2C_Params structure
I2C_open() Initialize I2C HW and set system dependencies
I2C_close() Disable I2C HW and release system dependencies
I2C_transfer() Start I2C transfer
I2C_transferTimeout() Start I2C transfer with a timeout
I2C_cancel() Cancels all I2C transfers

Supported Bit Rates

Supported Address Modes

Unsupported Functionality

The CC26XX I2C driver currently does not support:

Instrumentation

The I2C driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 basic I2C operations performed
Diags_USER2 detailed I2C operations performed