81 #ifndef ti_display_DisplayHost__include 82 #define ti_display_DisplayHost__include 122 void DisplayHost_clearLines(
Display_Handle handle, uint8_t fromLine, uint8_t toLine);
123 void DisplayHost_vprintf(
Display_Handle handle, uint8_t line, uint8_t column,
const char *fmt, va_list va);
125 int DisplayHost_control(
Display_Handle handle,
unsigned int cmd,
void *arg);
126 unsigned int DisplayHost_getType(
void);
uint16_t strBufLen
Definition: DisplayHost.h:102
DisplayHost Object.
Definition: DisplayHost.h:110
Display Parameters.
Definition: Display.h:485
struct DisplayHost_HWAttrs DisplayHost_HWAttrs
DisplayHost Attributes.
Generic interface for text output.
DisplayHost Attributes.
Definition: DisplayHost.h:97
struct DisplayHost_Object DisplayHost_Object
DisplayHost Object.
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:535
char * strBuf
Definition: DisplayHost.h:100
Display Global configuration.
Definition: Display.h:558