33 #ifndef ti_display_DisplayDogm1286__include 34 #define ti_display_DisplayDogm1286__include 36 #include <ti/drivers/dpl/SemaphoreP.h> 40 #include <ti/display/lcd/LCDDogm1286.h> 49 uint_least8_t powerPin;
56 SemaphoreP_Struct lcdMutex;
57 char lcdBuffer0[1024];
58 LCD_Buffer lcdBuffers[1];
64 void DisplayDogm1286_clearLines(
Display_Handle handle, uint8_t fromLine, uint8_t toLine);
65 void DisplayDogm1286_vprintf(
Display_Handle handle, uint8_t line, uint8_t column,
const char *fmt, va_list va);
67 int DisplayDogm1286_control(
Display_Handle handle,
unsigned int cmd,
void *arg);
68 unsigned int DisplayDogm1286_getType(
void);
69 #endif // ti_display_DisplayDogm1286__include Serial Peripheral Interface (SPI) Driver Interface.
Display Parameters.
Definition: Display.h:485
Generic interface for text output.
Definition: DisplayDogm1286.h:52
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:535
Definition: DisplayDogm1286.h:46
Display Global configuration.
Definition: Display.h:558
Display_LineClearMode
How to treat existing elements on a line when writing text.
Definition: Display.h:469