TI OAD API Documentation  9.14.00
Data Fields
HSMBareMetal_AssetOperationStruct Struct Reference

Struct containing the parameters required for asset create and plaintext key load operations. More...

Data Fields

HSMBareMetal_AESOperationMode aesOperationMode
 
HSMBareMetal_operationAlgorithm algorithm
 
bool isKeyGenerated
 
uint8_t * key
 
HSMBareMetal_AssetPairStruct keyAssetIDs
 
HSMBareMetal_AssetPairKeyBlobStruct keyBlobs
 
uint8_t keyLength
 
HSMBareMetal_MACOperationMode macOperationMode
 
HSMBareMetal_AssetOperationType operationType
 

Detailed Description

Struct containing the parameters required for asset create and plaintext key load operations.


The documentation for this struct was generated from the following file: