![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.00
|
PSM information format. More...
Data Fields | |
| uint16 | initPeerCredits |
| Number of LE-frames that peer device can send. More... | |
| uint8 | maxNumChannels |
| Maximum number of CO Channels supported by PSM. More... | |
| uint16 | mps |
| Maximum payload size that can be received by local device. More... | |
| uint16 | mtu |
| Maximum SDU size that can be received by local device. More... | |
| uint8 | numActiveChannels |
| Number of active CO Channels. More... | |
| uint16 | peerCreditThreshold |
| Low threshold for number of peer credits. More... | |
PSM information format.
| uint16 initPeerCredits |
Number of LE-frames that peer device can send.
| uint8 maxNumChannels |
Maximum number of CO Channels supported by PSM.
| uint16 mps |
Maximum payload size that can be received by local device.
| uint16 mtu |
Maximum SDU size that can be received by local device.
| uint8 numActiveChannels |
Number of active CO Channels.
| uint16 peerCreditThreshold |
Low threshold for number of peer credits.