TI BLE5-Stack API Documentation  9.14.00
Data Fields
hciRetParam_LeReadBufSize_t Struct Reference

Data structure for HCI Command Complete Event Return Parameter. More...

Data Fields

uint16 dataPktLen
 data packet length More...
 
uint8 numDataPkts
 number of data packets More...
 
uint8 status
 status of event More...
 

Detailed Description

Data structure for HCI Command Complete Event Return Parameter.

Field Documentation

§ dataPktLen

uint16 dataPktLen

data packet length

§ numDataPkts

uint8 numDataPkts

number of data packets

§ status

uint8 status

status of event


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale