TI BLE5-Stack API Documentation  9.14.00
Data Fields
hciEvt_VSCmdComplete_t Struct Reference

Vendor Specific Command Complete Event. More...

Data Fields

uint16 cmdOpcode
 command opcode More...
 
event_hdr_t hdr
 osal event header More...
 
uint8 length
 length of parametric data, in bytes More...
 
uint8 * pEventParam
 event parameters More...
 

Detailed Description

Vendor Specific Command Complete Event.

Field Documentation

§ cmdOpcode

uint16 cmdOpcode

command opcode

§ hdr

osal event header

§ length

uint8 length

length of parametric data, in bytes

§ pEventParam

uint8* pEventParam

event parameters


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale