TI BLE5-Stack API Documentation  9.14.00
Data Fields
hciEvt_CmdComplete_t Struct Reference

Command Complete Event. More...

Data Fields

uint16 cmdOpcode
 command opcode More...
 
event_hdr_t hdr
 osal event header More...
 
uint8 numHciCmdPkt
 number of HCI Command Packet More...
 
uint8 * pReturnParam
 pointer to the return parameter More...
 

Detailed Description

Command Complete Event.

Field Documentation

§ cmdOpcode

uint16 cmdOpcode

command opcode

§ hdr

osal event header

§ numHciCmdPkt

uint8 numHciCmdPkt

number of HCI Command Packet

§ pReturnParam

uint8* pReturnParam

pointer to the return parameter


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale