TI BLE5-Stack API Documentation  9.14.00
Data Fields
hciEvt_BLETransPwrReport_t Struct Reference

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint16 connHandle
 Connection handle. More...
 
uint8 delta
 The change of the Tx Power from previous power level. More...
 
event_hdr_t hdr
 Osal event header. More...
 
uint8 reason
 Who trigger the event - local or remote. More...
 
uint8 status
 status of event More...
 
uint8 txPhy
 On which phy the report is trigger. More...
 
uint8 txPowerFlag
 Tx Power at minimum or maximum level. More...
 
uint8 txPowerLevel
 Amount of power transmitting. More...
 

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ connHandle

uint16 connHandle

Connection handle.

§ delta

uint8 delta

The change of the Tx Power from previous power level.

§ hdr

Osal event header.

§ reason

uint8 reason

Who trigger the event - local or remote.

§ status

uint8 status

status of event

§ txPhy

uint8 txPhy

On which phy the report is trigger.

§ txPowerFlag

uint8 txPowerFlag

Tx Power at minimum or maximum level.

§ txPowerLevel

uint8 txPowerLevel

Amount of power transmitting.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale