TI BLE5-Stack API Documentation  9.14.00
Data Fields
hciEvt_BLEPeriodicAdvSyncEstablished_t Struct Reference

LE Periodic Advertising Sync Established event. More...

Data Fields

uint8 address [B_ADDR_LEN]
 Peer address. More...
 
uint8 addrType
 Peer address type. More...
 
uint8 BLEEventCode
 BLE Event Code. More...
 
uint8 clockAccuracy
 Peer Clock Accuracy. More...
 
event_hdr_t hdr
 osal event header More...
 
uint16 periodicInterval
 Periodic interval. More...
 
uint8 phy
 Peer PHY. More...
 
uint8 sid
 Peer SID. More...
 
uint8 status
 status of event More...
 
uint16 syncHandle
 sync handle More...
 

Detailed Description

LE Periodic Advertising Sync Established event.

Field Documentation

§ address

uint8 address[B_ADDR_LEN]

Peer address.

§ addrType

uint8 addrType

Peer address type.

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ clockAccuracy

uint8 clockAccuracy

Peer Clock Accuracy.

§ hdr

osal event header

§ periodicInterval

uint16 periodicInterval

Periodic interval.

§ phy

uint8 phy

Peer PHY.

§ sid

uint8 sid

Peer SID.

§ status

uint8 status

status of event

§ syncHandle

uint16 syncHandle

sync handle


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale