TI BLE5-Stack API Documentation  9.14.00
Data Fields
hciEvt_BLEPeriodicAdvReport_t Struct Reference

LE Periodic Advertising Report event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint8 cteType
 CTE type received. More...
 
uint8 * data
 Periodic data received from peer. More...
 
uint8 dataLen
 Periodic data length. More...
 
uint8 dataStatus
 Periodic data status. More...
 
event_hdr_t hdr
 osal event header More...
 
int8 rssi
 RSSI of the received packet. More...
 
uint16 syncHandle
 sync handle More...
 
int8 txPower
 Tx Power information. More...
 

Detailed Description

LE Periodic Advertising Report event.

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ cteType

uint8 cteType

CTE type received.

§ data

uint8* data

Periodic data received from peer.

§ dataLen

uint8 dataLen

Periodic data length.

§ dataStatus

uint8 dataStatus

Periodic data status.

§ hdr

osal event header

§ rssi

int8 rssi

RSSI of the received packet.

§ syncHandle

uint16 syncHandle

sync handle

§ txPower

int8 txPower

Tx Power information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale