TI BLE5-Stack API Documentation  9.14.00
Data Fields
hciEvt_BLECteConnectionlessIqReport_t Struct Reference

LE CTE Connectionless IQ Report Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint8 channelIndex
 index of channel More...
 
uint8 cteType
 cte type More...
 
uint16 eventCounter
 periodic adv event counter More...
 
event_hdr_t hdr
 osal event header More...
 
int8 * iqSamples
 list of interleaved I/Q samples More...
 
uint16 rssi
 current rssi More...
 
uint8 rssiAntenna
 antenna ID More...
 
uint8 sampleCount
 number of samples More...
 
uint8 slotDuration
 sampling slot 1us or 2us More...
 
uint8 status
 packet status (success or CRC error) More...
 
uint16 syncHandle
 sync handle in periodic adv More...
 

Detailed Description

LE CTE Connectionless IQ Report Event.

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ channelIndex

uint8 channelIndex

index of channel

§ cteType

uint8 cteType

cte type

§ eventCounter

uint16 eventCounter

periodic adv event counter

§ hdr

osal event header

§ iqSamples

int8* iqSamples

list of interleaved I/Q samples

§ rssi

uint16 rssi

current rssi

§ rssiAntenna

uint8 rssiAntenna

antenna ID

§ sampleCount

uint8 sampleCount

number of samples

§ slotDuration

uint8 slotDuration

sampling slot 1us or 2us

§ status

uint8 status

packet status (success or CRC error)

§ syncHandle

uint16 syncHandle

sync handle in periodic adv


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale