![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.00
|
LE Connection Complete Event. More...
Data Fields | |
| uint8 | BLEEventCode |
| BLE Event Code. More... | |
| uint8 | clockAccuracy |
| connection clock accuracy More... | |
| uint16 | connectionHandle |
| connection handle More... | |
| uint16 | connInterval |
| connection interval More... | |
| uint16 | connLatency |
| connection latency More... | |
| uint16 | connTimeout |
| connection supervision timeout More... | |
| event_hdr_t | hdr |
| osal event header More... | |
| uint8 | peerAddr [B_ADDR_LEN] |
| peer address More... | |
| uint8 | peerAddrType |
| peer address type More... | |
| uint8 | role |
| role of connection More... | |
| uint8 | status |
| status of event More... | |
LE Connection Complete Event.
| uint8 BLEEventCode |
BLE Event Code.
| uint8 clockAccuracy |
connection clock accuracy
| uint16 connectionHandle |
connection handle
| uint16 connInterval |
connection interval
| uint16 connLatency |
connection latency
| uint16 connTimeout |
connection supervision timeout
| event_hdr_t hdr |
osal event header
| uint8 peerAddr[B_ADDR_LEN] |
peer address
| uint8 peerAddrType |
peer address type
| uint8 role |
role of connection
| uint8 status |
status of event