![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.00
|
GATT_CLIENT_CHAR_CFG_UPDATED_EVENT message format. More...
Data Fields | |
| uint16 | attrHandle |
| attribute handle More... | |
| uint16 | connHandle |
| Connection message was received on. More... | |
| osal_event_hdr_t | hdr |
| GATT_SERV_MSG_EVENT and status. More... | |
| uint8 | method |
| GATT_CLIENT_CHAR_CFG_UPDATED_EVENT. More... | |
| uint16 | value |
| attribute new value More... | |
GATT_CLIENT_CHAR_CFG_UPDATED_EVENT message format.
This message is sent to the app when a Client Characteristic Configuration is updated.
| uint16 attrHandle |
attribute handle
| uint16 connHandle |
Connection message was received on.
| osal_event_hdr_t hdr |
GATT_SERV_MSG_EVENT and status.
| uint8 method |
GATT_CLIENT_CHAR_CFG_UPDATED_EVENT.
| uint16 value |
attribute new value